<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic stuckd: Bringing up secondary CPUs in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/stuckd-Bringing-up-secondary-CPUs/m-p/1314535#M8582</link>
    <description>&lt;P&gt;my custome board is lx2080。&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The kernel is stuck during boot&amp;nbsp;&lt;/SPAN&gt;smp, location is&amp;nbsp; Bringing up secondary CPUs ...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;SPAN&gt;Can you offer some ideas to solve this problem。&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;...........&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;[ 0.000000] ITS: using cache flushing for cmd queue&lt;BR /&gt;[ 0.000000] GICv3: Using preallocated redistributor tables&lt;BR /&gt;[ 0.000000] val: 207fe0008f&lt;BR /&gt;[ 0.000000]&lt;BR /&gt;[ 0.000000] 11111 gic_rdists-&amp;gt;prop_table_pa 207fe00000&lt;BR /&gt;[ 0.000000] 22222 gic_rdists-&amp;gt;prop_table_pa 207fe00000&lt;BR /&gt;[ 0.000000] prop_table_va (____ptrval____)&lt;BR /&gt;[ 0.000000] LPI_PROPBASE_SZ 10000&lt;BR /&gt;[ 0.000000] GICv3: using LPI property table @0x000000207fe00000&lt;BR /&gt;[ 0.000000] GICv3: CPU0: using reserved LPI pending table @0x000000207fe10000&lt;BR /&gt;[ 0.000000] random: get_random_bytes called from start_kernel+0x2b8/0x450 with crng_init=0&lt;BR /&gt;[ 0.000000] arch_timer: cp15 timer(s) running at 25.00MHz (phys).&lt;BR /&gt;[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x5c409fb33, max_idle_ns: 440795203156 ns&lt;BR /&gt;[ 0.000002] sched_clock: 56 bits at 25MHz, resolution 39ns, wraps every 4398046511103ns&lt;BR /&gt;[ 0.008378] Console: colour dummy device 80x25&lt;BR /&gt;[ 0.012915] Calibrating delay loop (skipped), value calculated using timer frequency.. 50.00 BogoMIPS (lpj=100000)&lt;BR /&gt;[ 0.023386] pid_max: default: 32768 minimum: 301&lt;BR /&gt;[ 0.028144] LSM: Security Framework initializing&lt;BR /&gt;[ 0.032872] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)&lt;BR /&gt;[ 0.040361] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)&lt;BR /&gt;[ 0.072334] ASID allocator initialised with 32768 entries&lt;BR /&gt;[ 0.085810] rcu: Hierarchical SRCU implementation.&lt;BR /&gt;[ 0.098700] Platform MSI: gic-its@6020000 domain created&lt;BR /&gt;[ 0.104124] PCI/MSI: /interrupt-controller@6000000/gic-its@6020000 domain created&lt;BR /&gt;[ 0.111729] fsl-mc MSI: gic-its@6020000 domain created&lt;BR /&gt;[ 0.124938] smp: Bringing up secondary CPUs ...&lt;/P&gt;&lt;/BLOCKQUOTE&gt;</description>
    <pubDate>Wed, 28 Jul 2021 12:18:25 GMT</pubDate>
    <dc:creator>muaxi8</dc:creator>
    <dc:date>2021-07-28T12:18:25Z</dc:date>
    <item>
      <title>stuckd: Bringing up secondary CPUs</title>
      <link>https://community.nxp.com/t5/Layerscape/stuckd-Bringing-up-secondary-CPUs/m-p/1314535#M8582</link>
      <description>&lt;P&gt;my custome board is lx2080。&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The kernel is stuck during boot&amp;nbsp;&lt;/SPAN&gt;smp, location is&amp;nbsp; Bringing up secondary CPUs ...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;SPAN&gt;Can you offer some ideas to solve this problem。&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;...........&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;[ 0.000000] ITS: using cache flushing for cmd queue&lt;BR /&gt;[ 0.000000] GICv3: Using preallocated redistributor tables&lt;BR /&gt;[ 0.000000] val: 207fe0008f&lt;BR /&gt;[ 0.000000]&lt;BR /&gt;[ 0.000000] 11111 gic_rdists-&amp;gt;prop_table_pa 207fe00000&lt;BR /&gt;[ 0.000000] 22222 gic_rdists-&amp;gt;prop_table_pa 207fe00000&lt;BR /&gt;[ 0.000000] prop_table_va (____ptrval____)&lt;BR /&gt;[ 0.000000] LPI_PROPBASE_SZ 10000&lt;BR /&gt;[ 0.000000] GICv3: using LPI property table @0x000000207fe00000&lt;BR /&gt;[ 0.000000] GICv3: CPU0: using reserved LPI pending table @0x000000207fe10000&lt;BR /&gt;[ 0.000000] random: get_random_bytes called from start_kernel+0x2b8/0x450 with crng_init=0&lt;BR /&gt;[ 0.000000] arch_timer: cp15 timer(s) running at 25.00MHz (phys).&lt;BR /&gt;[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x5c409fb33, max_idle_ns: 440795203156 ns&lt;BR /&gt;[ 0.000002] sched_clock: 56 bits at 25MHz, resolution 39ns, wraps every 4398046511103ns&lt;BR /&gt;[ 0.008378] Console: colour dummy device 80x25&lt;BR /&gt;[ 0.012915] Calibrating delay loop (skipped), value calculated using timer frequency.. 50.00 BogoMIPS (lpj=100000)&lt;BR /&gt;[ 0.023386] pid_max: default: 32768 minimum: 301&lt;BR /&gt;[ 0.028144] LSM: Security Framework initializing&lt;BR /&gt;[ 0.032872] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)&lt;BR /&gt;[ 0.040361] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)&lt;BR /&gt;[ 0.072334] ASID allocator initialised with 32768 entries&lt;BR /&gt;[ 0.085810] rcu: Hierarchical SRCU implementation.&lt;BR /&gt;[ 0.098700] Platform MSI: gic-its@6020000 domain created&lt;BR /&gt;[ 0.104124] PCI/MSI: /interrupt-controller@6000000/gic-its@6020000 domain created&lt;BR /&gt;[ 0.111729] fsl-mc MSI: gic-its@6020000 domain created&lt;BR /&gt;[ 0.124938] smp: Bringing up secondary CPUs ...&lt;/P&gt;&lt;/BLOCKQUOTE&gt;</description>
      <pubDate>Wed, 28 Jul 2021 12:18:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/stuckd-Bringing-up-secondary-CPUs/m-p/1314535#M8582</guid>
      <dc:creator>muaxi8</dc:creator>
      <dc:date>2021-07-28T12:18:25Z</dc:date>
    </item>
    <item>
      <title>Re: stuckd: Bringing up secondary CPUs</title>
      <link>https://community.nxp.com/t5/Layerscape/stuckd-Bringing-up-secondary-CPUs/m-p/1315787#M8605</link>
      <description>&lt;P&gt;Please download image&amp;nbsp;lsdk2012_yocto_tiny_LS_arm64.itb to do verification on your target board.&lt;/P&gt;
&lt;P&gt;wget &lt;A href="https://www.nxp.com/lgfiles/sdk/lsdk2012/lsdk2012_yocto_tiny_LS_arm64.itb" target="_blank"&gt;https://www.nxp.com/lgfiles/sdk/lsdk2012/lsdk2012_yocto_tiny_LS_arm64.itb&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;You also could get it&amp;nbsp;&lt;/P&gt;
&lt;P&gt;链接: &lt;A href="https://pan.baidu.com/s/1IyuUe0PHXbYiIb1RVHdSzw" target="_blank"&gt;https://pan.baidu.com/s/1IyuUe0PHXbYiIb1RVHdSzw&lt;/A&gt; 提取码: 9n7z&lt;/P&gt;
&lt;P&gt;Then run the following command on the target board.&lt;/P&gt;
&lt;P&gt;=&amp;gt; pri bootargs&lt;BR /&gt;bootargs=console=ttyAMA0,115200 root=/dev/ram0 earlycon=pl011,mmio32,0x21c0000 ramdisk_size=0x2000000&lt;BR /&gt;=&amp;gt; tftp 0xa0000000 lsdk2012_yocto_tiny_LS_arm64.itb&lt;/P&gt;
&lt;P&gt;=&amp;gt; bootm 0xa0000000#lx2160ardb&lt;/P&gt;
&lt;P&gt;If this problem remains, please create a bareboard project in CodeWarrior, then run and debug the program on the second core. Please refer to the section "3.2 Working with bareboard application" in&amp;nbsp;C:\Freescale\CW4NET_v2020.06\CW_ARMv8\ARMv8\Help\Getting_Started_for_CW_ARMv8.pdf.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="yipingwang_0-1627631411801.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/151345i5756ED22465E1D01/image-size/medium?v=v2&amp;amp;px=400" role="button" title="yipingwang_0-1627631411801.png" alt="yipingwang_0-1627631411801.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 30 Jul 2021 07:51:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/stuckd-Bringing-up-secondary-CPUs/m-p/1315787#M8605</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2021-07-30T07:51:43Z</dc:date>
    </item>
    <item>
      <title>Re: stuckd: Bringing up secondary CPUs</title>
      <link>https://community.nxp.com/t5/Layerscape/stuckd-Bringing-up-secondary-CPUs/m-p/1320837#M8681</link>
      <description>&lt;P&gt;&lt;SPAN&gt;i download image&amp;nbsp;lsdk2012_yocto_tiny_LS_arm64.itb to do verification on your target board, it is still can not&amp;nbsp;Boot the second cpu.&amp;nbsp;The log is attached。&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;then i create a bareboard project in CodeWarrior, then&amp;nbsp; debug the program on the second core,&amp;nbsp;There seems to be a mistake。&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="muaxi8_0-1628577079004.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/152390i1D953F4FA5E69D84/image-size/medium?v=v2&amp;amp;px=400" role="button" title="muaxi8_0-1628577079004.png" alt="muaxi8_0-1628577079004.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 10 Aug 2021 06:36:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/stuckd-Bringing-up-secondary-CPUs/m-p/1320837#M8681</guid>
      <dc:creator>muaxi8</dc:creator>
      <dc:date>2021-08-10T06:36:53Z</dc:date>
    </item>
    <item>
      <title>Re: stuckd: Bringing up secondary CPUs</title>
      <link>https://community.nxp.com/t5/Layerscape/stuckd-Bringing-up-secondary-CPUs/m-p/1320966#M8682</link>
      <description>&lt;P&gt;In your attached log, it seems that you still used your own image created on&amp;nbsp;2021-08-10.&lt;/P&gt;&lt;P&gt;Please download the pre-built image&amp;nbsp;&lt;SPAN&gt;lsdk2012_yocto_tiny_LS_arm64.itb and run the following command.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;=&amp;gt; tftp 0xa0000000 lsdk2012_yocto_tiny_LS_arm64.itb&lt;/P&gt;&lt;P&gt;=&amp;gt; bootm 0xa0000000#lx2160ardb&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 10 Aug 2021 09:20:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/stuckd-Bringing-up-secondary-CPUs/m-p/1320966#M8682</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2021-08-10T09:20:30Z</dc:date>
    </item>
    <item>
      <title>Re: stuckd: Bringing up secondary CPUs</title>
      <link>https://community.nxp.com/t5/Layerscape/stuckd-Bringing-up-secondary-CPUs/m-p/1321017#M8684</link>
      <description>&lt;P&gt;&lt;SPAN&gt;it is&amp;nbsp; Uboot problem ， has been resolved&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 11 Aug 2021 03:58:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/stuckd-Bringing-up-secondary-CPUs/m-p/1321017#M8684</guid>
      <dc:creator>muaxi8</dc:creator>
      <dc:date>2021-08-11T03:58:27Z</dc:date>
    </item>
  </channel>
</rss>