<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: In LS1043A which is the default Eth interface for tftp programming and GPIO for Watchdog circuit</title>
    <link>https://community.nxp.com/t5/Layerscape/In-LS1043A-which-is-the-default-Eth-interface-for-tftp/m-p/1305764#M8411</link>
    <description>&lt;P&gt;Thank you for the response.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sun, 11 Jul 2021 12:22:47 GMT</pubDate>
    <dc:creator>Abhilash_PV</dc:creator>
    <dc:date>2021-07-11T12:22:47Z</dc:date>
    <item>
      <title>In LS1043A which is the default Eth interface for tftp programming and GPIO for Watchdog circuit</title>
      <link>https://community.nxp.com/t5/Layerscape/In-LS1043A-which-is-the-default-Eth-interface-for-tftp/m-p/1305743#M8404</link>
      <description>&lt;P&gt;In the LS1043A is there any default Ethernet interface (&lt;SPAN&gt;like Ethernet Controller1(EC1) or EC2&lt;/SPAN&gt;) that should be used for tftp programming?&lt;/P&gt;&lt;P&gt;Can any GPIO of&amp;nbsp;LS1043A be used for giving pulse to an external Watchdog circuit or any dedicated GPIO is available for this purpose?&lt;/P&gt;</description>
      <pubDate>Sat, 10 Jul 2021 16:18:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/In-LS1043A-which-is-the-default-Eth-interface-for-tftp/m-p/1305743#M8404</guid>
      <dc:creator>Abhilash_PV</dc:creator>
      <dc:date>2021-07-10T16:18:50Z</dc:date>
    </item>
    <item>
      <title>Re: In LS1043A which is the default Eth interface for tftp programming and GPIO for Watchdog circuit</title>
      <link>https://community.nxp.com/t5/Layerscape/In-LS1043A-which-is-the-default-Eth-interface-for-tftp/m-p/1305752#M8409</link>
      <description>&lt;P&gt;Primary Ethernet interface is defined in the board's header file, for example "ls1043ardb.h":&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/qoriq/qoriq-components/u-boot/tree/include/configs/ls1043ardb.h?h=LSDK-20.12" target="_blank"&gt;https://source.codeaurora.org/external/qoriq/qoriq-components/u-boot/tree/include/configs/ls1043ardb.h?h=LSDK-20.12&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;as&lt;/P&gt;
&lt;PRE&gt;#define CONFIG_ETHPRIME			"FM1@DTSEC3"&lt;/PRE&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;GPIOs can be used according to the board's designer needs. &lt;/P&gt;</description>
      <pubDate>Sun, 11 Jul 2021 02:20:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/In-LS1043A-which-is-the-default-Eth-interface-for-tftp/m-p/1305752#M8409</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2021-07-11T02:20:03Z</dc:date>
    </item>
    <item>
      <title>Re: In LS1043A which is the default Eth interface for tftp programming and GPIO for Watchdog circuit</title>
      <link>https://community.nxp.com/t5/Layerscape/In-LS1043A-which-is-the-default-Eth-interface-for-tftp/m-p/1305764#M8411</link>
      <description>&lt;P&gt;Thank you for the response.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 11 Jul 2021 12:22:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/In-LS1043A-which-is-the-default-Eth-interface-for-tftp/m-p/1305764#M8411</guid>
      <dc:creator>Abhilash_PV</dc:creator>
      <dc:date>2021-07-11T12:22:47Z</dc:date>
    </item>
  </channel>
</rss>