<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 Re: PTP on LS1028ARDB Felix switch</title>
    <link>https://community.nxp.com/t5/Layerscape/PTP-on-LS1028ARDB-Felix-switch/m-p/1305140#M8392</link>
    <description>&lt;P&gt;Please refer to the explanation in&amp;nbsp;&lt;A href="https://community.nxp.com/t5/Layerscape/PTP-with-L2-Forwarding-switch-LS1028ARDB/td-p/1303249" target="_blank"&gt;https://community.nxp.com/t5/Layerscape/PTP-with-L2-Forwarding-switch-LS1028ARDB/td-p/1303249&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 09 Jul 2021 04:08:27 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2021-07-09T04:08:27Z</dc:date>
    <item>
      <title>PTP on LS1028ARDB Felix switch</title>
      <link>https://community.nxp.com/t5/Layerscape/PTP-on-LS1028ARDB-Felix-switch/m-p/1303185#M8355</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have two LS1028ARDB, that I connected to each other using their SWP0 interface.&lt;BR /&gt;I then configured the "Single port mode" on both boards, to be able to use these interfaces independently (&lt;A href="https://docs.nxp.com/bundle/GUID-C3A436DA-E944-4F73-9811-2335DEBD04D6/page/GUID-F27864B5-2195-4FC0-81EA-77D341023F09.html):" target="_blank"&gt;https://docs.nxp.com/bundle/GUID-C3A436DA-E944-4F73-9811-2335DEBD04D6/page/GUID-F27864B5-2195-4FC0-81EA-77D341023F09.html)&lt;/A&gt;:&lt;BR /&gt;On Board A:&lt;BR /&gt;# ip a add 192.168.0.1/24 brd + dev swp0&lt;BR /&gt;# ip l set eno0 up&lt;BR /&gt;# ip l set swp0 up&lt;BR /&gt;On Board B:&lt;BR /&gt;# ip a add 192.168.0.2/24 brd + dev swp0&lt;BR /&gt;# ip l set eno0 up&lt;BR /&gt;# ip l set swp0 up&lt;/P&gt;&lt;P&gt;I then launch a PTP synchronization on both boards (using L2 Transport):&lt;BR /&gt;# ptp4l -i swp0 -2 -m&lt;BR /&gt;It works fine.&lt;/P&gt;&lt;P&gt;BUT, when I try to use UDP/IPv4, it doesn't work anymore:&lt;BR /&gt;# ptp4l -i swp0 -m&lt;BR /&gt;ptp4l[xxxx.xxx]: selected /dev/ptp1 as PTP clock&lt;BR /&gt;ptp4l[xxxx.xxx]: port 1: INITIALIZING to LISTENING on INIT_COMPLETE&lt;BR /&gt;ptp4l[xxxx.xxx]: port 0:&amp;nbsp;INITIALIZING to LISTENING on INIT_COMPLETE&lt;BR /&gt;ptp4l[xxxx.xxx]: port 1: LISTENING to MASTER on ANNOUNCE_RECEIPT_TIMEOUT_EXPIRES&lt;BR /&gt;ptp4l[xxxx.xxx]: selected local clock yyyyyy.yyyy.yyyyyy as best master&lt;BR /&gt;ptp4l[xxxx.xxx]: assuming the grand master role&lt;/P&gt;&lt;P&gt;Is there a problem with the configuration of the interfaces ? I don't understand why it doesn't work with IP transport but it does with L2...&lt;/P&gt;&lt;P&gt;Thank you in advance for your help.&lt;/P&gt;&lt;P&gt;ceroone&lt;/P&gt;</description>
      <pubDate>Tue, 06 Jul 2021 13:37:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/PTP-on-LS1028ARDB-Felix-switch/m-p/1303185#M8355</guid>
      <dc:creator>ceroone</dc:creator>
      <dc:date>2021-07-06T13:37:30Z</dc:date>
    </item>
    <item>
      <title>Re: PTP on LS1028ARDB Felix switch</title>
      <link>https://community.nxp.com/t5/Layerscape/PTP-on-LS1028ARDB-Felix-switch/m-p/1303189#M8356</link>
      <description>&lt;P&gt;The correct link:&amp;nbsp;&lt;A href="https://docs.nxp.com/bundle/GUID-C3A436DA-E944-4F73-9811-2335DEBD04D6/page/GUID-F27864B5-2195-4FC0-81EA-77D341023F09.html" target="_blank"&gt;https://docs.nxp.com/bundle/GUID-C3A436DA-E944-4F73-9811-2335DEBD04D6/page/GUID-F27864B5-2195-4FC0-81EA-77D341023F09.html&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 06 Jul 2021 13:39:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/PTP-on-LS1028ARDB-Felix-switch/m-p/1303189#M8356</guid>
      <dc:creator>ceroone</dc:creator>
      <dc:date>2021-07-06T13:39:32Z</dc:date>
    </item>
    <item>
      <title>Re: PTP on LS1028ARDB Felix switch</title>
      <link>https://community.nxp.com/t5/Layerscape/PTP-on-LS1028ARDB-Felix-switch/m-p/1305140#M8392</link>
      <description>&lt;P&gt;Please refer to the explanation in&amp;nbsp;&lt;A href="https://community.nxp.com/t5/Layerscape/PTP-with-L2-Forwarding-switch-LS1028ARDB/td-p/1303249" target="_blank"&gt;https://community.nxp.com/t5/Layerscape/PTP-with-L2-Forwarding-switch-LS1028ARDB/td-p/1303249&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 09 Jul 2021 04:08:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/PTP-on-LS1028ARDB-Felix-switch/m-p/1305140#M8392</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2021-07-09T04:08:27Z</dc:date>
    </item>
  </channel>
</rss>