<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic CMSIS-DAP vs JTAG in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/CMSIS-DAP-vs-JTAG/m-p/1303128#M8354</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are designing PCB board for our application that uses ls1043a processor. For programming and debugging purpose, we want to go with JTAG interface instead of CMSIS-DAP interface due to the board space constraint.&lt;/P&gt;&lt;P&gt;Let me know if it is OK to use JTAG instead of CMSIS-DAP.&lt;/P&gt;&lt;P&gt;If "No" is the answer, please tell me the proper reason for it and also let me know what are all the additional features available in CMSIS-DAP.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
    <pubDate>Tue, 06 Jul 2021 12:06:23 GMT</pubDate>
    <dc:creator>TrinathK</dc:creator>
    <dc:date>2021-07-06T12:06:23Z</dc:date>
    <item>
      <title>CMSIS-DAP vs JTAG</title>
      <link>https://community.nxp.com/t5/Layerscape/CMSIS-DAP-vs-JTAG/m-p/1303128#M8354</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are designing PCB board for our application that uses ls1043a processor. For programming and debugging purpose, we want to go with JTAG interface instead of CMSIS-DAP interface due to the board space constraint.&lt;/P&gt;&lt;P&gt;Let me know if it is OK to use JTAG instead of CMSIS-DAP.&lt;/P&gt;&lt;P&gt;If "No" is the answer, please tell me the proper reason for it and also let me know what are all the additional features available in CMSIS-DAP.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Tue, 06 Jul 2021 12:06:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/CMSIS-DAP-vs-JTAG/m-p/1303128#M8354</guid>
      <dc:creator>TrinathK</dc:creator>
      <dc:date>2021-07-06T12:06:23Z</dc:date>
    </item>
    <item>
      <title>Re: CMSIS-DAP vs JTAG</title>
      <link>https://community.nxp.com/t5/Layerscape/CMSIS-DAP-vs-JTAG/m-p/1303361#M8359</link>
      <description>&lt;P&gt;&amp;gt; Let me know if it is OK to use JTAG instead of CMSIS-DAP.&lt;/P&gt;
&lt;P&gt;CMSIS-DAP is an optional module - i.e. JTAG can be used for the board bring-up solely.&lt;/P&gt;</description>
      <pubDate>Tue, 06 Jul 2021 18:15:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/CMSIS-DAP-vs-JTAG/m-p/1303361#M8359</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2021-07-06T18:15:31Z</dc:date>
    </item>
  </channel>
</rss>