<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 Re: NFS Mount Uboot environment for LS1043ardb</title>
    <link>https://community.nxp.com/t5/Layerscape/NFS-Mount-Uboot-environment-for-LS1043ardb/m-p/479908#M829</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;SPAN class="jive-username-link jiveTT-hover-user"&gt;Michelle Fleischer,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="jive-username-link jiveTT-hover-user"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="jive-username-link jiveTT-hover-user"&gt;Please configure the following u-boot parameters according to your real environment.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;=&amp;gt;setenv bootargs root=/dev/nfs rw nfsroot=&amp;lt;tftp_serverip&amp;gt;:&amp;lt;nfs_root_path&amp;gt; ip=&amp;lt;board_ipaddr&amp;gt;:&amp;lt;tftp_serverip&amp;gt;:&amp;lt;your_gatewayip&amp;gt;:&amp;lt;your_netmask&amp;gt;:&amp;lt;board_name&amp;gt;:&amp;lt;ethx&amp;gt;:off console=ttyS0,115200&lt;/P&gt;&lt;P&gt;=&amp;gt;saveenv&lt;/P&gt;&lt;P&gt;&lt;SPAN class="jive-username-link jiveTT-hover-user"&gt;&amp;lt;ethx&amp;gt; is the port connected on the Linux boot network.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;=&amp;gt;tftp a0000000 kernel.itb;&lt;/P&gt;&lt;P&gt;=&amp;gt;bootm a0000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note:&lt;/P&gt;&lt;P&gt;a. On the Linux host NFS server, add the following line in the file /etc/exports:&lt;/P&gt;&lt;P&gt;nfs_root_path board_ipaddress(rw,no_root_squash,async)&lt;/P&gt;&lt;P&gt;b. Restart the NFS service:&lt;/P&gt;&lt;P&gt;/etc/init.d/portmap restart&lt;/P&gt;&lt;P&gt;/etc/init.d/nfs-kernel-server restart&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yiping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 May 2016 10:55:27 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2016-05-03T10:55:27Z</dc:date>
    <item>
      <title>NFS Mount Uboot environment for LS1043ardb</title>
      <link>https://community.nxp.com/t5/Layerscape/NFS-Mount-Uboot-environment-for-LS1043ardb/m-p/479907#M828</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Has anyone tested NFS mount for filesystem using our SDK 0.5 for LS1043ardb?&amp;nbsp; If this did work, please share the u-boot environment for settings of the SECs and the kernel boot args (a print of uboot environment would be great!)...&amp;nbsp; Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Apr 2016 12:10:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/NFS-Mount-Uboot-environment-for-LS1043ardb/m-p/479907#M828</guid>
      <dc:creator>michelle</dc:creator>
      <dc:date>2016-04-26T12:10:53Z</dc:date>
    </item>
    <item>
      <title>Re: NFS Mount Uboot environment for LS1043ardb</title>
      <link>https://community.nxp.com/t5/Layerscape/NFS-Mount-Uboot-environment-for-LS1043ardb/m-p/479908#M829</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;SPAN class="jive-username-link jiveTT-hover-user"&gt;Michelle Fleischer,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="jive-username-link jiveTT-hover-user"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="jive-username-link jiveTT-hover-user"&gt;Please configure the following u-boot parameters according to your real environment.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;=&amp;gt;setenv bootargs root=/dev/nfs rw nfsroot=&amp;lt;tftp_serverip&amp;gt;:&amp;lt;nfs_root_path&amp;gt; ip=&amp;lt;board_ipaddr&amp;gt;:&amp;lt;tftp_serverip&amp;gt;:&amp;lt;your_gatewayip&amp;gt;:&amp;lt;your_netmask&amp;gt;:&amp;lt;board_name&amp;gt;:&amp;lt;ethx&amp;gt;:off console=ttyS0,115200&lt;/P&gt;&lt;P&gt;=&amp;gt;saveenv&lt;/P&gt;&lt;P&gt;&lt;SPAN class="jive-username-link jiveTT-hover-user"&gt;&amp;lt;ethx&amp;gt; is the port connected on the Linux boot network.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;=&amp;gt;tftp a0000000 kernel.itb;&lt;/P&gt;&lt;P&gt;=&amp;gt;bootm a0000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note:&lt;/P&gt;&lt;P&gt;a. On the Linux host NFS server, add the following line in the file /etc/exports:&lt;/P&gt;&lt;P&gt;nfs_root_path board_ipaddress(rw,no_root_squash,async)&lt;/P&gt;&lt;P&gt;b. Restart the NFS service:&lt;/P&gt;&lt;P&gt;/etc/init.d/portmap restart&lt;/P&gt;&lt;P&gt;/etc/init.d/nfs-kernel-server restart&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yiping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 May 2016 10:55:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/NFS-Mount-Uboot-environment-for-LS1043ardb/m-p/479908#M829</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2016-05-03T10:55:27Z</dc:date>
    </item>
    <item>
      <title>Re: NFS Mount Uboot environment for LS1043ardb</title>
      <link>https://community.nxp.com/t5/Layerscape/NFS-Mount-Uboot-environment-for-LS1043ardb/m-p/479909#M830</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;=&amp;gt; printenv&lt;BR /&gt;baudrate=115200&lt;BR /&gt;bootargs=root=/dev/nfs rw nfsroot=192.168.1.2:/home/bsanders/rootfs ip=192.168.1.3:192.168.1.2:192.168.1.2:255.255.255.0::eth0:off earlycon=uart8250,0x21c0500,115200 console=ttyS0,115200 rootdelay=5&lt;BR /&gt;bootcmd=cp.b $kernel_start $kernel_load $kernel_size &amp;amp;&amp;amp; bootm $kernel_load&lt;BR /&gt;bootdelay=10&lt;BR /&gt;console=ttyAMA0,38400n8&lt;BR /&gt;eth1addr=00:04:9F:04:03:0E&lt;BR /&gt;eth2addr=00:04:9F:04:03:0F&lt;BR /&gt;eth3addr=00:04:9F:04:03:10&lt;BR /&gt;eth4addr=00:04:9F:04:03:11&lt;BR /&gt;eth5addr=00:04:9F:04:03:12&lt;BR /&gt;eth6addr=00:04:9F:04:03:13&lt;BR /&gt;ethact=FM1@DTSEC1&lt;BR /&gt;ethaddr=00:04:9F:04:03:0D&lt;BR /&gt;ethprime=FM1@DTSEC1&lt;BR /&gt;fdt_high=0xffffffffffffffff&lt;BR /&gt;fman_ucode=60300000&lt;BR /&gt;hwconfig=fsl_ddr:bank_intlv=auto&lt;BR /&gt;initrd_high=0xffffffffffffffff&lt;BR /&gt;ipaddr=192.168.1.3&lt;BR /&gt;kernel_addr=0x100000&lt;BR /&gt;kernel_load=0x807f0000&lt;BR /&gt;kernel_size=0x1000000&lt;BR /&gt;kernel_start=0x61200000&lt;BR /&gt;loadaddr=0x80100000&lt;BR /&gt;ramdisk_addr=0x800000&lt;BR /&gt;ramdisk_size=0x2000000&lt;BR /&gt;serverip=192.168.1.2&lt;BR /&gt;stderr=serial&lt;BR /&gt;stdin=serial&lt;BR /&gt;stdout=serial&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Nov 2016 14:56:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/NFS-Mount-Uboot-environment-for-LS1043ardb/m-p/479909#M830</guid>
      <dc:creator>williamwatts</dc:creator>
      <dc:date>2016-11-11T14:56:23Z</dc:date>
    </item>
  </channel>
</rss>