<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LX2160: Adding new flash device to Code warrior flash programmer in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LX2160-Adding-new-flash-device-to-Code-warrior-flash-programmer/m-p/1297060#M8269</link>
    <description>&lt;P&gt;You wrote:&lt;/P&gt;
&lt;P&gt;&amp;gt; Is that possible to add MX66UM1G45G similar way?&lt;/P&gt;
&lt;P&gt;Yes.&lt;/P&gt;
&lt;P&gt;&amp;gt; Can you give details on choosing the closest device file&lt;/P&gt;
&lt;P&gt;&amp;gt; which can be used to create configuration for the new device?&lt;/P&gt;
&lt;P&gt;c:\Freescale\CW4NET_v2020.06\CW_ARMv8\Config\flash\devices\MT35XU512ABA.xml&lt;/P&gt;</description>
    <pubDate>Wed, 23 Jun 2021 17:39:41 GMT</pubDate>
    <dc:creator>ufedor</dc:creator>
    <dc:date>2021-06-23T17:39:41Z</dc:date>
    <item>
      <title>LX2160: Adding new flash device to Code warrior flash programmer</title>
      <link>https://community.nxp.com/t5/Layerscape/LX2160-Adding-new-flash-device-to-Code-warrior-flash-programmer/m-p/1296982#M8268</link>
      <description>&lt;P&gt;Does CW flash programmer support&amp;nbsp;MX66UM1G45G flash device?&lt;/P&gt;&lt;P&gt;&amp;nbsp;I tried using the default flash device MT35XU512ABA supported for the Lx2160A RDB.&amp;nbsp; I was able to program once. But it does not work after programming it second time.&lt;/P&gt;&lt;P&gt;I referred the documentation to add a new flash device.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Layerscape-Knowledge-Base/LX2160ARDB-How-to-configure-a-new-flash-device-for-a-Layerscape/ta-p/1101353" target="_blank"&gt;https://community.nxp.com/t5/Layerscape-Knowledge-Base/LX2160ARDB-How-to-configure-a-new-flash-device-for-a-Layerscape/ta-p/1101353&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is that possible to add&amp;nbsp;MX66UM1G45G&amp;nbsp; similar way?&amp;nbsp; Can you give details on choosing the closest device file which can be used to create configuration for the new device?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Wed, 23 Jun 2021 14:36:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LX2160-Adding-new-flash-device-to-Code-warrior-flash-programmer/m-p/1296982#M8268</guid>
      <dc:creator>rams</dc:creator>
      <dc:date>2021-06-23T14:36:10Z</dc:date>
    </item>
    <item>
      <title>Re: LX2160: Adding new flash device to Code warrior flash programmer</title>
      <link>https://community.nxp.com/t5/Layerscape/LX2160-Adding-new-flash-device-to-Code-warrior-flash-programmer/m-p/1297060#M8269</link>
      <description>&lt;P&gt;You wrote:&lt;/P&gt;
&lt;P&gt;&amp;gt; Is that possible to add MX66UM1G45G similar way?&lt;/P&gt;
&lt;P&gt;Yes.&lt;/P&gt;
&lt;P&gt;&amp;gt; Can you give details on choosing the closest device file&lt;/P&gt;
&lt;P&gt;&amp;gt; which can be used to create configuration for the new device?&lt;/P&gt;
&lt;P&gt;c:\Freescale\CW4NET_v2020.06\CW_ARMv8\Config\flash\devices\MT35XU512ABA.xml&lt;/P&gt;</description>
      <pubDate>Wed, 23 Jun 2021 17:39:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LX2160-Adding-new-flash-device-to-Code-warrior-flash-programmer/m-p/1297060#M8269</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2021-06-23T17:39:41Z</dc:date>
    </item>
  </channel>
</rss>