<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックLS1012 failed to flash QSPI NAND</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1012-failed-to-flash-QSPI-NAND/m-p/1294201#M8229</link>
    <description>&lt;P&gt;We are developing a custom board with LS1012. When we connect it to the CW TAP the diagnose runs fine and no error is found. However, we fail to flash the QSPI NAND.&lt;/P&gt;&lt;P&gt;I've tried, through the gdb terminal, to unprotect, erase and write the whole memory. The first two steps worked fine, but only 2,112 bytes could be writen. Our Nand has a page size of 2,176 bytes, but the qspi nand on the ls1012afrwy kit, which we did use as reference, has 2,112 bytes of page size.&lt;/P&gt;&lt;P&gt;The QSPI nand from the Freeway board is W25N01GW.&lt;/P&gt;&lt;P&gt;Our is MT29F1G01ABBFDSF.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="LuisSchabarum_0-1623942885996.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/147362i4CAD7E70CBFE7EEA/image-size/medium?v=v2&amp;amp;px=400" role="button" title="LuisSchabarum_0-1623942885996.png" alt="LuisSchabarum_0-1623942885996.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;LuisSchabarum_0-1623942885996.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I've copied the Target Initialization File from the Freeway kit and changed the nand qspi to our.&lt;/P&gt;&lt;P&gt;I'm also using the hard-coded rcw.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 17 Jun 2021 15:24:37 GMT</pubDate>
    <dc:creator>LuisSchabarum</dc:creator>
    <dc:date>2021-06-17T15:24:37Z</dc:date>
    <item>
      <title>LS1012 failed to flash QSPI NAND</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1012-failed-to-flash-QSPI-NAND/m-p/1294201#M8229</link>
      <description>&lt;P&gt;We are developing a custom board with LS1012. When we connect it to the CW TAP the diagnose runs fine and no error is found. However, we fail to flash the QSPI NAND.&lt;/P&gt;&lt;P&gt;I've tried, through the gdb terminal, to unprotect, erase and write the whole memory. The first two steps worked fine, but only 2,112 bytes could be writen. Our Nand has a page size of 2,176 bytes, but the qspi nand on the ls1012afrwy kit, which we did use as reference, has 2,112 bytes of page size.&lt;/P&gt;&lt;P&gt;The QSPI nand from the Freeway board is W25N01GW.&lt;/P&gt;&lt;P&gt;Our is MT29F1G01ABBFDSF.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="LuisSchabarum_0-1623942885996.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/147362i4CAD7E70CBFE7EEA/image-size/medium?v=v2&amp;amp;px=400" role="button" title="LuisSchabarum_0-1623942885996.png" alt="LuisSchabarum_0-1623942885996.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;LuisSchabarum_0-1623942885996.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I've copied the Target Initialization File from the Freeway kit and changed the nand qspi to our.&lt;/P&gt;&lt;P&gt;I'm also using the hard-coded rcw.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 17 Jun 2021 15:24:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1012-failed-to-flash-QSPI-NAND/m-p/1294201#M8229</guid>
      <dc:creator>LuisSchabarum</dc:creator>
      <dc:date>2021-06-17T15:24:37Z</dc:date>
    </item>
    <item>
      <title>Re: LS1012 failed to flash QSPI NAND</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1012-failed-to-flash-QSPI-NAND/m-p/1298139#M8289</link>
      <description>&lt;P&gt;Test NAND on your board using CodeWarrior wizrad for simple program example creation. Is there problem for this NAND Flash reading? See Flash configuration in the LS1012A_FRWY_init.py using the following path: C:\Freescale\CW4NET_v2020.06\CW_ARMv8\Config\boards&lt;/P&gt;</description>
      <pubDate>Fri, 25 Jun 2021 06:07:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1012-failed-to-flash-QSPI-NAND/m-p/1298139#M8289</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2021-06-25T06:07:58Z</dc:date>
    </item>
  </channel>
</rss>