<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LX2160ARDB 25Gb compatible issue in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LX2160ARDB-25Gb-compatible-issue/m-p/1293881#M8222</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Correct. It was in the DPC file. If you don't make the changes, the MC firmware will overwrite anything you do.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;LX2 RDB has QSFP+ cage to support 40G XLAUI. I have seen a 40G breakout into x4 10G SFP+.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Each lane operates at 10.3125Gbps.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;for 100G, this is x4 25G-AUI. If a QSFP28 is used, then the Inphi in the path may need reprograming if it can support the 25G-AUI lanes. &lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 17 Jun 2021 07:37:40 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2021-06-17T07:37:40Z</dc:date>
    <item>
      <title>LX2160ARDB 25Gb compatible issue</title>
      <link>https://community.nxp.com/t5/Layerscape/LX2160ARDB-25Gb-compatible-issue/m-p/1289570#M8180</link>
      <description>&lt;P&gt;Hi, All:&lt;/P&gt;&lt;P&gt;I met one problem about 25Gb connection problem, I tried to use "&lt;SPAN&gt;Cisco QSFP-4SFP25G-CU3M Compatible 100G QSFP28 to 4x25G SFP28 Passive Direct Attach Copper Breakout Cable" or similar cable and connect to one 25Gb SFP28 and one 100Gb QSFP.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;And then using 25Gb SFP28 on LX2160ARDB, and another side is 100Gb QSFP and configured it as 25Gb.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;But they showed no link and seems no Link up showed on both devices respectively.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;By the way, another side is &amp;nbsp;a general server , and ever used in other device with same scenario but no problem on that.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Does everyone have same problem on LX2160ARDB?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The module I used is FS QSFP28-SR4-100G and Mellanox MMA2P00 SFP28.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Howard.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jun 2021 03:58:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LX2160ARDB-25Gb-compatible-issue/m-p/1289570#M8180</guid>
      <dc:creator>howardlu1</dc:creator>
      <dc:date>2021-06-09T03:58:35Z</dc:date>
    </item>
    <item>
      <title>Re: LX2160ARDB 25Gb compatible issue</title>
      <link>https://community.nxp.com/t5/Layerscape/LX2160ARDB-25Gb-compatible-issue/m-p/1290994#M8197</link>
      <description>&lt;P&gt;&lt;SPAN&gt;The only thing I can suggest now is to see if RS-FEC enabled makes any&amp;nbsp; difference if it is not enabled already.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Obtaining 100G breakout cable to try will take some time. Would have to order and then try in the lab.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Has been over a year since I have been in the lab. So finding the equipment to test might be another hurdle.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 11 Jun 2021 02:14:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LX2160ARDB-25Gb-compatible-issue/m-p/1290994#M8197</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2021-06-11T02:14:50Z</dc:date>
    </item>
    <item>
      <title>Re: LX2160ARDB 25Gb compatible issue</title>
      <link>https://community.nxp.com/t5/Layerscape/LX2160ARDB-25Gb-compatible-issue/m-p/1291090#M8198</link>
      <description>&lt;P&gt;Hi, Yiping:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks a lot, and I saw RS-FEC could be enabled by MC-BIN only, and we cannot enable/disable it by general MC-BIN version, isn't it?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Howard.&lt;/P&gt;</description>
      <pubDate>Fri, 11 Jun 2021 05:30:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LX2160ARDB-25Gb-compatible-issue/m-p/1291090#M8198</guid>
      <dc:creator>howardlu1</dc:creator>
      <dc:date>2021-06-11T05:30:15Z</dc:date>
    </item>
    <item>
      <title>Re: LX2160ARDB 25Gb compatible issue</title>
      <link>https://community.nxp.com/t5/Layerscape/LX2160ARDB-25Gb-compatible-issue/m-p/1293881#M8222</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Correct. It was in the DPC file. If you don't make the changes, the MC firmware will overwrite anything you do.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;LX2 RDB has QSFP+ cage to support 40G XLAUI. I have seen a 40G breakout into x4 10G SFP+.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Each lane operates at 10.3125Gbps.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;for 100G, this is x4 25G-AUI. If a QSFP28 is used, then the Inphi in the path may need reprograming if it can support the 25G-AUI lanes. &lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 17 Jun 2021 07:37:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LX2160ARDB-25Gb-compatible-issue/m-p/1293881#M8222</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2021-06-17T07:37:40Z</dc:date>
    </item>
  </channel>
</rss>