<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LS1012ARDB Murata wifi SN8000 load module failed in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1012ARDB-Murata-wifi-SN8000-load-module-failed/m-p/1291712#M8205</link>
    <description>&lt;P&gt;Hello Experts,&lt;/P&gt;&lt;P&gt;I have LS1012ARDB board with&amp;nbsp;ls1012ardb_ask_8.0.0-B1 installed on it.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have problem while loading murata wifi driver, mostly it will fail to load the driver, and I need to reboot the board and try to load the driver module again until success. Here is the error message&lt;/P&gt;&lt;PRE&gt;# insmod /lib/modules/4.9.73/bcmdhd.ko nvram_path=/lib/firmware/bcmdhd.SN8000.SDIO.cal firmware_path=/lib/firmware/fw_bcmdhd.bin&lt;BR /&gt;&lt;BR /&gt;[ 81.770295] dhd_module_init in&lt;BR /&gt;[ 81.777679] CFG80211-ERROR) wl_netlink_init : [ 81.785579] nl_sk is not ready&lt;BR /&gt;[ 81.788639] Power-up adapter 'DHD generic adapter'&lt;BR /&gt;[ 81.801767] wifi_platform_bus_enumerate device present 1&lt;BR /&gt;[ 81.838011] dhdsdio_probe_attach: si_attach failed!&lt;BR /&gt;[ 81.845556] dhdsdio_probe: dhdsdio_probe_attach failed&lt;BR /&gt;[ 81.857657] bcmsdh_sdmmc: probe of mmc0:0001:2 failed with error -12&lt;BR /&gt;[ 94.028214] dhd_wifi_platform_load_sdio: sdio_register_driver timeout or error&lt;BR /&gt;[ 94.040568] wifi_platform_bus_enumerate device present 0&lt;BR /&gt;[ 94.052242] bcmdhd_wlan: probe of bcmdhd_wlan@0 failed with error -62&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;BR /&gt;I also attach boot message.&lt;/P&gt;&lt;P&gt;What make the driver installation failed?&lt;BR /&gt;What should I do to prevent this happening?&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;&lt;BR /&gt;Huda&lt;/P&gt;</description>
    <pubDate>Mon, 14 Jun 2021 04:07:23 GMT</pubDate>
    <dc:creator>miftahul_huda</dc:creator>
    <dc:date>2021-06-14T04:07:23Z</dc:date>
    <item>
      <title>LS1012ARDB Murata wifi SN8000 load module failed</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1012ARDB-Murata-wifi-SN8000-load-module-failed/m-p/1291712#M8205</link>
      <description>&lt;P&gt;Hello Experts,&lt;/P&gt;&lt;P&gt;I have LS1012ARDB board with&amp;nbsp;ls1012ardb_ask_8.0.0-B1 installed on it.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have problem while loading murata wifi driver, mostly it will fail to load the driver, and I need to reboot the board and try to load the driver module again until success. Here is the error message&lt;/P&gt;&lt;PRE&gt;# insmod /lib/modules/4.9.73/bcmdhd.ko nvram_path=/lib/firmware/bcmdhd.SN8000.SDIO.cal firmware_path=/lib/firmware/fw_bcmdhd.bin&lt;BR /&gt;&lt;BR /&gt;[ 81.770295] dhd_module_init in&lt;BR /&gt;[ 81.777679] CFG80211-ERROR) wl_netlink_init : [ 81.785579] nl_sk is not ready&lt;BR /&gt;[ 81.788639] Power-up adapter 'DHD generic adapter'&lt;BR /&gt;[ 81.801767] wifi_platform_bus_enumerate device present 1&lt;BR /&gt;[ 81.838011] dhdsdio_probe_attach: si_attach failed!&lt;BR /&gt;[ 81.845556] dhdsdio_probe: dhdsdio_probe_attach failed&lt;BR /&gt;[ 81.857657] bcmsdh_sdmmc: probe of mmc0:0001:2 failed with error -12&lt;BR /&gt;[ 94.028214] dhd_wifi_platform_load_sdio: sdio_register_driver timeout or error&lt;BR /&gt;[ 94.040568] wifi_platform_bus_enumerate device present 0&lt;BR /&gt;[ 94.052242] bcmdhd_wlan: probe of bcmdhd_wlan@0 failed with error -62&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;BR /&gt;I also attach boot message.&lt;/P&gt;&lt;P&gt;What make the driver installation failed?&lt;BR /&gt;What should I do to prevent this happening?&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;&lt;BR /&gt;Huda&lt;/P&gt;</description>
      <pubDate>Mon, 14 Jun 2021 04:07:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1012ARDB-Murata-wifi-SN8000-load-module-failed/m-p/1291712#M8205</guid>
      <dc:creator>miftahul_huda</dc:creator>
      <dc:date>2021-06-14T04:07:23Z</dc:date>
    </item>
    <item>
      <title>Re: LS1012ARDB Murata wifi SN8000 load module failed</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1012ARDB-Murata-wifi-SN8000-load-module-failed/m-p/1296753#M8261</link>
      <description>&lt;P&gt;Please refer to the following threads.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/SD2-card-slot-is-not-working-for-WiFi/m-p/232016" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/SD2-card-slot-is-not-working-for-WiFi/m-p/232016&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/murata-wifi-on-imx6ul/m-p/835744?commentID=1065713" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/murata-wifi-on-imx6ul/m-p/835744?commentID=1065713&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 23 Jun 2021 09:25:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1012ARDB-Murata-wifi-SN8000-load-module-failed/m-p/1296753#M8261</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2021-06-23T09:25:38Z</dc:date>
    </item>
    <item>
      <title>Re: LS1012ARDB Murata wifi SN8000 load module failed</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1012ARDB-Murata-wifi-SN8000-load-module-failed/m-p/1298836#M8305</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/52411" target="_self"&gt;&lt;SPAN class=""&gt;yipingwang&amp;nbsp;&lt;/SPAN&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;From this thread&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/SD2-card-slot-is-not-working-for-WiFi/m-p/232016" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/i-MX-Processors/SD2-card-slot-is-not-working-for-WiFi/m-p/232016&lt;/A&gt;&lt;/P&gt;&lt;PRE&gt;&lt;SPAN&gt;From log messages, It seems that mmc1 didn't find new attached device(wifi) at the beginning, So could you try to power up wifi in BSP file ? At first, we should ensure mmc controller can find wifi&lt;/SPAN&gt;&lt;/PRE&gt;&lt;P&gt;&lt;SPAN&gt;I am not clear about "BSP file", where could I find it? Is it accessible in OpenWRT? Since I only have the board LS1012ARDB, prebuilt firmware&amp;nbsp;ls1012ardb_ask_bhr_8.0.0-B1, and OpenWRT 18.06 to build package that compatible for&amp;nbsp;firmware&amp;nbsp;ls1012ardb_ask_bhr_8.0.0-B1. If it not, what should I do to obtain it?&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;&lt;BR /&gt;Huda&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 28 Jun 2021 04:49:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1012ARDB-Murata-wifi-SN8000-load-module-failed/m-p/1298836#M8305</guid>
      <dc:creator>miftahul_huda</dc:creator>
      <dc:date>2021-06-28T04:49:14Z</dc:date>
    </item>
    <item>
      <title>Re: LS1012ARDB Murata wifi SN8000 load module failed</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1012ARDB-Murata-wifi-SN8000-load-module-failed/m-p/1301497#M8339</link>
      <description>&lt;P&gt;Please refer to the following Openwrt&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/qoriq/qoriq-components/openwrt/" target="_blank"&gt;https://source.codeaurora.org/external/qoriq/qoriq-components/openwrt/&lt;/A&gt; &lt;BR /&gt;tag: layerscape-20.09&lt;/P&gt;</description>
      <pubDate>Fri, 02 Jul 2021 04:05:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1012ARDB-Murata-wifi-SN8000-load-module-failed/m-p/1301497#M8339</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2021-07-02T04:05:16Z</dc:date>
    </item>
  </channel>
</rss>