<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: L3 layer encrypted packets drop in dpdk in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/L3-layer-encrypted-packets-drop-in-dpdk/m-p/1287416#M8150</link>
    <description>&lt;P&gt;&lt;SPAN&gt;There are two methods for received L4 checksum error packet from Fman ports,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;1. Disable Fman L3/L4 checksum. Unset "DEV_RX_OFFLOAD_CHECKSUM" of "port_conf.rxmode.offloads" to disable L3/L4 checksum for Fman when compile l3fwd application.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;&lt;SPAN&gt;2. Receive the checksum error packets to error FQ with the attached patch.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 04 Jun 2021 09:18:19 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2021-06-04T09:18:19Z</dc:date>
    <item>
      <title>L3 layer encrypted packets drop in dpdk</title>
      <link>https://community.nxp.com/t5/Layerscape/L3-layer-encrypted-packets-drop-in-dpdk/m-p/1284043#M8106</link>
      <description>&lt;P&gt;I am using dpdk for encrypting IP Packet (IP payload) in L1046ardb Kit. At the receive side , the dpaa driver is dropping the encrypted packet (Not sure whether due to length corruption or checksum corruption as both are encrypted).&lt;/P&gt;&lt;P&gt;How do i disable dpaa not to drop any packets??&lt;/P&gt;&lt;P&gt;I tried the solution mentioned in this thread&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Layerscape/checksum-disabling-in-dpaa-driver-in-dpdk/m-p/1283323#M8096" target="_blank"&gt;https://community.nxp.com/t5/Layerscape/checksum-disabling-in-dpaa-driver-in-dpdk/m-p/1283323#M8096&lt;/A&gt;&lt;/P&gt;&lt;P&gt;but am still not able to receive the packet at the application layer.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 28 May 2021 08:56:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/L3-layer-encrypted-packets-drop-in-dpdk/m-p/1284043#M8106</guid>
      <dc:creator>rashmikj</dc:creator>
      <dc:date>2021-05-28T08:56:04Z</dc:date>
    </item>
    <item>
      <title>Re: L3 layer encrypted packets drop in dpdk</title>
      <link>https://community.nxp.com/t5/Layerscape/L3-layer-encrypted-packets-drop-in-dpdk/m-p/1287416#M8150</link>
      <description>&lt;P&gt;&lt;SPAN&gt;There are two methods for received L4 checksum error packet from Fman ports,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;1. Disable Fman L3/L4 checksum. Unset "DEV_RX_OFFLOAD_CHECKSUM" of "port_conf.rxmode.offloads" to disable L3/L4 checksum for Fman when compile l3fwd application.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;&lt;SPAN&gt;2. Receive the checksum error packets to error FQ with the attached patch.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 04 Jun 2021 09:18:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/L3-layer-encrypted-packets-drop-in-dpdk/m-p/1287416#M8150</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2021-06-04T09:18:19Z</dc:date>
    </item>
  </channel>
</rss>