<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 Re: modfiy RCW in LSDK2012</title>
    <link>https://community.nxp.com/t5/Layerscape/modfiy-RCW-in-LSDK2012/m-p/1286792#M8139</link>
    <description>&lt;P&gt;Use the following command sequence:&lt;/P&gt;
&lt;OL&gt;
&lt;LI&gt;Change RCW in .cfg file in u-boot source folder. Use the following path:&lt;/LI&gt;
&lt;/OL&gt;
&lt;P&gt;/flexbuild_lsdk2012/packages/firmware/u-boot/board/freescale/ls1021atwr&lt;/P&gt;
&lt;OL start="2"&gt;
&lt;LI&gt;use the command "flex-builder -c uboot -m ls1021atwr -b sd" to generate new uboot image uboot_ls1021atwr_sdcard_ifc.bin&lt;/LI&gt;
&lt;/OL&gt;
&lt;P&gt;This file available using the following path: /flexbuild_lsdk2012/build/firmware/u-boot/ls1021atwr&lt;/P&gt;</description>
    <pubDate>Thu, 03 Jun 2021 11:39:14 GMT</pubDate>
    <dc:creator>Pavel</dc:creator>
    <dc:date>2021-06-03T11:39:14Z</dc:date>
    <item>
      <title>modfiy RCW in LSDK2012</title>
      <link>https://community.nxp.com/t5/Layerscape/modfiy-RCW-in-LSDK2012/m-p/1286651#M8135</link>
      <description>&lt;P&gt;Hi Everyone. I hope to modify the RCW setting in LSDK2012,but it is failure, I do following steps according the user guide:&lt;/P&gt;&lt;P&gt;1.modify the setting packages/firmware/rcw/ls1021atwr/SSR_PNS_30/rcw_1200_sdboot.rcw, the CGA_PLL1_RAT old item is 12, I change it as 10&lt;/P&gt;&lt;P&gt;2. use the command flex-builder -c rcw -m ls1021atwr -b sd to generate new rcw_1200_sboot.bin&lt;/P&gt;&lt;P&gt;3.use the command flex-builder -c uboot -m ls1021atwr -b sd to generate new uboot image uboot_ls1021atwr_sdcard_ifc.bin&amp;nbsp; but the RCW bits in uboot is still as before.(from the manifest file&lt;/P&gt;&lt;P&gt;I can assure such file : uboot_sdboot=$FBOUTDIR/firmware/u-boot/ls1021atwr/uboot_ls1021atwr_sdcard_ifc.bin)&lt;/P&gt;&lt;P&gt;for the new rcw_1200_sdboot.bin the first 24 bit is AA 55 AA 55 01 EE 01 00 06 08 00 0A&lt;/P&gt;&lt;P&gt;the old rcw_1200_sdboot.bin the first 24 bit is &amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp; AA 55 AA 55 01 EE 01 00 06 08 00 0C&lt;/P&gt;&lt;P&gt;so the RCW binary file had been modified sucessfully.&lt;/P&gt;&lt;P&gt;but the first 24bit in uboot_ls1021atwr_sdcard_ifc.bin is same as old rcw file&lt;/P&gt;&lt;P&gt;why ?&amp;nbsp; Is there any wrong operation ?please give suggestion about it. Thank you!&lt;/P&gt;</description>
      <pubDate>Thu, 03 Jun 2021 08:25:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/modfiy-RCW-in-LSDK2012/m-p/1286651#M8135</guid>
      <dc:creator>niexuzhong</dc:creator>
      <dc:date>2021-06-03T08:25:31Z</dc:date>
    </item>
    <item>
      <title>Re: modfiy RCW in LSDK2012</title>
      <link>https://community.nxp.com/t5/Layerscape/modfiy-RCW-in-LSDK2012/m-p/1286792#M8139</link>
      <description>&lt;P&gt;Use the following command sequence:&lt;/P&gt;
&lt;OL&gt;
&lt;LI&gt;Change RCW in .cfg file in u-boot source folder. Use the following path:&lt;/LI&gt;
&lt;/OL&gt;
&lt;P&gt;/flexbuild_lsdk2012/packages/firmware/u-boot/board/freescale/ls1021atwr&lt;/P&gt;
&lt;OL start="2"&gt;
&lt;LI&gt;use the command "flex-builder -c uboot -m ls1021atwr -b sd" to generate new uboot image uboot_ls1021atwr_sdcard_ifc.bin&lt;/LI&gt;
&lt;/OL&gt;
&lt;P&gt;This file available using the following path: /flexbuild_lsdk2012/build/firmware/u-boot/ls1021atwr&lt;/P&gt;</description>
      <pubDate>Thu, 03 Jun 2021 11:39:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/modfiy-RCW-in-LSDK2012/m-p/1286792#M8139</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2021-06-03T11:39:14Z</dc:date>
    </item>
  </channel>
</rss>