<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックLS1043A DDR3L Address Routing</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1043A-DDR3L-Address-Routing/m-p/1286775#M8138</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are currently designing LS1043A board with DDR3L 32+4bit interface. I have a question at that point about address matching for fly by topology. AN3940 states as follows;&lt;BR /&gt;"• Tune signals to +/-10 mils of the clock at each device"&lt;/P&gt;&lt;P&gt;What does it mean? There are two options about it.&lt;/P&gt;&lt;P&gt;------------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Board Design Address Routing;&lt;/P&gt;&lt;P&gt;LS1043A ----- L1 ----- |DDR3L1| ----- L2 ----- |DDR3L2| ----- L3 ----- |DDR3L3| ---- Termination&lt;/P&gt;&lt;P&gt;------------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;1. Option&lt;/P&gt;&lt;P&gt;L1 = +/-10mil match between address-clock&lt;BR /&gt;L2 = +/-10mil match between address-clock&lt;BR /&gt;L3 = +/-10mil match between address-clock&lt;/P&gt;&lt;P&gt;DDR3L1 will have 10mils tolerance in worst case.&lt;BR /&gt;DDR3L2 will have 20mils tolerance in worst case.&lt;BR /&gt;DDR3L3 will have 30mils tolerance in worst case.&lt;/P&gt;&lt;P&gt;------------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;2. Option&lt;BR /&gt;L1&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;= +/-10mil match between address-clock&lt;BR /&gt;L1+L2&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;= +/-10mil match between address-clock&lt;BR /&gt;L1+L2+L3 = +/-10mil match between address-clock&lt;/P&gt;&lt;P&gt;DDR3L1 will have 10mils tolerance in worst case.&lt;BR /&gt;DDR3L2 will have 10mils tolerance in worst case.&lt;BR /&gt;DDR3L3 will have 10mils tolerance in worst case.&lt;/P&gt;&lt;P&gt;------------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Which options is mentioned by AN3940? If the second option is mentioned, it is a bit strict for maximum 1600Mbit/s (for LS1043A) interface.&lt;/P&gt;&lt;P&gt;Have a nice day&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 03 Jun 2021 12:11:04 GMT</pubDate>
    <dc:creator>serkanOz</dc:creator>
    <dc:date>2021-06-03T12:11:04Z</dc:date>
    <item>
      <title>LS1043A DDR3L Address Routing</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-DDR3L-Address-Routing/m-p/1286775#M8138</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are currently designing LS1043A board with DDR3L 32+4bit interface. I have a question at that point about address matching for fly by topology. AN3940 states as follows;&lt;BR /&gt;"• Tune signals to +/-10 mils of the clock at each device"&lt;/P&gt;&lt;P&gt;What does it mean? There are two options about it.&lt;/P&gt;&lt;P&gt;------------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Board Design Address Routing;&lt;/P&gt;&lt;P&gt;LS1043A ----- L1 ----- |DDR3L1| ----- L2 ----- |DDR3L2| ----- L3 ----- |DDR3L3| ---- Termination&lt;/P&gt;&lt;P&gt;------------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;1. Option&lt;/P&gt;&lt;P&gt;L1 = +/-10mil match between address-clock&lt;BR /&gt;L2 = +/-10mil match between address-clock&lt;BR /&gt;L3 = +/-10mil match between address-clock&lt;/P&gt;&lt;P&gt;DDR3L1 will have 10mils tolerance in worst case.&lt;BR /&gt;DDR3L2 will have 20mils tolerance in worst case.&lt;BR /&gt;DDR3L3 will have 30mils tolerance in worst case.&lt;/P&gt;&lt;P&gt;------------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;2. Option&lt;BR /&gt;L1&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;= +/-10mil match between address-clock&lt;BR /&gt;L1+L2&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;= +/-10mil match between address-clock&lt;BR /&gt;L1+L2+L3 = +/-10mil match between address-clock&lt;/P&gt;&lt;P&gt;DDR3L1 will have 10mils tolerance in worst case.&lt;BR /&gt;DDR3L2 will have 10mils tolerance in worst case.&lt;BR /&gt;DDR3L3 will have 10mils tolerance in worst case.&lt;/P&gt;&lt;P&gt;------------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Which options is mentioned by AN3940? If the second option is mentioned, it is a bit strict for maximum 1600Mbit/s (for LS1043A) interface.&lt;/P&gt;&lt;P&gt;Have a nice day&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 03 Jun 2021 12:11:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-DDR3L-Address-Routing/m-p/1286775#M8138</guid>
      <dc:creator>serkanOz</dc:creator>
      <dc:date>2021-06-03T12:11:04Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A DDR3L Address Routing</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-DDR3L-Address-Routing/m-p/1287430#M8151</link>
      <description>&lt;P&gt;You are right, the app note says "Tune signals to +/-10 mils of the clock at each device". This statement corresponds to option 2 in your description, regardless of device position in the fly-by chain, all address/command/control signals at the device should be +/-10 mils of the clock. This is specified for 2133MT/s speed, can be slightly relaxed for 1600MT/s, but we can not provide numeric values for this relaxing.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Bulat&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 04 Jun 2021 09:40:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-DDR3L-Address-Routing/m-p/1287430#M8151</guid>
      <dc:creator>Bulat</dc:creator>
      <dc:date>2021-06-04T09:40:48Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A DDR3L Address Routing</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-DDR3L-Address-Routing/m-p/1288233#M8160</link>
      <description>&lt;P&gt;Thanks for your explanation.&lt;/P&gt;</description>
      <pubDate>Mon, 07 Jun 2021 10:49:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-DDR3L-Address-Routing/m-p/1288233#M8160</guid>
      <dc:creator>serkanOz</dc:creator>
      <dc:date>2021-06-07T10:49:35Z</dc:date>
    </item>
  </channel>
</rss>