<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: PCIe data transfer rate</title>
    <link>https://community.nxp.com/t5/Layerscape/PCIe-data-transfer-rate/m-p/1277521#M8013</link>
    <description>&lt;P&gt;Thank you for the reply. As I understand (If I am not wrong) , you mean that the data (Packet) is transferred over the PCIe link at a rate of of 2.5 GTps or 5 or 8 GTps (based on PCIe generation).&amp;nbsp;&lt;/P&gt;&lt;P&gt;If my understanding is right, can be use cables from one backplane to other , to transfer data over PCIe at this rate. Are there any specialized cables for this purpose.&lt;/P&gt;</description>
    <pubDate>Mon, 17 May 2021 09:32:30 GMT</pubDate>
    <dc:creator>SrinivasP</dc:creator>
    <dc:date>2021-05-17T09:32:30Z</dc:date>
    <item>
      <title>PCIe data transfer rate</title>
      <link>https://community.nxp.com/t5/Layerscape/PCIe-data-transfer-rate/m-p/1277360#M8007</link>
      <description>&lt;P&gt;I want to get clarified on PCIe transfer rate (or Baud rate) in LS1043A I.MX8Q. As per PCIe spec and generation a specified transfer rate is mentioned (2. GTps , 5 GTps etc). Is this transfer rate fixed or can we configure any transfer rate below the maximum specified&amp;nbsp; rate.&lt;/P&gt;</description>
      <pubDate>Mon, 17 May 2021 05:22:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/PCIe-data-transfer-rate/m-p/1277360#M8007</guid>
      <dc:creator>SrinivasP</dc:creator>
      <dc:date>2021-05-17T05:22:37Z</dc:date>
    </item>
    <item>
      <title>Re: PCIe data transfer rate</title>
      <link>https://community.nxp.com/t5/Layerscape/PCIe-data-transfer-rate/m-p/1277395#M8008</link>
      <description>&lt;P&gt;&amp;gt; Is this transfer rate fixed&lt;/P&gt;
&lt;P&gt;The PCIe &lt;STRONG&gt;link rate&lt;/STRONG&gt; is fixed.&lt;/P&gt;
&lt;P&gt;Consider that data is transferred through this link in packets, so resulting &lt;STRONG&gt;data rate&lt;/STRONG&gt; can vary.&lt;/P&gt;</description>
      <pubDate>Mon, 17 May 2021 06:19:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/PCIe-data-transfer-rate/m-p/1277395#M8008</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2021-05-17T06:19:16Z</dc:date>
    </item>
    <item>
      <title>Re: PCIe data transfer rate</title>
      <link>https://community.nxp.com/t5/Layerscape/PCIe-data-transfer-rate/m-p/1277521#M8013</link>
      <description>&lt;P&gt;Thank you for the reply. As I understand (If I am not wrong) , you mean that the data (Packet) is transferred over the PCIe link at a rate of of 2.5 GTps or 5 or 8 GTps (based on PCIe generation).&amp;nbsp;&lt;/P&gt;&lt;P&gt;If my understanding is right, can be use cables from one backplane to other , to transfer data over PCIe at this rate. Are there any specialized cables for this purpose.&lt;/P&gt;</description>
      <pubDate>Mon, 17 May 2021 09:32:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/PCIe-data-transfer-rate/m-p/1277521#M8013</guid>
      <dc:creator>SrinivasP</dc:creator>
      <dc:date>2021-05-17T09:32:30Z</dc:date>
    </item>
  </channel>
</rss>