<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPUART on LS1046A in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LPUART-on-LS1046A/m-p/1271233#M7914</link>
    <description>&lt;P&gt;Sorry, it appears that my question was cut off somehow.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So I wanted to connect the LPUART interface the same way as the DUART interface as on LS1046ARDB board (RS232 transceiver and then a connector).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can this be done? I can't seem to find anything that shows how this interface is hooked up.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
    <pubDate>Mon, 03 May 2021 10:48:46 GMT</pubDate>
    <dc:creator>matthej</dc:creator>
    <dc:date>2021-05-03T10:48:46Z</dc:date>
    <item>
      <title>LPUART on LS1046A</title>
      <link>https://community.nxp.com/t5/Layerscape/LPUART-on-LS1046A/m-p/1267582#M7867</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have the LS1046ARDB eval board schematics which show the DUART connection to an RS232 xcvr and RJ45 connector.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I wanted to do the same thing for the LPUART on the LS1046A processor (connect it to the RS232 xcvr and then a connector.&lt;/P&gt;</description>
      <pubDate>Sat, 24 Apr 2021 12:03:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LPUART-on-LS1046A/m-p/1267582#M7867</guid>
      <dc:creator>matthej</dc:creator>
      <dc:date>2021-04-24T12:03:17Z</dc:date>
    </item>
    <item>
      <title>Re: LPUART on LS1046A</title>
      <link>https://community.nxp.com/t5/Layerscape/LPUART-on-LS1046A/m-p/1268520#M7887</link>
      <description>&lt;P&gt;The LS1046 LPUART is supported in LSDK 2012.&lt;/P&gt;
&lt;P&gt;See the Table 4 in LSDK 2012 User Guide:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/user-guide/LSDKUG_Rev20.12.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/user-guide/LSDKUG_Rev20.12.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Use the Section 7.2.7 in LSDK 2012 User Guide for LPUART setting on the LS1046a board.&lt;/P&gt;</description>
      <pubDate>Tue, 27 Apr 2021 04:19:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LPUART-on-LS1046A/m-p/1268520#M7887</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2021-04-27T04:19:28Z</dc:date>
    </item>
    <item>
      <title>Re: LPUART on LS1046A</title>
      <link>https://community.nxp.com/t5/Layerscape/LPUART-on-LS1046A/m-p/1271233#M7914</link>
      <description>&lt;P&gt;Sorry, it appears that my question was cut off somehow.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So I wanted to connect the LPUART interface the same way as the DUART interface as on LS1046ARDB board (RS232 transceiver and then a connector).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can this be done? I can't seem to find anything that shows how this interface is hooked up.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Mon, 03 May 2021 10:48:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LPUART-on-LS1046A/m-p/1271233#M7914</guid>
      <dc:creator>matthej</dc:creator>
      <dc:date>2021-05-03T10:48:46Z</dc:date>
    </item>
  </channel>
</rss>