<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LS1043 SFP interface on SGMII in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1043-SFP-interface-on-SGMII/m-p/1271051#M7910</link>
    <description>&lt;P&gt;&amp;gt; Can I connect the SFP directly to the SGMII.&lt;/P&gt;
&lt;P&gt;It is possible if SFP with SGMII interface is used.&lt;/P&gt;</description>
    <pubDate>Sat, 01 May 2021 06:00:58 GMT</pubDate>
    <dc:creator>ufedor</dc:creator>
    <dc:date>2021-05-01T06:00:58Z</dc:date>
    <item>
      <title>LS1043 SFP interface on SGMII</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043-SFP-interface-on-SGMII/m-p/1270977#M7909</link>
      <description>&lt;P&gt;We are having design progressing With LS1043. There are 4 Ethernet Interfaces planned , 2 Copper and 2 Fiber (SFP). Copper Ports will be Interfaced via RGMII to EC1 and EC2 . Planning to Use Serdes Lane A and Lane B as SGMII mode to connect the SFP . Can I connect the SFP directly to the SGMII. Is there any Retimers required ? Is there any timing or Electrical Compatibility issue .&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="EbyJayan88_0-1619807326128.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/143751i252497A11933299B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="EbyJayan88_0-1619807326128.png" alt="EbyJayan88_0-1619807326128.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 30 Apr 2021 18:30:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043-SFP-interface-on-SGMII/m-p/1270977#M7909</guid>
      <dc:creator>EbyJayan88</dc:creator>
      <dc:date>2021-04-30T18:30:29Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043 SFP interface on SGMII</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043-SFP-interface-on-SGMII/m-p/1271051#M7910</link>
      <description>&lt;P&gt;&amp;gt; Can I connect the SFP directly to the SGMII.&lt;/P&gt;
&lt;P&gt;It is possible if SFP with SGMII interface is used.&lt;/P&gt;</description>
      <pubDate>Sat, 01 May 2021 06:00:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043-SFP-interface-on-SGMII/m-p/1271051#M7910</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2021-05-01T06:00:58Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043 SFP interface on SGMII</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043-SFP-interface-on-SGMII/m-p/1368937#M9296</link>
      <description>&lt;P&gt;Can you share part number for SPF recommended to be used with LS1043&lt;/P&gt;</description>
      <pubDate>Wed, 10 Nov 2021 05:30:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043-SFP-interface-on-SGMII/m-p/1368937#M9296</guid>
      <dc:creator>EbyJayan88</dc:creator>
      <dc:date>2021-11-10T05:30:50Z</dc:date>
    </item>
  </channel>
</rss>