<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic TSN Frame Preemption Test on LS1028ARDB in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/TSN-Frame-Preemption-Test-on-LS1028ARDB/m-p/1268248#M7882</link>
    <description>&lt;P&gt;Hi experts,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am trying to perform the Qbu test on ENETC for the LS1028ARDB board (can be found in the OpenILUG_Rev1.10.pdf file, page 88). As I have only one LS1028ARDB board, I am testing the version where MAC0 is linked to SWP0. In fact the demo works but I still have some questions:&lt;/P&gt;&lt;P&gt;-&amp;nbsp; Does the command "qbuset --device eno0 --preemptable 0xfe" mean that traffic class #0 or the frames in queue #0 will be preempted?&lt;/P&gt;&lt;P&gt;- The port with the address 90:e2:ba:ff:ff:ff shouldn't be swp0 instead of eno0, as the traffic flows from eno0 to swp0, and the option -m of pktgen_twoqueue.sh specifies the destination MAC address?&lt;/P&gt;&lt;P&gt;- What does the value 0x111 that we have to write at the address 0x1fc100048 correspond to? And more generally, where can I find a document which gives more information about the registers&amp;nbsp;0x1fc100048 and&amp;nbsp;0x11f18 ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your help.&lt;/P&gt;</description>
    <pubDate>Mon, 26 Apr 2021 15:43:46 GMT</pubDate>
    <dc:creator>ceroone</dc:creator>
    <dc:date>2021-04-26T15:43:46Z</dc:date>
    <item>
      <title>TSN Frame Preemption Test on LS1028ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/TSN-Frame-Preemption-Test-on-LS1028ARDB/m-p/1268248#M7882</link>
      <description>&lt;P&gt;Hi experts,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am trying to perform the Qbu test on ENETC for the LS1028ARDB board (can be found in the OpenILUG_Rev1.10.pdf file, page 88). As I have only one LS1028ARDB board, I am testing the version where MAC0 is linked to SWP0. In fact the demo works but I still have some questions:&lt;/P&gt;&lt;P&gt;-&amp;nbsp; Does the command "qbuset --device eno0 --preemptable 0xfe" mean that traffic class #0 or the frames in queue #0 will be preempted?&lt;/P&gt;&lt;P&gt;- The port with the address 90:e2:ba:ff:ff:ff shouldn't be swp0 instead of eno0, as the traffic flows from eno0 to swp0, and the option -m of pktgen_twoqueue.sh specifies the destination MAC address?&lt;/P&gt;&lt;P&gt;- What does the value 0x111 that we have to write at the address 0x1fc100048 correspond to? And more generally, where can I find a document which gives more information about the registers&amp;nbsp;0x1fc100048 and&amp;nbsp;0x11f18 ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your help.&lt;/P&gt;</description>
      <pubDate>Mon, 26 Apr 2021 15:43:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/TSN-Frame-Preemption-Test-on-LS1028ARDB/m-p/1268248#M7882</guid>
      <dc:creator>ceroone</dc:creator>
      <dc:date>2021-04-26T15:43:46Z</dc:date>
    </item>
  </channel>
</rss>