<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: TSN Switch problem with OpenIL</title>
    <link>https://community.nxp.com/t5/Layerscape/TSN-Switch-problem-with-OpenIL/m-p/1267650#M7871</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I found it is because the value of MDIO_QSGMII&amp;nbsp; status register still 0x9. Why does this register take effect on linking up. My PHY connects to EMDIO.&lt;/P&gt;</description>
    <pubDate>Sun, 25 Apr 2021 12:02:04 GMT</pubDate>
    <dc:creator>ainolike</dc:creator>
    <dc:date>2021-04-25T12:02:04Z</dc:date>
    <item>
      <title>TSN Switch problem with OpenIL</title>
      <link>https://community.nxp.com/t5/Layerscape/TSN-Switch-problem-with-OpenIL/m-p/1266275#M7850</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I have some problem when using LS1028A TSN switch. The TSN Switch configuration as follows in Linux.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;ip link set eno2 up&lt;/P&gt;&lt;P&gt;ip link add name switch type bridge&lt;/P&gt;&lt;P&gt;ip link set dev swp0 master switch &amp;amp;&amp;amp; ip link set swp0 up&lt;/P&gt;&lt;P&gt;ip link set dev swp1 master switch &amp;amp;&amp;amp; ip link set swp1 up&lt;/P&gt;&lt;P&gt;ip link set dev swp2 master switch &amp;amp;&amp;amp; ip link set swp2 up&lt;/P&gt;&lt;P&gt;ip link set dev swp3 master switch &amp;amp;&amp;amp; ip link set swp3 up&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;ifconfig switch 192.168.1.100&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;When using openil-v1.10, if I plug in the network cable first and then configure the command, I can ping the host at the other end of the network. If I configure the command first and then plug in the network cable, I cannot ping the host at the other end of the network, but after I plug in the network cable again, I can ping the host at the other end of the network.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;When using LSDK2004, no matter I configure the command first or plug in the network cable, it can ping normally.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 22 Apr 2021 03:32:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/TSN-Switch-problem-with-OpenIL/m-p/1266275#M7850</guid>
      <dc:creator>ainolike</dc:creator>
      <dc:date>2021-04-22T03:32:55Z</dc:date>
    </item>
    <item>
      <title>Re: TSN Switch problem with OpenIL</title>
      <link>https://community.nxp.com/t5/Layerscape/TSN-Switch-problem-with-OpenIL/m-p/1267650#M7871</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I found it is because the value of MDIO_QSGMII&amp;nbsp; status register still 0x9. Why does this register take effect on linking up. My PHY connects to EMDIO.&lt;/P&gt;</description>
      <pubDate>Sun, 25 Apr 2021 12:02:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/TSN-Switch-problem-with-OpenIL/m-p/1267650#M7871</guid>
      <dc:creator>ainolike</dc:creator>
      <dc:date>2021-04-25T12:02:04Z</dc:date>
    </item>
    <item>
      <title>Re: TSN Switch problem with OpenIL</title>
      <link>https://community.nxp.com/t5/Layerscape/TSN-Switch-problem-with-OpenIL/m-p/1270616#M7906</link>
      <description>&lt;P&gt;The PHY chip has been linked up, but the LINK_STAT bit of&amp;nbsp;&lt;SPAN class="fontstyle0"&gt;QSGMII Status&lt;/SPAN&gt;&amp;nbsp;Register is still 0.&amp;nbsp;Why does this bit not change？In what circumstances will it change？&lt;/P&gt;</description>
      <pubDate>Fri, 30 Apr 2021 02:56:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/TSN-Switch-problem-with-OpenIL/m-p/1270616#M7906</guid>
      <dc:creator>ainolike</dc:creator>
      <dc:date>2021-04-30T02:56:04Z</dc:date>
    </item>
  </channel>
</rss>