<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LS1088A Thermal problem (-40 Degree) in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1088A-Thermal-problem-40-Degree/m-p/1265909#M7846</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are using "LS1088AXE7MQA" CPU in our board. We powered our board at -40 Degree. Device boot itself at -40 degree and during 1-2 hours,&amp;nbsp; It's functions run correctly (clocks and powers are also all stable) however after 1-2 hours, LS1088 assertes a reset request from its "RESET_REQ_B" pin and CPU resets itself and the boot sequance restarts. After reboot sequence complated, CPU again starts working correctly. However, this can be happen periodically eg in every&amp;nbsp; 1-2 hours. We turned off thermal management unit (TMU) inside the chip. Turning off TMU made device more stable at -40 degree however, we can still encounter this reboot problem periodically eg 3-4 hours after TMU is disabled. What are the possible reasons that cause this fault ? In which conditions does LS1088AXE7MQA assert reset request?&amp;nbsp; I also wrote down our RCW datas :&amp;nbsp;&lt;/P&gt;&lt;P&gt;Reset Configuration Word (RCW):&lt;BR /&gt;00000000: 30004014 00000030 00000000 00000000&lt;BR /&gt;00000010: 00000000 000a0000 00300000 00000000&lt;BR /&gt;00000020: 016011a0 00002580 00000000 00000000&lt;BR /&gt;00000030: 0000004b 00000000 00002403 00000000&lt;BR /&gt;00000040: 00000000 00000000 00000000 00000000&lt;BR /&gt;00000050: 00000000 00000000 00000000 00000000&lt;BR /&gt;00000060: 00000000 00000000 00000009 000009e7&lt;BR /&gt;00000070: 33110004 00006050&lt;BR /&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You can also find the attached block diagram of the design.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mustafa Oguz Donmez.&lt;/P&gt;</description>
    <pubDate>Wed, 21 Apr 2021 14:31:29 GMT</pubDate>
    <dc:creator>MustafaOguz</dc:creator>
    <dc:date>2021-04-21T14:31:29Z</dc:date>
    <item>
      <title>LS1088A Thermal problem (-40 Degree)</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1088A-Thermal-problem-40-Degree/m-p/1265909#M7846</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are using "LS1088AXE7MQA" CPU in our board. We powered our board at -40 Degree. Device boot itself at -40 degree and during 1-2 hours,&amp;nbsp; It's functions run correctly (clocks and powers are also all stable) however after 1-2 hours, LS1088 assertes a reset request from its "RESET_REQ_B" pin and CPU resets itself and the boot sequance restarts. After reboot sequence complated, CPU again starts working correctly. However, this can be happen periodically eg in every&amp;nbsp; 1-2 hours. We turned off thermal management unit (TMU) inside the chip. Turning off TMU made device more stable at -40 degree however, we can still encounter this reboot problem periodically eg 3-4 hours after TMU is disabled. What are the possible reasons that cause this fault ? In which conditions does LS1088AXE7MQA assert reset request?&amp;nbsp; I also wrote down our RCW datas :&amp;nbsp;&lt;/P&gt;&lt;P&gt;Reset Configuration Word (RCW):&lt;BR /&gt;00000000: 30004014 00000030 00000000 00000000&lt;BR /&gt;00000010: 00000000 000a0000 00300000 00000000&lt;BR /&gt;00000020: 016011a0 00002580 00000000 00000000&lt;BR /&gt;00000030: 0000004b 00000000 00002403 00000000&lt;BR /&gt;00000040: 00000000 00000000 00000000 00000000&lt;BR /&gt;00000050: 00000000 00000000 00000000 00000000&lt;BR /&gt;00000060: 00000000 00000000 00000009 000009e7&lt;BR /&gt;00000070: 33110004 00006050&lt;BR /&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You can also find the attached block diagram of the design.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mustafa Oguz Donmez.&lt;/P&gt;</description>
      <pubDate>Wed, 21 Apr 2021 14:31:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1088A-Thermal-problem-40-Degree/m-p/1265909#M7846</guid>
      <dc:creator>MustafaOguz</dc:creator>
      <dc:date>2021-04-21T14:31:29Z</dc:date>
    </item>
    <item>
      <title>Re: LS1088A Thermal problem (-40 Degree)</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1088A-Thermal-problem-40-Degree/m-p/1267574#M7865</link>
      <description>&lt;P&gt;To determine RESET_REQ_B cause:&lt;/P&gt;
&lt;P&gt;1) Disable PORESET_B assertion in response to RESET_REQ_B assertion.&lt;/P&gt;
&lt;P&gt;2) After RESET_REQ_B assertion execute following commands in the ccs (CodeWarrior Connection Server) console:&lt;/P&gt;
&lt;P&gt;&lt;FONT face="courier new,courier"&gt;delete all&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT face="courier new,courier"&gt;config cc cwtap&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT face="courier new,courier"&gt;ccs::config_chain {ls1088a sap2}&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT face="courier new,courier"&gt;display ccs::get_config_chain&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT face="courier new,courier"&gt;display ccs::read_mem 2 0x1E60018 4 0 1&lt;BR /&gt;&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 24 Apr 2021 09:37:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1088A-Thermal-problem-40-Degree/m-p/1267574#M7865</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2021-04-24T09:37:42Z</dc:date>
    </item>
  </channel>
</rss>