<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic mdio read write in Linux in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/mdio-read-write-in-Linux/m-p/1265571#M7842</link>
    <description>&lt;P&gt;I am using phytool "&lt;A href="https://github.com/wkz/phytool&amp;quot;" target="_blank"&gt;https://github.com/wkz/phytool"&lt;/A&gt;&amp;nbsp;to read / write MDIO bus in Linux on LS1046ARDB Kit.&lt;/P&gt;&lt;P&gt;The read works fine but when i try to write , it gives following error&lt;/P&gt;&lt;P&gt;"error: phy_write (-22)".&lt;/P&gt;&lt;P&gt;Is it related to some permissions. Kindly help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 21 Apr 2021 04:49:50 GMT</pubDate>
    <dc:creator>rashmikj</dc:creator>
    <dc:date>2021-04-21T04:49:50Z</dc:date>
    <item>
      <title>mdio read write in Linux</title>
      <link>https://community.nxp.com/t5/Layerscape/mdio-read-write-in-Linux/m-p/1265571#M7842</link>
      <description>&lt;P&gt;I am using phytool "&lt;A href="https://github.com/wkz/phytool&amp;quot;" target="_blank"&gt;https://github.com/wkz/phytool"&lt;/A&gt;&amp;nbsp;to read / write MDIO bus in Linux on LS1046ARDB Kit.&lt;/P&gt;&lt;P&gt;The read works fine but when i try to write , it gives following error&lt;/P&gt;&lt;P&gt;"error: phy_write (-22)".&lt;/P&gt;&lt;P&gt;Is it related to some permissions. Kindly help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 21 Apr 2021 04:49:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/mdio-read-write-in-Linux/m-p/1265571#M7842</guid>
      <dc:creator>rashmikj</dc:creator>
      <dc:date>2021-04-21T04:49:50Z</dc:date>
    </item>
    <item>
      <title>Re: mdio read write in Linux</title>
      <link>https://community.nxp.com/t5/Layerscape/mdio-read-write-in-Linux/m-p/1266585#M7856</link>
      <description>&lt;P&gt;It seems that there is problem with this application. You could use "mdio write" command in u-boot, please refer to the following example.&lt;/P&gt;
&lt;P&gt;=&amp;gt; mdio write FM1@DTSEC3 0xd 0x7&lt;BR /&gt;=&amp;gt; mdio write FM1@DTSEC3 0xe 0x3c&lt;BR /&gt;=&amp;gt; mdio write FM1@DTSEC3 0xd 0x4007&lt;BR /&gt;=&amp;gt; mdio read FM1@DTSEC3 0xe&lt;BR /&gt;Reading from bus FSL_MDIO0&lt;BR /&gt;PHY at address 1:&lt;BR /&gt;14 - 0x6&lt;BR /&gt;=&amp;gt; mdio write FM1@DTSEC3 0xe 0x0&lt;BR /&gt;=&amp;gt; mdio read FM1@DTSEC3 0xe&lt;BR /&gt;Reading from bus FSL_MDIO0&lt;BR /&gt;PHY at address 1:&lt;BR /&gt;14 - 0x0&lt;BR /&gt;=&amp;gt;&lt;/P&gt;</description>
      <pubDate>Thu, 22 Apr 2021 10:16:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/mdio-read-write-in-Linux/m-p/1266585#M7856</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2021-04-22T10:16:07Z</dc:date>
    </item>
    <item>
      <title>Re: mdio read write in Linux</title>
      <link>https://community.nxp.com/t5/Layerscape/mdio-read-write-in-Linux/m-p/1266587#M7857</link>
      <description>&lt;P&gt;at uboot , it is working.&amp;nbsp; I want to access phy registers in Linux. Kindly help.&lt;/P&gt;</description>
      <pubDate>Thu, 22 Apr 2021 10:21:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/mdio-read-write-in-Linux/m-p/1266587#M7857</guid>
      <dc:creator>rashmikj</dc:creator>
      <dc:date>2021-04-22T10:21:48Z</dc:date>
    </item>
  </channel>
</rss>