<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックUSB Over Current Condition in LS1046</title>
    <link>https://community.nxp.com/t5/Layerscape/USB-Over-Current-Condition-in-LS1046/m-p/1253979#M7759</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I am working on our custom board based on LS1046A Processor.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The kernel log has&lt;STRONG&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;"usb usb3-port1: over-current condition"&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;and&amp;nbsp;&lt;STRONG&gt;"usb usb4-port1: over-current condition" .&lt;/STRONG&gt;&amp;nbsp; &amp;nbsp;We are not using USB in our card and USB_PWRFAULT pin is connected to ground and&amp;nbsp; USB_DRVVBUS is left floating.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;We even tried modifying this register&amp;nbsp;&lt;STRONG&gt;"SCFG_USBPWRFAULT_SELCR&amp;nbsp;"&amp;nbsp;&amp;nbsp;&lt;/STRONG&gt;with both 0x00000000 and 0x00000015(little-endian) But there is no change.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;USB2_PWRFAULT,&amp;nbsp; USB3_PWRFAULT,&amp;nbsp;USB2_DRVVBUS and&amp;nbsp;USB3_DRVVBUS is used as GPIOs.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 30 Mar 2021 05:08:16 GMT</pubDate>
    <dc:creator>rashmikj</dc:creator>
    <dc:date>2021-03-30T05:08:16Z</dc:date>
    <item>
      <title>USB Over Current Condition in LS1046</title>
      <link>https://community.nxp.com/t5/Layerscape/USB-Over-Current-Condition-in-LS1046/m-p/1253979#M7759</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I am working on our custom board based on LS1046A Processor.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The kernel log has&lt;STRONG&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;"usb usb3-port1: over-current condition"&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;and&amp;nbsp;&lt;STRONG&gt;"usb usb4-port1: over-current condition" .&lt;/STRONG&gt;&amp;nbsp; &amp;nbsp;We are not using USB in our card and USB_PWRFAULT pin is connected to ground and&amp;nbsp; USB_DRVVBUS is left floating.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;We even tried modifying this register&amp;nbsp;&lt;STRONG&gt;"SCFG_USBPWRFAULT_SELCR&amp;nbsp;"&amp;nbsp;&amp;nbsp;&lt;/STRONG&gt;with both 0x00000000 and 0x00000015(little-endian) But there is no change.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;USB2_PWRFAULT,&amp;nbsp; USB3_PWRFAULT,&amp;nbsp;USB2_DRVVBUS and&amp;nbsp;USB3_DRVVBUS is used as GPIOs.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 30 Mar 2021 05:08:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/USB-Over-Current-Condition-in-LS1046/m-p/1253979#M7759</guid>
      <dc:creator>rashmikj</dc:creator>
      <dc:date>2021-03-30T05:08:16Z</dc:date>
    </item>
    <item>
      <title>Re: USB Over Current Condition in LS1046</title>
      <link>https://community.nxp.com/t5/Layerscape/USB-Over-Current-Condition-in-LS1046/m-p/1254164#M7760</link>
      <description>&lt;P&gt;Default configuration in u-boot for the SCFG_USBPWRFAULT_SELCR register is 0x2900_0000 (big-endian).&lt;/P&gt;
&lt;P&gt;It means that USB1, USB2 and USB3 controllers receive PWRFAULT from dedicated USBx_PWRFAULT I/O.&lt;/P&gt;
&lt;P&gt;The USB3_PWRFAULT signal is not used and this pin is assigned to TDMB_RQ. See the LS1043ARDB schematic.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Use the following command in u-boot:&lt;/P&gt;
&lt;P&gt;mw 0x1570414 0x09000000&lt;/P&gt;
&lt;P&gt;This command sets 0b00 for USB3:&lt;/P&gt;
&lt;P&gt;00 - USB controller 3 has its PWRFAULT input tied inactive (no fault)&lt;/P&gt;</description>
      <pubDate>Tue, 30 Mar 2021 09:24:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/USB-Over-Current-Condition-in-LS1046/m-p/1254164#M7760</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2021-03-30T09:24:32Z</dc:date>
    </item>
  </channel>
</rss>