<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: uboot not loading in LS1046 in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/uboot-not-loading-in-LS1046/m-p/1250031#M7711</link>
    <description>&lt;P&gt;It seems that there is DDR initialization problem to cause the failing to read u-boot from DDR memory.&lt;/P&gt;
&lt;P&gt;Please use QCVS DDRv tool to do DDR configuration parameters optimization and validation. Please create a QCVS DDR project with "read from SPD" method, you could refer to document&amp;nbsp;&lt;A href="https://community.nxp.com/t5/Qonverge-Knowledge-Base/DDR-Controller-Configuration-on-LS2085-LS2080-Bringing-up/ta-p/1128310" target="_blank"&gt;https://community.nxp.com/t5/Qonverge-Knowledge-Base/DDR-Controller-Configuration-on-LS2085-LS2080-Bringing-up/ta-p/1128310&lt;/A&gt;&amp;nbsp;to do DDRv optimization.&lt;/P&gt;
&lt;P&gt;After using DDRv tool to get the optimized DDR controller configuration parameters, please modify atf source code in packages/firmware/atf/.&lt;/P&gt;
&lt;P&gt;Please modify the section "const struct ddr_cfg_regs static_1600" in plat/nxp/soc-ls1046/ls1046ardb/ddr_init.c.&lt;/P&gt;
&lt;P&gt;In addition please define&amp;nbsp;CONFIG_STATIC_DDR in&amp;nbsp;plat/nxp/soc-ls1046/ls1046ardb/platform_def.h.&lt;/P&gt;</description>
    <pubDate>Tue, 23 Mar 2021 03:36:09 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2021-03-23T03:36:09Z</dc:date>
    <item>
      <title>uboot not loading in LS1046</title>
      <link>https://community.nxp.com/t5/Layerscape/uboot-not-loading-in-LS1046/m-p/1249322#M7703</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I modified&amp;nbsp;ls1046ardb_tfa_defconfig as per our custom board and generated the fip.bin. this is log messages generated.&lt;/P&gt;&lt;P&gt;INFO: RCW BOOT SRC is QSPI&lt;BR /&gt;INFO: RCW BOOT SRC is QSPI&lt;BR /&gt;INFO: time base 5 ms&lt;BR /&gt;NOTICE: Fixed DDR on board&lt;BR /&gt;INFO: Time after parsing SPD 4 ms&lt;BR /&gt;INFO: Time before programming controller 8 ms&lt;BR /&gt;NOTICE: 4 GB DDR4, 64-bit, CL=15, ECC on&lt;BR /&gt;INFO: Time used by DDR driver 427 ms&lt;BR /&gt;NOTICE: BL2: v1.5(debug):LSDK-20.04-update-290520-dirty&lt;BR /&gt;NOTICE: BL2: Built : 09:24:41, Mar 22 2021&lt;BR /&gt;INFO: Configuring TrustZone Controller&lt;BR /&gt;INFO: Value of region base = ffe00000&lt;BR /&gt;INFO: Value of region base = 1ffe00000&lt;BR /&gt;INFO: Value of region base = fbe00000&lt;BR /&gt;INFO: Value of region base = 980000000&lt;BR /&gt;INFO: BL2: Doing platform setup&lt;BR /&gt;INFO: BL2: Loading image id 3&lt;BR /&gt;INFO: Loading image id=3 at address 0xfbe00000&lt;BR /&gt;INFO: Image id=3 loaded: 0xfbe00000 - 0xfbe0c644&lt;BR /&gt;INFO: BL2: Loading image id 5&lt;BR /&gt;INFO: Loading image id=5 at address 0x82000000&lt;BR /&gt;INFO: Image id=5 loaded: 0x82000000 - 0x820b694c&lt;BR /&gt;NOTICE: BL2: Booting BL31&lt;BR /&gt;INFO: Entry point address = 0xfbe00000&lt;BR /&gt;INFO: SPSR = 0x3cd&lt;BR /&gt;NOTICE: BL31: v1.5(debug):LSDK-20.04-update-290520-dirty&lt;BR /&gt;NOTICE: BL31: Built : 09:20:18, Mar 22 2021&lt;BR /&gt;NOTICE: Welcome to LS1046 BL31 Phase&lt;BR /&gt;INFO: ARM GICv2 driver initialized&lt;BR /&gt;INFO: BL31: Initializing runtime services&lt;BR /&gt;WARNING: BL31: cortex_a72: CPU workaround for 859971 was missing!&lt;BR /&gt;INFO: BL31: cortex_a72: CPU workaround for cve_2017_5715 was applied&lt;BR /&gt;INFO: BL31: cortex_a72: CPU workaround for cve_2018_3639 was applied&lt;BR /&gt;INFO: BL31: Preparing for EL3 exit to normal world&lt;BR /&gt;INFO: Entry point address = 0x82000000&lt;BR /&gt;INFO: SPSR = 0x3c9&lt;/P&gt;&lt;P&gt;It stops after this . What is the issue. Kindly help.&lt;/P&gt;</description>
      <pubDate>Mon, 22 Mar 2021 04:58:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/uboot-not-loading-in-LS1046/m-p/1249322#M7703</guid>
      <dc:creator>rashmikj</dc:creator>
      <dc:date>2021-03-22T04:58:13Z</dc:date>
    </item>
    <item>
      <title>Re: uboot not loading in LS1046</title>
      <link>https://community.nxp.com/t5/Layerscape/uboot-not-loading-in-LS1046/m-p/1250031#M7711</link>
      <description>&lt;P&gt;It seems that there is DDR initialization problem to cause the failing to read u-boot from DDR memory.&lt;/P&gt;
&lt;P&gt;Please use QCVS DDRv tool to do DDR configuration parameters optimization and validation. Please create a QCVS DDR project with "read from SPD" method, you could refer to document&amp;nbsp;&lt;A href="https://community.nxp.com/t5/Qonverge-Knowledge-Base/DDR-Controller-Configuration-on-LS2085-LS2080-Bringing-up/ta-p/1128310" target="_blank"&gt;https://community.nxp.com/t5/Qonverge-Knowledge-Base/DDR-Controller-Configuration-on-LS2085-LS2080-Bringing-up/ta-p/1128310&lt;/A&gt;&amp;nbsp;to do DDRv optimization.&lt;/P&gt;
&lt;P&gt;After using DDRv tool to get the optimized DDR controller configuration parameters, please modify atf source code in packages/firmware/atf/.&lt;/P&gt;
&lt;P&gt;Please modify the section "const struct ddr_cfg_regs static_1600" in plat/nxp/soc-ls1046/ls1046ardb/ddr_init.c.&lt;/P&gt;
&lt;P&gt;In addition please define&amp;nbsp;CONFIG_STATIC_DDR in&amp;nbsp;plat/nxp/soc-ls1046/ls1046ardb/platform_def.h.&lt;/P&gt;</description>
      <pubDate>Tue, 23 Mar 2021 03:36:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/uboot-not-loading-in-LS1046/m-p/1250031#M7711</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2021-03-23T03:36:09Z</dc:date>
    </item>
  </channel>
</rss>