<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LS1028A / LS1018A: multicore support in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1028A-LS1018A-multicore-support/m-p/1248320#M7690</link>
    <description>&lt;P&gt;The difference between LS1028A and LS1018A is that LS1028A is a multi-core SoC and LS1018A is not.&lt;/P&gt;&lt;P&gt;Is the multi-core support fully operational on LS1028A?&lt;/P&gt;&lt;P&gt;Which kind of setup specifies the number of core to use?&lt;/P&gt;&lt;P&gt;Is there some source code in some repository (kernel repository?) that enables or initializes the one or the two CPU cores?&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;</description>
    <pubDate>Thu, 18 Mar 2021 16:42:42 GMT</pubDate>
    <dc:creator>mbourhis</dc:creator>
    <dc:date>2021-03-18T16:42:42Z</dc:date>
    <item>
      <title>LS1028A / LS1018A: multicore support</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1028A-LS1018A-multicore-support/m-p/1248320#M7690</link>
      <description>&lt;P&gt;The difference between LS1028A and LS1018A is that LS1028A is a multi-core SoC and LS1018A is not.&lt;/P&gt;&lt;P&gt;Is the multi-core support fully operational on LS1028A?&lt;/P&gt;&lt;P&gt;Which kind of setup specifies the number of core to use?&lt;/P&gt;&lt;P&gt;Is there some source code in some repository (kernel repository?) that enables or initializes the one or the two CPU cores?&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;</description>
      <pubDate>Thu, 18 Mar 2021 16:42:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1028A-LS1018A-multicore-support/m-p/1248320#M7690</guid>
      <dc:creator>mbourhis</dc:creator>
      <dc:date>2021-03-18T16:42:42Z</dc:date>
    </item>
    <item>
      <title>Re: LS1028A / LS1018A: multicore support</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1028A-LS1018A-multicore-support/m-p/1248568#M7695</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Multi-core supports fully operational on LS1028A.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;In order to&amp;nbsp;specify&amp;nbsp; the number of core to use, you could use&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;bootargs&lt;/STRONG&gt; "maxcpus“, modify Linux Kernel configuration CONFIG_NR_CPUS or modify the&amp;nbsp;&lt;SPAN&gt;dts file only defining CPU.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;For example, you could specify "maxcpus=1" in the &lt;STRONG&gt;bootargs&lt;/STRONG&gt; to only run Linux on core0.&lt;/P&gt;
&lt;P&gt;Kernel command line: root=/dev/ram rw console=ttyS0,115200 maxcpus=1&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Initializing one or the two CPU cores, you could refer to the following.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;smp_setup_processor_id in&amp;nbsp;arch/arm64/kernel/setup.c&lt;/P&gt;
&lt;P&gt;__cpu_up in&amp;nbsp;arch/arm64/kernel/smp.c&lt;/P&gt;
&lt;P&gt;smp_init in&amp;nbsp;kernel/smp.c&lt;/P&gt;</description>
      <pubDate>Fri, 19 Mar 2021 03:44:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1028A-LS1018A-multicore-support/m-p/1248568#M7695</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2021-03-19T03:44:14Z</dc:date>
    </item>
  </channel>
</rss>