<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LS1028ARDB  AUDIO SGTL5000 in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1028ARDB-AUDIO-SGTL5000/m-p/1244087#M7657</link>
    <description>&lt;P&gt;Check your setting using the Section 7.2.13 of LSDK 2012 User Guide:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/user-guide/LSDKUG_Rev20.12.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/user-guide/LSDKUG_Rev20.12.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Draw attention on the following:&lt;/P&gt;
&lt;P&gt;1) Set EC1_SAI4_5_PMUX = 2 in rcw &lt;BR /&gt;2) Either Set SW5[8] = ON or do i2c mw 0x66 0x53 0x4” on U-Boot prompt &lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 11 Mar 2021 09:51:29 GMT</pubDate>
    <dc:creator>Pavel</dc:creator>
    <dc:date>2021-03-11T09:51:29Z</dc:date>
    <item>
      <title>LS1028ARDB  AUDIO SGTL5000</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1028ARDB-AUDIO-SGTL5000/m-p/1243939#M7656</link>
      <description>&lt;P&gt;I tested the audio on the ls1028ardb reference board. I tested it with reference to chapter 7.2.13 of LSDKUG_Rev20.12 and found that there was no audio output.&lt;BR /&gt;I found that the sai of ls1028 and imx8mq-evk use the same driver, so I found imx8mq for a comparison test. After comparing and testing with imx8mq-evk, and then tracking the code, it is found that the following functions cannot be entered in fsl-sai.c&amp;nbsp;&lt;/P&gt;&lt;P&gt;1.In&amp;nbsp;fsl_sai_check_ver functions ,execute the following code and return directly.&lt;/P&gt;&lt;P&gt;if (FSL_SAI_TCSR(offset) == FSL_SAI_VERID)&lt;BR /&gt;return 0;&lt;/P&gt;&lt;P&gt;2.In&amp;nbsp;fsl_sai_hw_params functions ,cannot enter the following if judgment。&lt;/P&gt;&lt;P&gt;if (!sai-&amp;gt;slave_mode[tx]) {&lt;BR /&gt;ret = fsl_sai_set_bclk(cpu_dai, tx, bclk);&lt;BR /&gt;if (ret)&lt;BR /&gt;return ret;&lt;/P&gt;&lt;P&gt;The above two pieces of code can run successfully on the imx8mq-evk board.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 11 Mar 2021 07:14:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1028ARDB-AUDIO-SGTL5000/m-p/1243939#M7656</guid>
      <dc:creator>540915622</dc:creator>
      <dc:date>2021-03-11T07:14:17Z</dc:date>
    </item>
    <item>
      <title>Re: LS1028ARDB  AUDIO SGTL5000</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1028ARDB-AUDIO-SGTL5000/m-p/1244087#M7657</link>
      <description>&lt;P&gt;Check your setting using the Section 7.2.13 of LSDK 2012 User Guide:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/user-guide/LSDKUG_Rev20.12.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/user-guide/LSDKUG_Rev20.12.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Draw attention on the following:&lt;/P&gt;
&lt;P&gt;1) Set EC1_SAI4_5_PMUX = 2 in rcw &lt;BR /&gt;2) Either Set SW5[8] = ON or do i2c mw 0x66 0x53 0x4” on U-Boot prompt &lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 11 Mar 2021 09:51:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1028ARDB-AUDIO-SGTL5000/m-p/1244087#M7657</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2021-03-11T09:51:29Z</dc:date>
    </item>
  </channel>
</rss>