<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: sdk_dpaa missing from mainline kernel?</title>
    <link>https://community.nxp.com/t5/Layerscape/sdk-dpaa-missing-from-mainline-kernel/m-p/1243362#M7655</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I met the same issue on&amp;nbsp;kernel-default-5.3.18-24.49.2... and cannot build with the option you mention...any additional idea for that?&lt;/P&gt;</description>
    <pubDate>Wed, 10 Mar 2021 15:06:48 GMT</pubDate>
    <dc:creator>masafumiohta</dc:creator>
    <dc:date>2021-03-10T15:06:48Z</dc:date>
    <item>
      <title>sdk_dpaa missing from mainline kernel?</title>
      <link>https://community.nxp.com/t5/Layerscape/sdk-dpaa-missing-from-mainline-kernel/m-p/908981#M4298</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It seems that&amp;nbsp;freescale/sdk_dpaa is missing from the mainline kernel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There seem to be a freescale/dpaa but that doesn't seem to work with the ethernet interfaces of the ls1043ardb board as it fails with:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;[ 2.775370] fsl_dpaa_mac 1ae0000.ethernet: dpaa_fq_alloc() failed&lt;BR /&gt;[ 2.781463] fsl_dpaa_mac 1ae0000.ethernet: dpaa_alloc_all_fqs() failed&lt;BR /&gt;[ 2.788524] fsl_dpa: probe of dpaa-ethernet.0 failed with error -12&lt;BR /&gt;[ 2.795077] fsl_dpaa_mac 1ae2000.ethernet: dpaa_fq_alloc() failed&lt;BR /&gt;[ 2.801168] fsl_dpaa_mac 1ae2000.ethernet: dpaa_alloc_all_fqs() failed&lt;BR /&gt;[ 2.808214] fsl_dpa: probe of dpaa-ethernet.1 failed with error -12&lt;BR /&gt;[ 2.814754] fsl_dpaa_mac 1ae4000.ethernet: dpaa_fq_alloc() failed&lt;BR /&gt;[ 2.820844] fsl_dpaa_mac 1ae4000.ethernet: dpaa_alloc_all_fqs() failed&lt;BR /&gt;[ 2.827882] fsl_dpa: probe of dpaa-ethernet.2 failed with error -12&lt;BR /&gt;[ 2.834421] fsl_dpaa_mac 1ae6000.ethernet: dpaa_fq_alloc() failed&lt;BR /&gt;[ 2.838293] ata1: SATA link down (SStatus 0 SControl 300)&lt;BR /&gt;[ 2.840515] fsl_dpaa_mac 1ae6000.ethernet: dpaa_alloc_all_fqs() failed&lt;BR /&gt;[ 2.852942] fsl_dpa: probe of dpaa-ethernet.3 failed with error -12&lt;BR /&gt;[ 2.859481] fsl_dpaa_mac 1ae8000.ethernet: dpaa_fq_alloc() failed&lt;BR /&gt;[ 2.865574] fsl_dpaa_mac 1ae8000.ethernet: dpaa_alloc_all_fqs() failed&lt;BR /&gt;[ 2.872609] fsl_dpa: probe of dpaa-ethernet.4 failed with error -12&lt;BR /&gt;[ 2.879149] fsl_dpaa_mac 1aea000.ethernet: dpaa_fq_alloc() failed&lt;BR /&gt;[ 2.885239] fsl_dpaa_mac 1aea000.ethernet: dpaa_alloc_all_fqs() failed&lt;BR /&gt;[ 2.892288] fsl_dpa: probe of dpaa-ethernet.5 failed with error -12&lt;BR /&gt;[ 2.898826] fsl_dpaa_mac 1af0000.ethernet: dpaa_fq_alloc() failed&lt;BR /&gt;[ 2.904916] fsl_dpaa_mac 1af0000.ethernet: dpaa_alloc_all_fqs() failed&lt;BR /&gt;[ 2.911953] fsl_dpa: probe of dpaa-ethernet.6 failed with error -12&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What would be the correct mainline driver to use?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Aug 2019 21:27:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/sdk-dpaa-missing-from-mainline-kernel/m-p/908981#M4298</guid>
      <dc:creator>francoisgervais</dc:creator>
      <dc:date>2019-08-27T21:27:49Z</dc:date>
    </item>
    <item>
      <title>Re: sdk_dpaa missing from mainline kernel?</title>
      <link>https://community.nxp.com/t5/Layerscape/sdk-dpaa-missing-from-mainline-kernel/m-p/908982#M4299</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="305433" data-username="francoisgervais" href="https://community.nxp.com/people/francoisgervais"&gt;Francois Gervais&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The followings are kernel options of upstream dpaa driver.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Repo:&amp;nbsp; git://git.kernel.org/pub/scm/linux/kernel/git/torvalds/linux.git&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Dtb: fsl-ls1043a-rdb.dtb&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;FSL_FMAN=y&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;FSL_DPAA=y&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;FSL_DPAA_ETH=y&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The mainline Kernel doesn't include freescale/sdk_dpaa, if you need it, you need to do the porting from LSDK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yiping&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Aug 2019 09:48:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/sdk-dpaa-missing-from-mainline-kernel/m-p/908982#M4299</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2019-08-28T09:48:19Z</dc:date>
    </item>
    <item>
      <title>Re: sdk_dpaa missing from mainline kernel?</title>
      <link>https://community.nxp.com/t5/Layerscape/sdk-dpaa-missing-from-mainline-kernel/m-p/908983#M4300</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I do have those configs but it fails with the error shown in the first post.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any idea why?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Aug 2019 13:54:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/sdk-dpaa-missing-from-mainline-kernel/m-p/908983#M4300</guid>
      <dc:creator>francoisgervais</dc:creator>
      <dc:date>2019-08-30T13:54:29Z</dc:date>
    </item>
    <item>
      <title>Re: sdk_dpaa missing from mainline kernel?</title>
      <link>https://community.nxp.com/t5/Layerscape/sdk-dpaa-missing-from-mainline-kernel/m-p/908984#M4301</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please use the attached Kernel configuration to build Kernel image, which is provided by the testing team.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Sep 2019 07:10:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/sdk-dpaa-missing-from-mainline-kernel/m-p/908984#M4301</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2019-09-03T07:10:49Z</dc:date>
    </item>
    <item>
      <title>Re: sdk_dpaa missing from mainline kernel?</title>
      <link>https://community.nxp.com/t5/Layerscape/sdk-dpaa-missing-from-mainline-kernel/m-p/1243362#M7655</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I met the same issue on&amp;nbsp;kernel-default-5.3.18-24.49.2... and cannot build with the option you mention...any additional idea for that?&lt;/P&gt;</description>
      <pubDate>Wed, 10 Mar 2021 15:06:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/sdk-dpaa-missing-from-mainline-kernel/m-p/1243362#M7655</guid>
      <dc:creator>masafumiohta</dc:creator>
      <dc:date>2021-03-10T15:06:48Z</dc:date>
    </item>
  </channel>
</rss>