<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Encrypted udp packet drop in LS1046arbd kit in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Encrypted-udp-packet-drop-in-LS1046arbd-kit/m-p/1239920#M7614</link>
    <description>&lt;P&gt;I am trying establish end to end secure communication between two PCs and two LS1046ardb kit between PCs with AES encryption for IP data using dpdk . Please find attached setup diagram.&lt;/P&gt;&lt;P&gt;The encrypted packet comes out of one Kit where am unable to see in the rx queue of the other kit.&lt;/P&gt;&lt;P&gt;As IP data is encrypted, UDP ports and length is also encrypted hence length might be out of range of standard length .&lt;/P&gt;&lt;P&gt;Does FMC drop packets based on UDP data length?&lt;/P&gt;&lt;P&gt;If so how do i change it?&lt;/P&gt;&lt;P&gt;I am using following files for fmc.&lt;/P&gt;&lt;P&gt;export DPAA_FMC_MODE=1&lt;/P&gt;&lt;P&gt;fmc -c /usr/local/dpdk/dpaa/usdpaa_config_ls1046.xml -p /usr/local/dpdk/dpaa/usdpaa_policy_hash_ipv4_1queue.xml -a&lt;/P&gt;</description>
    <pubDate>Thu, 04 Mar 2021 04:44:11 GMT</pubDate>
    <dc:creator>rashmikj</dc:creator>
    <dc:date>2021-03-04T04:44:11Z</dc:date>
    <item>
      <title>Encrypted udp packet drop in LS1046arbd kit</title>
      <link>https://community.nxp.com/t5/Layerscape/Encrypted-udp-packet-drop-in-LS1046arbd-kit/m-p/1239920#M7614</link>
      <description>&lt;P&gt;I am trying establish end to end secure communication between two PCs and two LS1046ardb kit between PCs with AES encryption for IP data using dpdk . Please find attached setup diagram.&lt;/P&gt;&lt;P&gt;The encrypted packet comes out of one Kit where am unable to see in the rx queue of the other kit.&lt;/P&gt;&lt;P&gt;As IP data is encrypted, UDP ports and length is also encrypted hence length might be out of range of standard length .&lt;/P&gt;&lt;P&gt;Does FMC drop packets based on UDP data length?&lt;/P&gt;&lt;P&gt;If so how do i change it?&lt;/P&gt;&lt;P&gt;I am using following files for fmc.&lt;/P&gt;&lt;P&gt;export DPAA_FMC_MODE=1&lt;/P&gt;&lt;P&gt;fmc -c /usr/local/dpdk/dpaa/usdpaa_config_ls1046.xml -p /usr/local/dpdk/dpaa/usdpaa_policy_hash_ipv4_1queue.xml -a&lt;/P&gt;</description>
      <pubDate>Thu, 04 Mar 2021 04:44:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Encrypted-udp-packet-drop-in-LS1046arbd-kit/m-p/1239920#M7614</guid>
      <dc:creator>rashmikj</dc:creator>
      <dc:date>2021-03-04T04:44:11Z</dc:date>
    </item>
    <item>
      <title>Re: Encrypted udp packet drop in LS1046arbd kit</title>
      <link>https://community.nxp.com/t5/Layerscape/Encrypted-udp-packet-drop-in-LS1046arbd-kit/m-p/1253087#M7751</link>
      <description>&lt;P&gt;If you encrypt everything past the IP header, the the first check that will&lt;BR /&gt;fail is UDP checksum.&amp;nbsp; You received explanations&lt;BR /&gt;in &lt;A href="https://community.nxp.com/t5/Layerscape/udp-checksum-on-rx-packet-of-dpdk/td-p/1242890" target="_self"&gt;this thread&lt;/A&gt;. More details on the checks performed over L4 headers can be&lt;BR /&gt;found in LS1046ADPAARM, Section 5.9.4.7.15. For valid methods to&lt;BR /&gt;handle cryptographically protected traffic, study l2fwd-crypto and ipsec-secgw &lt;BR /&gt;DPDK applications described in LSDK User Guide, Section 9.2.4.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Platon&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 27 Mar 2021 01:11:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Encrypted-udp-packet-drop-in-LS1046arbd-kit/m-p/1253087#M7751</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2021-03-27T01:11:26Z</dc:date>
    </item>
  </channel>
</rss>