<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: BL2 run next image failed</title>
    <link>https://community.nxp.com/t5/Layerscape/BL2-run-next-image-failed/m-p/1235672#M7598</link>
    <description>&lt;P&gt;DDR initialization is a key step at BL2&amp;nbsp; stage that later boot stages&lt;BR /&gt;and the OS rely on. Making sure it creates a reliable DDR memory configuration is essential for the rest of the boot process. You can find advanced information &lt;BR /&gt;on DDR ATF driver in L SDK User Guide, Section 5.2.1.1. The document can be downloaded by following &lt;A href="https://www.nxp.com/docs/en/user-guide/LSDKUG_Rev20.04_290520.pdf" target="_self"&gt;this link.&lt;/A&gt; DDR settings are specific to the board and&lt;BR /&gt;used memory chips, thus no universal settings can be provided. My suggestion in&lt;BR /&gt;regards to the described issue is to use the &lt;A href="https://docs.nxp.com/bundle/GUID-062F363E-637F-47AB-8C1A-84C46F4167DA/page/GUID-415D1193-1613-48B5-9AE1-259A86A506A1.html" target="_self"&gt;DDR tool from QCVS&lt;/A&gt; software suite &lt;BR /&gt;to setup and verify your configuration before you proceed with debugging of the&lt;BR /&gt;rest of the boot code.&lt;/P&gt;
&lt;P&gt;I'm also moving your recent inquiry about caslat_x to a new thread to be&lt;BR /&gt;followed by another engineer with expertise in DDR memory hardware. If you have&lt;BR /&gt;more questions specifically about ATF or ATF debugging, please feel free to update this thread.&lt;/P&gt;
&lt;P&gt;For questions that are more DDR memory related and specific LS1028A DDR controller&lt;BR /&gt;initialization, please post in the &lt;A href="https://community.nxp.com/t5/Layerscape/Re-BL2-run-next-image-failed/m-p/1233896/highlight/true#M7597" target="_self"&gt;new thread&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Platon.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 24 Feb 2021 10:05:34 GMT</pubDate>
    <dc:creator>bpe</dc:creator>
    <dc:date>2021-02-24T10:05:34Z</dc:date>
    <item>
      <title>BL2 run next image failed</title>
      <link>https://community.nxp.com/t5/Layerscape/BL2-run-next-image-failed/m-p/1232688#M7548</link>
      <description>&lt;P&gt;Hi, I'm testing lsdk2012 atf code on LS1028.&amp;nbsp;BL2 has loaded BL31 and U-Boot image successfully, while there is no more print info when BL2 calls bl2_run_next_image. The print info as following:&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;NOTICE:&amp;nbsp; 4GB DDR4, 32-bit, CL=11, ECC off&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;INFO:&amp;nbsp; &amp;nbsp; Time used by DDR driver 18 ms&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;NOTICE: BL2: v1.5(release):LSDK-20.12-dirty&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;NOTICE: BL2:Build: 07:50:34, Feb 18 2021&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;INFO:&amp;nbsp; &amp;nbsp;Configuration TrustZone Controller&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;INFO:&amp;nbsp; &amp;nbsp;Value of region base = ffe00000&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;INFO:&amp;nbsp; &amp;nbsp;Value of region base = 1ffe00000&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;INFO:&amp;nbsp; &amp;nbsp;Value of region base = fbe00000&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;INFO:&amp;nbsp; &amp;nbsp;Value of region base = 2180000000&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;INFO:&amp;nbsp; &amp;nbsp;BL2: Doing paltform setup&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;INFO:&amp;nbsp; &amp;nbsp;BL2: Loading image id 3&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;INFO:&amp;nbsp; &amp;nbsp;Loading image id=3 at address 0xfbe00000&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;INFO:&amp;nbsp; &amp;nbsp;Image id=3 loaded: 0xfbe00000 - 0xfbe0a169&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;INFO:&amp;nbsp; &amp;nbsp;BL2: Loading image id 5&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;INFO:&amp;nbsp; &amp;nbsp;Loading image id=5 at address 0x82000000&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;INFO:&amp;nbsp; &amp;nbsp;Image id=5 loaded: 0x82000000 - 0x820b4477&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;NOTICE:&amp;nbsp; BL2: Booting BL31&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;INFO:&amp;nbsp; &amp;nbsp; Entry point address =&amp;nbsp;0xfbe00000&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;INFO:&amp;nbsp; &amp;nbsp; SPSR = 0x3cd&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 18 Feb 2021 08:47:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/BL2-run-next-image-failed/m-p/1232688#M7548</guid>
      <dc:creator>ainolike</dc:creator>
      <dc:date>2021-02-18T08:47:28Z</dc:date>
    </item>
    <item>
      <title>Re: BL2 run next image failed</title>
      <link>https://community.nxp.com/t5/Layerscape/BL2-run-next-image-failed/m-p/1235668#M7570</link>
      <description>caslat_x question moved to a new thread</description>
      <pubDate>Sat, 20 Feb 2021 05:17:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/BL2-run-next-image-failed/m-p/1235668#M7570</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2021-02-20T05:17:46Z</dc:date>
    </item>
    <item>
      <title>Re: BL2 run next image failed</title>
      <link>https://community.nxp.com/t5/Layerscape/BL2-run-next-image-failed/m-p/1235672#M7598</link>
      <description>&lt;P&gt;DDR initialization is a key step at BL2&amp;nbsp; stage that later boot stages&lt;BR /&gt;and the OS rely on. Making sure it creates a reliable DDR memory configuration is essential for the rest of the boot process. You can find advanced information &lt;BR /&gt;on DDR ATF driver in L SDK User Guide, Section 5.2.1.1. The document can be downloaded by following &lt;A href="https://www.nxp.com/docs/en/user-guide/LSDKUG_Rev20.04_290520.pdf" target="_self"&gt;this link.&lt;/A&gt; DDR settings are specific to the board and&lt;BR /&gt;used memory chips, thus no universal settings can be provided. My suggestion in&lt;BR /&gt;regards to the described issue is to use the &lt;A href="https://docs.nxp.com/bundle/GUID-062F363E-637F-47AB-8C1A-84C46F4167DA/page/GUID-415D1193-1613-48B5-9AE1-259A86A506A1.html" target="_self"&gt;DDR tool from QCVS&lt;/A&gt; software suite &lt;BR /&gt;to setup and verify your configuration before you proceed with debugging of the&lt;BR /&gt;rest of the boot code.&lt;/P&gt;
&lt;P&gt;I'm also moving your recent inquiry about caslat_x to a new thread to be&lt;BR /&gt;followed by another engineer with expertise in DDR memory hardware. If you have&lt;BR /&gt;more questions specifically about ATF or ATF debugging, please feel free to update this thread.&lt;/P&gt;
&lt;P&gt;For questions that are more DDR memory related and specific LS1028A DDR controller&lt;BR /&gt;initialization, please post in the &lt;A href="https://community.nxp.com/t5/Layerscape/Re-BL2-run-next-image-failed/m-p/1233896/highlight/true#M7597" target="_self"&gt;new thread&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Platon.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 24 Feb 2021 10:05:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/BL2-run-next-image-failed/m-p/1235672#M7598</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2021-02-24T10:05:34Z</dc:date>
    </item>
  </channel>
</rss>