<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Display Clock Frequency in U-Boot for LS1043ARDB in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Display-Clock-Frequency-in-U-Boot-for-LS1043ARDB/m-p/1232715#M7549</link>
    <description>&lt;P&gt;See attached snapshot. This snapshot shows that u-boot reports CPUx clock, Bus clock, DDR clock and FMAN clock on the LS1043a board.&lt;/P&gt;
&lt;P&gt;Is additional clock needed to show?&lt;/P&gt;</description>
    <pubDate>Thu, 18 Feb 2021 09:11:33 GMT</pubDate>
    <dc:creator>Pavel</dc:creator>
    <dc:date>2021-02-18T09:11:33Z</dc:date>
    <item>
      <title>Display Clock Frequency in U-Boot for LS1043ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/Display-Clock-Frequency-in-U-Boot-for-LS1043ARDB/m-p/1232245#M7544</link>
      <description>&lt;P&gt;How do I display the CPU clock frequencies in U-Boot? CMD_CLK is deprecated and the only other cmd that possibly displays this information is CMD_CPU, however, enabling CMD_CPU causes U-Boot not to build. Is there a command available that I can enable that will display the clock frequencies?&lt;/P&gt;</description>
      <pubDate>Wed, 17 Feb 2021 20:37:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Display-Clock-Frequency-in-U-Boot-for-LS1043ARDB/m-p/1232245#M7544</guid>
      <dc:creator>aismail102</dc:creator>
      <dc:date>2021-02-17T20:37:07Z</dc:date>
    </item>
    <item>
      <title>Re: Display Clock Frequency in U-Boot for LS1043ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/Display-Clock-Frequency-in-U-Boot-for-LS1043ARDB/m-p/1232715#M7549</link>
      <description>&lt;P&gt;See attached snapshot. This snapshot shows that u-boot reports CPUx clock, Bus clock, DDR clock and FMAN clock on the LS1043a board.&lt;/P&gt;
&lt;P&gt;Is additional clock needed to show?&lt;/P&gt;</description>
      <pubDate>Thu, 18 Feb 2021 09:11:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Display-Clock-Frequency-in-U-Boot-for-LS1043ARDB/m-p/1232715#M7549</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2021-02-18T09:11:33Z</dc:date>
    </item>
  </channel>
</rss>