<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 Re: LS1046ARDB KIT EEPROM READ AND WRITE</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1046ARDB-KIT-EEPROM-READ-AND-WRITE/m-p/1231280#M7528</link>
    <description>&lt;P&gt;The source code is attached .I could open the eeprom i2c interface.But after that fail to write i2c address errror is coming. Kindly help. Also i would like to know which address locations MAC address and other important data is stored.&lt;/P&gt;</description>
    <pubDate>Tue, 16 Feb 2021 03:43:13 GMT</pubDate>
    <dc:creator>IB2020</dc:creator>
    <dc:date>2021-02-16T03:43:13Z</dc:date>
    <item>
      <title>LS1046ARDB KIT EEPROM READ AND WRITE</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046ARDB-KIT-EEPROM-READ-AND-WRITE/m-p/1227674#M7472</link>
      <description>&lt;P&gt;i was trying to read and write data bytes to EEPROM CAT24C05. It is not working.I could open the i2c&amp;nbsp; interface with slave address 52 .After that writing address byte is not happening.&lt;/P&gt;</description>
      <pubDate>Mon, 08 Feb 2021 05:08:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046ARDB-KIT-EEPROM-READ-AND-WRITE/m-p/1227674#M7472</guid>
      <dc:creator>IB2020</dc:creator>
      <dc:date>2021-02-08T05:08:57Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046ARDB KIT EEPROM READ AND WRITE</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046ARDB-KIT-EEPROM-READ-AND-WRITE/m-p/1227715#M7476</link>
      <description>&lt;P&gt;Please provide log of the performed operations.&lt;/P&gt;
&lt;P&gt;Please consider that the SEEPROM contains important system information (like MAC addresses), so it has to be handled accurately.&lt;/P&gt;</description>
      <pubDate>Mon, 08 Feb 2021 06:22:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046ARDB-KIT-EEPROM-READ-AND-WRITE/m-p/1227715#M7476</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2021-02-08T06:22:47Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046ARDB KIT EEPROM READ AND WRITE</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046ARDB-KIT-EEPROM-READ-AND-WRITE/m-p/1231280#M7528</link>
      <description>&lt;P&gt;The source code is attached .I could open the eeprom i2c interface.But after that fail to write i2c address errror is coming. Kindly help. Also i would like to know which address locations MAC address and other important data is stored.&lt;/P&gt;</description>
      <pubDate>Tue, 16 Feb 2021 03:43:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046ARDB-KIT-EEPROM-READ-AND-WRITE/m-p/1231280#M7528</guid>
      <dc:creator>IB2020</dc:creator>
      <dc:date>2021-02-16T03:43:13Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046ARDB KIT EEPROM READ AND WRITE</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046ARDB-KIT-EEPROM-READ-AND-WRITE/m-p/1231418#M7530</link>
      <description>&lt;P&gt;For the I2C source code refer to the U-Boot driver:&lt;/P&gt;
&lt;PRE&gt;drivers/i2c/mxc_i2c.c&lt;/PRE&gt;</description>
      <pubDate>Tue, 16 Feb 2021 08:59:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046ARDB-KIT-EEPROM-READ-AND-WRITE/m-p/1231418#M7530</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2021-02-16T08:59:05Z</dc:date>
    </item>
  </channel>
</rss>