<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックLS1028A Power Sequencing Conflict In Documentation</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1028A-Power-Sequencing-Conflict-In-Documentation/m-p/1225855#M7460</link>
    <description>&lt;P&gt;I believe there is a power sequencing conflict between the LS1028A datasheet and the PMIC datasheet.&lt;/P&gt;&lt;P&gt;The LS1028A datasheet shows the power sequencing requirements as follows.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Step 1: 1.8V&lt;/LI&gt;&lt;LI&gt;Step 2: 1.0V / 0.9V&lt;/LI&gt;&lt;LI&gt;Step 3: 1.35V&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;The PMIC for the LS1028A (34VR500V9) shows the following sequence.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Step 1: 2.5V&lt;/LI&gt;&lt;LI&gt;Step 2: 1.8V&lt;/LI&gt;&lt;LI&gt;Step 3: 1.35V&lt;/LI&gt;&lt;LI&gt;Step 4: 1.0V / 0.9V, LDO output for VDD enable&lt;/LI&gt;&lt;LI&gt;Step 5: LDO output for DDR enable&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;The 1.35V and 1.0V (VDD) are out order between the two datasheets.&lt;/P&gt;&lt;P&gt;We are considering implementing a custom power scheme not utilizing the NXP PMIC. What order is correct?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 03 Feb 2021 21:57:38 GMT</pubDate>
    <dc:creator>jimmymm</dc:creator>
    <dc:date>2021-02-03T21:57:38Z</dc:date>
    <item>
      <title>LS1028A Power Sequencing Conflict In Documentation</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1028A-Power-Sequencing-Conflict-In-Documentation/m-p/1225855#M7460</link>
      <description>&lt;P&gt;I believe there is a power sequencing conflict between the LS1028A datasheet and the PMIC datasheet.&lt;/P&gt;&lt;P&gt;The LS1028A datasheet shows the power sequencing requirements as follows.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Step 1: 1.8V&lt;/LI&gt;&lt;LI&gt;Step 2: 1.0V / 0.9V&lt;/LI&gt;&lt;LI&gt;Step 3: 1.35V&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;The PMIC for the LS1028A (34VR500V9) shows the following sequence.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Step 1: 2.5V&lt;/LI&gt;&lt;LI&gt;Step 2: 1.8V&lt;/LI&gt;&lt;LI&gt;Step 3: 1.35V&lt;/LI&gt;&lt;LI&gt;Step 4: 1.0V / 0.9V, LDO output for VDD enable&lt;/LI&gt;&lt;LI&gt;Step 5: LDO output for DDR enable&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;The 1.35V and 1.0V (VDD) are out order between the two datasheets.&lt;/P&gt;&lt;P&gt;We are considering implementing a custom power scheme not utilizing the NXP PMIC. What order is correct?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 03 Feb 2021 21:57:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1028A-Power-Sequencing-Conflict-In-Documentation/m-p/1225855#M7460</guid>
      <dc:creator>jimmymm</dc:creator>
      <dc:date>2021-02-03T21:57:38Z</dc:date>
    </item>
    <item>
      <title>Re: LS1028A Power Sequencing Conflict In Documentation</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1028A-Power-Sequencing-Conflict-In-Documentation/m-p/1226087#M7462</link>
      <description>&lt;P&gt;The power sequence described in the data sheet is correct.&lt;/P&gt;
&lt;P&gt;Note that 'Step 3' of the power sequence contains following remark:&lt;/P&gt;
&lt;P&gt;"System with DDR4 memory (1.2V): G1VDD (&lt;STRONG&gt;XVDD, AVDDSD1_PLL1 and AVDD_SD1_PLL2 can be powered up in any step&lt;/STRONG&gt;)". In other words, 1.35V order is relaxed in DDR4 case, so no conflict.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Bulat&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 04 Feb 2021 05:15:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1028A-Power-Sequencing-Conflict-In-Documentation/m-p/1226087#M7462</guid>
      <dc:creator>Bulat</dc:creator>
      <dc:date>2021-02-04T05:15:27Z</dc:date>
    </item>
  </channel>
</rss>