<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックESD precautions while using the LS1028ARDB?</title>
    <link>https://community.nxp.com/t5/Layerscape/ESD-precautions-while-using-the-LS1028ARDB/m-p/1223764#M7428</link>
    <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I wanted to know if there are any ESD precautions I need to follow while using the LS1028ARDB boards. Correct me if I am wrong, but these boards are designed to be used in Industrial environments so I am assuming that they do not need to be handled with any ESD precautions.&lt;/P&gt;&lt;P&gt;Any documentation regarding how to handle and store these boards would be helpful.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
    <pubDate>Mon, 01 Feb 2021 05:54:55 GMT</pubDate>
    <dc:creator>acentauri92</dc:creator>
    <dc:date>2021-02-01T05:54:55Z</dc:date>
    <item>
      <title>ESD precautions while using the LS1028ARDB?</title>
      <link>https://community.nxp.com/t5/Layerscape/ESD-precautions-while-using-the-LS1028ARDB/m-p/1223764#M7428</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I wanted to know if there are any ESD precautions I need to follow while using the LS1028ARDB boards. Correct me if I am wrong, but these boards are designed to be used in Industrial environments so I am assuming that they do not need to be handled with any ESD precautions.&lt;/P&gt;&lt;P&gt;Any documentation regarding how to handle and store these boards would be helpful.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Mon, 01 Feb 2021 05:54:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/ESD-precautions-while-using-the-LS1028ARDB/m-p/1223764#M7428</guid>
      <dc:creator>acentauri92</dc:creator>
      <dc:date>2021-02-01T05:54:55Z</dc:date>
    </item>
    <item>
      <title>Re: ESD precautions while using the LS1028ARDB?</title>
      <link>https://community.nxp.com/t5/Layerscape/ESD-precautions-while-using-the-LS1028ARDB/m-p/1227878#M7486</link>
      <description>&lt;P&gt;The QorIQ® LS1028A reference design board (LS1028ARDB) is a computing, evaluation, development, and test platform&lt;BR /&gt;supporting the QorIQ LS1028A processor,&lt;/P&gt;
&lt;P&gt;The LS1028ARDB can be used to develop and demonstrate human machine interface systems, industrial control systems such&lt;BR /&gt;as robotics controllers and motion controllers, and PLCs. The reference design also provides the functionality needed for Industrial&lt;BR /&gt;IoT gateways, edge computing, industrial PCs, and wireless or wired networking gateways.&lt;/P&gt;
&lt;P&gt;Developers using the LS1028ARDB can perform standard debugging tasks, such as:&lt;/P&gt;
&lt;P&gt;• Upload and run code&lt;BR /&gt;• Set breakpoints&lt;BR /&gt;• Display memory and registers&lt;BR /&gt;• Connect and incorporate proprietary hardware into target systems using the LS1028A as a host processor&lt;BR /&gt;• Use the LS1028ARDB as a demonstration tool&lt;/P&gt;
&lt;P&gt;The LS1028ARDB was not designed to be directly used in any Industrial environments so it need to be handled with all ESD precautions.&lt;/P&gt;</description>
      <pubDate>Mon, 08 Feb 2021 10:20:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/ESD-precautions-while-using-the-LS1028ARDB/m-p/1227878#M7486</guid>
      <dc:creator>andrei_skok</dc:creator>
      <dc:date>2021-02-08T10:20:13Z</dc:date>
    </item>
  </channel>
</rss>