<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LS1088a external interrupt in Linux in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1088a-external-interrupt-in-Linux/m-p/1222744#M7414</link>
    <description>&lt;P&gt;Use sysfs for GPIO inputs.&lt;/P&gt;
&lt;P&gt;This LSDK provides correct operation for sysfs using for GPIO inputs.&lt;/P&gt;
&lt;P&gt;Use sysfs for using interrupt from the GPIO4_06.&lt;/P&gt;
&lt;P&gt;See attached message dump for testing the GPIO4_06 input.&lt;/P&gt;</description>
    <pubDate>Thu, 28 Jan 2021 15:34:34 GMT</pubDate>
    <dc:creator>Pavel</dc:creator>
    <dc:date>2021-01-28T15:34:34Z</dc:date>
    <item>
      <title>LS1088a external interrupt in Linux</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1088a-external-interrupt-in-Linux/m-p/1205039#M7281</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Does anyone have a working example of setting up an external (active low) interrupt to the ls1088a processor which they could share? I am writing a kernel module to handle interrupts and I have tried setting this up as a direct interrupt and as a GPIO through expander. I have also tried using the recent ‘extirq’ linux kernel changes added to v5.5. In all cases the processor does not recognize the interrupt assertion.&lt;/P&gt;&lt;P&gt;Any help is much appreciated. Thank you.&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 29 Dec 2020 22:35:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1088a-external-interrupt-in-Linux/m-p/1205039#M7281</guid>
      <dc:creator>mrecoskie</dc:creator>
      <dc:date>2020-12-29T22:35:16Z</dc:date>
    </item>
    <item>
      <title>Re: LS1088a external interrupt in Linux</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1088a-external-interrupt-in-Linux/m-p/1222744#M7414</link>
      <description>&lt;P&gt;Use sysfs for GPIO inputs.&lt;/P&gt;
&lt;P&gt;This LSDK provides correct operation for sysfs using for GPIO inputs.&lt;/P&gt;
&lt;P&gt;Use sysfs for using interrupt from the GPIO4_06.&lt;/P&gt;
&lt;P&gt;See attached message dump for testing the GPIO4_06 input.&lt;/P&gt;</description>
      <pubDate>Thu, 28 Jan 2021 15:34:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1088a-external-interrupt-in-Linux/m-p/1222744#M7414</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2021-01-28T15:34:34Z</dc:date>
    </item>
  </channel>
</rss>