<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックLS1027A using a switch with SGMII</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1027A-using-a-switch-with-SGMII/m-p/1221414#M7395</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We are using the LS1027AE processor in a custom board with an Ethernet Switch (KSZ9477S, datasheet attached in this post) connected through SGMII1G-S in the Lane C of the SerDes protocol. This Switch will communicate via I2C with the processor during its configuration. According to the LS1028A Reference Manual, in the SerDes chapter, the SGMII1G-S uses the TSN Switch peripheral instead of ENETC. We configured the Switch as a slave I2C and the MDIO PHYs in our DTS (find it attached), which was based on the LS1028A-RDB file. However, we couldn't establish an Ethernet communication (e.g. ping some local IP).&lt;BR /&gt;Is there something wrong with our DTS? Is there any documentation showing how to port the Switch in the SerDes protocol?&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Igor&lt;/P&gt;</description>
    <pubDate>Tue, 26 Jan 2021 19:04:47 GMT</pubDate>
    <dc:creator>igor_franco</dc:creator>
    <dc:date>2021-01-26T19:04:47Z</dc:date>
    <item>
      <title>LS1027A using a switch with SGMII</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1027A-using-a-switch-with-SGMII/m-p/1221414#M7395</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We are using the LS1027AE processor in a custom board with an Ethernet Switch (KSZ9477S, datasheet attached in this post) connected through SGMII1G-S in the Lane C of the SerDes protocol. This Switch will communicate via I2C with the processor during its configuration. According to the LS1028A Reference Manual, in the SerDes chapter, the SGMII1G-S uses the TSN Switch peripheral instead of ENETC. We configured the Switch as a slave I2C and the MDIO PHYs in our DTS (find it attached), which was based on the LS1028A-RDB file. However, we couldn't establish an Ethernet communication (e.g. ping some local IP).&lt;BR /&gt;Is there something wrong with our DTS? Is there any documentation showing how to port the Switch in the SerDes protocol?&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Igor&lt;/P&gt;</description>
      <pubDate>Tue, 26 Jan 2021 19:04:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1027A-using-a-switch-with-SGMII/m-p/1221414#M7395</guid>
      <dc:creator>igor_franco</dc:creator>
      <dc:date>2021-01-26T19:04:47Z</dc:date>
    </item>
    <item>
      <title>Re: LS1027A using a switch with SGMII</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1027A-using-a-switch-with-SGMII/m-p/1221908#M7403</link>
      <description>&lt;P&gt;I have forgotten to say that our U-Boot, RCW, and ATF version are LSDK-20.04-update-290520.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 27 Jan 2021 10:57:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1027A-using-a-switch-with-SGMII/m-p/1221908#M7403</guid>
      <dc:creator>igor_franco</dc:creator>
      <dc:date>2021-01-27T10:57:26Z</dc:date>
    </item>
    <item>
      <title>Re: LS1027A using a switch with SGMII</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1027A-using-a-switch-with-SGMII/m-p/1229240#M7501</link>
      <description>&lt;P&gt;I have solved the problem by myself.&lt;/P&gt;&lt;P&gt;For anyone that needs something similar.&lt;/P&gt;&lt;P&gt;The SGMII connection with Switch is considered MAC to MAC, once we don't have a PHY. For this kind of connection, it is not possible to use auto-negotiation. Therefore, the problem was solved just disabling the auto-negotiation on both the processor and the Switch, using a default full-duplex 1Gbps configuration. After this, everything works fine.&lt;/P&gt;&lt;P&gt;P.s.: I need to change the driver because the auto-negotiation register value was hardcoded.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Igor&lt;/P&gt;</description>
      <pubDate>Wed, 10 Feb 2021 10:23:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1027A-using-a-switch-with-SGMII/m-p/1229240#M7501</guid>
      <dc:creator>igor_franco</dc:creator>
      <dc:date>2021-02-10T10:23:07Z</dc:date>
    </item>
  </channel>
</rss>