<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 Re: LS1046ARDB NET-SNMP service cross-compile</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1046ARDB-NET-SNMP-service-cross-compile/m-p/1217870#M7364</link>
    <description>&lt;P&gt;leftover screenshots are here... please refer it. maximum 5 only i can share so here attached remaining.&lt;/P&gt;</description>
    <pubDate>Wed, 20 Jan 2021 10:35:02 GMT</pubDate>
    <dc:creator>Ghouse</dc:creator>
    <dc:date>2021-01-20T10:35:02Z</dc:date>
    <item>
      <title>LS1046ARDB NET-SNMP service cross-compile</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046ARDB-NET-SNMP-service-cross-compile/m-p/1217868#M7363</link>
      <description>&lt;P&gt;I have build net-snmp in ubantu 18.04.&lt;/P&gt;&lt;P&gt;./configure using cross compiler fsl-qoriql arrch64-fsl-linux-gnu, i am able to run service in ubuntu 18.04 successfully, but target machine is showing&lt;/P&gt;&lt;P&gt;.&lt;STRONG&gt;/snmpd -d -f -L &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;warning: no access control information configured &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;[config search path: /ncs/etc/snmp:/ncs/share/snmp:/ncs/lib/snmp:/root/.snmp]&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Run snmpconf -g basic-setup to help you configure the snmpd.conf file for this agent.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;service is started but I am not able to get the agent response in client side here are the attached screenshots.&amp;nbsp;&lt;/P&gt;&lt;P&gt;please help to get it sort it out.&lt;/P&gt;</description>
      <pubDate>Wed, 20 Jan 2021 10:32:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046ARDB-NET-SNMP-service-cross-compile/m-p/1217868#M7363</guid>
      <dc:creator>Ghouse</dc:creator>
      <dc:date>2021-01-20T10:32:55Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046ARDB NET-SNMP service cross-compile</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046ARDB-NET-SNMP-service-cross-compile/m-p/1217870#M7364</link>
      <description>&lt;P&gt;leftover screenshots are here... please refer it. maximum 5 only i can share so here attached remaining.&lt;/P&gt;</description>
      <pubDate>Wed, 20 Jan 2021 10:35:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046ARDB-NET-SNMP-service-cross-compile/m-p/1217870#M7364</guid>
      <dc:creator>Ghouse</dc:creator>
      <dc:date>2021-01-20T10:35:02Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046ARDB NET-SNMP service cross-compile</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046ARDB-NET-SNMP-service-cross-compile/m-p/1219318#M7373</link>
      <description>&lt;P&gt;Please run the following command to configure and generate&amp;nbsp;snmpd.conf in&amp;nbsp;/ncs/share/snmp&lt;/P&gt;
&lt;P&gt;$cd /ncs&lt;/P&gt;
&lt;P&gt;$ perl ./bin/snmpconf -i&lt;/P&gt;
&lt;P&gt;Please refer to the following link to configure&amp;nbsp;snmpd.conf file for the agent.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://kb.juniper.net/InfoCenter/index?page=content&amp;amp;id=KB25949" target="_blank"&gt;https://kb.juniper.net/InfoCenter/index?page=content&amp;amp;id=KB25949&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Then run command&lt;/P&gt;
&lt;P&gt;./sbin/snmpd -d -f -L&lt;/P&gt;</description>
      <pubDate>Fri, 22 Jan 2021 05:08:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046ARDB-NET-SNMP-service-cross-compile/m-p/1219318#M7373</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2021-01-22T05:08:22Z</dc:date>
    </item>
  </channel>
</rss>