<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: LS1043 soft reset persistent register</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1043-soft-reset-persistent-register/m-p/1216790#M7355</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/52411"&gt;@yipingwang&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;I see that this register has multiple read only bitfields.&lt;/P&gt;&lt;P&gt;It also has "Reserved" zones that are marked as writable.&lt;/P&gt;&lt;P&gt;So if I write to these "Reserved" zones(for example bits 24-31) should I expect the values to be persistent between resets?&lt;/P&gt;</description>
    <pubDate>Tue, 19 Jan 2021 10:09:42 GMT</pubDate>
    <dc:creator>sebastianpancea</dc:creator>
    <dc:date>2021-01-19T10:09:42Z</dc:date>
    <item>
      <title>LS1043 soft reset persistent register</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043-soft-reset-persistent-register/m-p/1211160#M7337</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm running Linux(LSDK19.06 based) on the LS1043 SoC and I need to pass the reboot reason to ATF/u-boot.&lt;/P&gt;&lt;P&gt;I searched the reference manual for a register that has its value persisted over soft resets but I couldn't find such a register.&lt;/P&gt;&lt;P&gt;Could you please advise on how to pass some information at Linux reboot to the bootloader stages?&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Wed, 13 Jan 2021 14:21:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043-soft-reset-persistent-register/m-p/1211160#M7337</guid>
      <dc:creator>sebastianpancea</dc:creator>
      <dc:date>2021-01-13T14:21:54Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043 soft reset persistent register</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043-soft-reset-persistent-register/m-p/1211626#M7338</link>
      <description>&lt;P&gt;&lt;SPAN&gt;You could&amp;nbsp;execute "fw_printenv" and "fw_setenv" to read and write u-boot environment in Linux before invoke soft reset. About how to create the configuration file, please refer to the last post in&amp;nbsp;&lt;A href="https://community.nxp.com/t5/Layerscape/How-to-build-fw-printenv-and-fw-setenv-for-LS1012AFRWY-OpenWrt/m-p/1012900" target="_blank"&gt;https://community.nxp.com/t5/Layerscape/How-to-build-fw-printenv-and-fw-setenv-for-LS1012AFRWY-OpenWrt/m-p/1012900&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 14 Jan 2021 08:51:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043-soft-reset-persistent-register/m-p/1211626#M7338</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2021-01-14T08:51:23Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043 soft reset persistent register</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043-soft-reset-persistent-register/m-p/1211953#M7342</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/52411"&gt;@yipingwang&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;Thank you for your reply!&lt;/P&gt;&lt;P&gt;Using "fw_setenv" tool, means storing the variable into non-volatile memory.&lt;/P&gt;&lt;P&gt;What I was asking for, is a CPU register or RAM zone that is persistent between reboots, and is cleared only when the SoC is powered down.&lt;/P&gt;&lt;P&gt;Other SoCs have such registers, for example IMX6: &lt;A href="https://community.nxp.com/t5/i-MX-Processors/iMX6-persistent-data-storage/m-p/648339#M99095" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/i-MX-Processors/iMX6-persistent-data-storage/m-p/648339#M99095&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Any idea of a similar feature on LS1043?&lt;/P&gt;</description>
      <pubDate>Thu, 14 Jan 2021 21:27:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043-soft-reset-persistent-register/m-p/1211953#M7342</guid>
      <dc:creator>sebastianpancea</dc:creator>
      <dc:date>2021-01-14T21:27:20Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043 soft reset persistent register</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043-soft-reset-persistent-register/m-p/1216784#M7354</link>
      <description>&lt;P&gt;Please refer to "DCFG_CCSR_RSTRQSR1" in LS1043 Reference Manual.&lt;/P&gt;</description>
      <pubDate>Tue, 19 Jan 2021 10:03:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043-soft-reset-persistent-register/m-p/1216784#M7354</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2021-01-19T10:03:03Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043 soft reset persistent register</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043-soft-reset-persistent-register/m-p/1216790#M7355</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/52411"&gt;@yipingwang&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;I see that this register has multiple read only bitfields.&lt;/P&gt;&lt;P&gt;It also has "Reserved" zones that are marked as writable.&lt;/P&gt;&lt;P&gt;So if I write to these "Reserved" zones(for example bits 24-31) should I expect the values to be persistent between resets?&lt;/P&gt;</description>
      <pubDate>Tue, 19 Jan 2021 10:09:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043-soft-reset-persistent-register/m-p/1216790#M7355</guid>
      <dc:creator>sebastianpancea</dc:creator>
      <dc:date>2021-01-19T10:09:42Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043 soft reset persistent register</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043-soft-reset-persistent-register/m-p/1216799#M7356</link>
      <description>&lt;P&gt;I tried to write to this register in the "Reserved" zones but it doesn't work&lt;/P&gt;</description>
      <pubDate>Tue, 19 Jan 2021 10:18:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043-soft-reset-persistent-register/m-p/1216799#M7356</guid>
      <dc:creator>sebastianpancea</dc:creator>
      <dc:date>2021-01-19T10:18:33Z</dc:date>
    </item>
  </channel>
</rss>