<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: Loading the uboot and kernel from the SPI NOR flash on the LS1043A based custom board?</title>
    <link>https://community.nxp.com/t5/Layerscape/Loading-the-uboot-and-kernel-from-the-SPI-NOR-flash-on-the/m-p/1205640#M7304</link>
    <description>&lt;P&gt;It is needed to build composite firmware image (1) and program it into the SPI Flash (2) - refer to the Layerscape SDK Documentation:&lt;/P&gt;
&lt;P&gt;1) &lt;A href="https://docs.nxp.com/bundle/GUID-3FFCCD77-5220-414D-8664-09E6FB1B02C6/page/GUID-EB58F77F-97D9-459A-A5F2-BCD4B6E8A93E.html" target="_blank"&gt;https://docs.nxp.com/bundle/GUID-3FFCCD77-5220-414D-8664-09E6FB1B02C6/page/GUID-EB58F77F-97D9-459A-A5F2-BCD4B6E8A93E.html&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;2) &lt;A href="https://docs.nxp.com/bundle/GUID-3FFCCD77-5220-414D-8664-09E6FB1B02C6/page/GUID-DCD3FA8A-CA37-4DCF-B96D-98B0AE591912.html" target="_blank"&gt;https://docs.nxp.com/bundle/GUID-3FFCCD77-5220-414D-8664-09E6FB1B02C6/page/GUID-DCD3FA8A-CA37-4DCF-B96D-98B0AE591912.html&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sun, 03 Jan 2021 10:16:27 GMT</pubDate>
    <dc:creator>ufedor</dc:creator>
    <dc:date>2021-01-03T10:16:27Z</dc:date>
    <item>
      <title>Loading the uboot and kernel from the SPI NOR flash on the LS1043A based custom board?</title>
      <link>https://community.nxp.com/t5/Layerscape/Loading-the-uboot-and-kernel-from-the-SPI-NOR-flash-on-the/m-p/1205638#M7302</link>
      <description>&lt;P&gt;How do I load the uboot and kernel from the SPI NOR flash on the&amp;nbsp;LS1043 based custom board?&lt;/P&gt;&lt;P&gt;(Assuming that the SPI Flash MTD driver is already present in the kernel and uboot).&lt;/P&gt;</description>
      <pubDate>Sun, 03 Jan 2021 09:16:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Loading-the-uboot-and-kernel-from-the-SPI-NOR-flash-on-the/m-p/1205638#M7302</guid>
      <dc:creator>ts1234</dc:creator>
      <dc:date>2021-01-03T09:16:27Z</dc:date>
    </item>
    <item>
      <title>Re: Loading the uboot and kernel from the SPI NOR flash on the LS1043A based custom board?</title>
      <link>https://community.nxp.com/t5/Layerscape/Loading-the-uboot-and-kernel-from-the-SPI-NOR-flash-on-the/m-p/1205640#M7304</link>
      <description>&lt;P&gt;It is needed to build composite firmware image (1) and program it into the SPI Flash (2) - refer to the Layerscape SDK Documentation:&lt;/P&gt;
&lt;P&gt;1) &lt;A href="https://docs.nxp.com/bundle/GUID-3FFCCD77-5220-414D-8664-09E6FB1B02C6/page/GUID-EB58F77F-97D9-459A-A5F2-BCD4B6E8A93E.html" target="_blank"&gt;https://docs.nxp.com/bundle/GUID-3FFCCD77-5220-414D-8664-09E6FB1B02C6/page/GUID-EB58F77F-97D9-459A-A5F2-BCD4B6E8A93E.html&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;2) &lt;A href="https://docs.nxp.com/bundle/GUID-3FFCCD77-5220-414D-8664-09E6FB1B02C6/page/GUID-DCD3FA8A-CA37-4DCF-B96D-98B0AE591912.html" target="_blank"&gt;https://docs.nxp.com/bundle/GUID-3FFCCD77-5220-414D-8664-09E6FB1B02C6/page/GUID-DCD3FA8A-CA37-4DCF-B96D-98B0AE591912.html&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 03 Jan 2021 10:16:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Loading-the-uboot-and-kernel-from-the-SPI-NOR-flash-on-the/m-p/1205640#M7304</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2021-01-03T10:16:27Z</dc:date>
    </item>
  </channel>
</rss>