<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: Loading LS1043ARDB's u-boot image using qemu-system-aarch64</title>
    <link>https://community.nxp.com/t5/Layerscape/Loading-LS1043ARDB-s-u-boot-image-using-qemu-system-aarch64/m-p/1205587#M7294</link>
    <description>&lt;P&gt;&lt;BR /&gt;u-Boot expects to run on a real hardware. Although in theory it is possible to &lt;BR /&gt;run it in a VM, such scenario is outside of the supported feature set in either &lt;BR /&gt;LSDK or OpenIL.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Platon&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sat, 02 Jan 2021 08:41:06 GMT</pubDate>
    <dc:creator>bpe</dc:creator>
    <dc:date>2021-01-02T08:41:06Z</dc:date>
    <item>
      <title>Loading LS1043ARDB's u-boot image using qemu-system-aarch64</title>
      <link>https://community.nxp.com/t5/Layerscape/Loading-LS1043ARDB-s-u-boot-image-using-qemu-system-aarch64/m-p/1205146#M7283</link>
      <description>&lt;P&gt;How do I load the&amp;nbsp;LS1043ARDB's u-boot.bin image on&amp;nbsp;qemu-system-aarch64?&lt;/P&gt;&lt;P&gt;It is working only for the linux kernel and rootfs, but it does not load the u-boot.bin (screen hang..no logs).&lt;/P&gt;&lt;P&gt;I have tried uboot from LSDK as well as from OpenIL.&lt;/P&gt;&lt;P&gt;I have also checked these uboot images with the latest qemu (5.2) release as well.&lt;/P&gt;</description>
      <pubDate>Wed, 30 Dec 2020 05:52:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Loading-LS1043ARDB-s-u-boot-image-using-qemu-system-aarch64/m-p/1205146#M7283</guid>
      <dc:creator>ts1234</dc:creator>
      <dc:date>2020-12-30T05:52:29Z</dc:date>
    </item>
    <item>
      <title>Re: Loading LS1043ARDB's u-boot image using qemu-system-aarch64</title>
      <link>https://community.nxp.com/t5/Layerscape/Loading-LS1043ARDB-s-u-boot-image-using-qemu-system-aarch64/m-p/1205587#M7294</link>
      <description>&lt;P&gt;&lt;BR /&gt;u-Boot expects to run on a real hardware. Although in theory it is possible to &lt;BR /&gt;run it in a VM, such scenario is outside of the supported feature set in either &lt;BR /&gt;LSDK or OpenIL.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Platon&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 02 Jan 2021 08:41:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Loading-LS1043ARDB-s-u-boot-image-using-qemu-system-aarch64/m-p/1205587#M7294</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2021-01-02T08:41:06Z</dc:date>
    </item>
  </channel>
</rss>