<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LS1027A with DDR3 failed on CodeWarrior - D_INIT timeout in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1027A-with-DDR3-failed-on-CodeWarrior-D-INIT-timeout/m-p/1205256#M7286</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We are using the LS1027AE processor in a custom board with a DDR3 (IS43/46TR16256BL-125K). We are trying to program its eMMC with the CodeWarrior. First, we try to run the diagnostic routine to see if is everything OK. After executing it, the target initialization script fails due to D_INIT timeout (ERR_DETECT = 0x80), making the "Test DDR memory access" failing it too. See the image below:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="TARGET_INIT.PNG" style="width: 636px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/133687iD95F4A4A4CD0CB62/image-dimensions/636x415?v=v2" width="636" height="415" role="button" title="TARGET_INIT.PNG" alt="TARGET_INIT.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Could someone help me to understand where our mistake is?&lt;/P&gt;&lt;P&gt;Obs.: Find our target initialization file, the DDR datasheet, and the CCS log (with log v) attached to this post.&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Igor&lt;/P&gt;</description>
    <pubDate>Wed, 30 Dec 2020 11:47:35 GMT</pubDate>
    <dc:creator>igor_franco</dc:creator>
    <dc:date>2020-12-30T11:47:35Z</dc:date>
    <item>
      <title>LS1027A with DDR3 failed on CodeWarrior - D_INIT timeout</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1027A-with-DDR3-failed-on-CodeWarrior-D-INIT-timeout/m-p/1205256#M7286</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We are using the LS1027AE processor in a custom board with a DDR3 (IS43/46TR16256BL-125K). We are trying to program its eMMC with the CodeWarrior. First, we try to run the diagnostic routine to see if is everything OK. After executing it, the target initialization script fails due to D_INIT timeout (ERR_DETECT = 0x80), making the "Test DDR memory access" failing it too. See the image below:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="TARGET_INIT.PNG" style="width: 636px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/133687iD95F4A4A4CD0CB62/image-dimensions/636x415?v=v2" width="636" height="415" role="button" title="TARGET_INIT.PNG" alt="TARGET_INIT.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Could someone help me to understand where our mistake is?&lt;/P&gt;&lt;P&gt;Obs.: Find our target initialization file, the DDR datasheet, and the CCS log (with log v) attached to this post.&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Igor&lt;/P&gt;</description>
      <pubDate>Wed, 30 Dec 2020 11:47:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1027A-with-DDR3-failed-on-CodeWarrior-D-INIT-timeout/m-p/1205256#M7286</guid>
      <dc:creator>igor_franco</dc:creator>
      <dc:date>2020-12-30T11:47:35Z</dc:date>
    </item>
    <item>
      <title>Re: LS1027A with DDR3 failed on CodeWarrior - D_INIT timeout</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1027A-with-DDR3-failed-on-CodeWarrior-D-INIT-timeout/m-p/1205530#M7291</link>
      <description>&lt;P&gt;Flash Programmer can operate even if DDR SDRAM is not initialized.&lt;/P&gt;
&lt;P&gt;Please use the CodeWarrior QCVS DDR Tool wizard and provide screenshot of the filled DDR configuration (refer to the attached).&lt;/P&gt;
&lt;P&gt;Please provide the processor connection schematics as PDF for inspection.&lt;/P&gt;</description>
      <pubDate>Fri, 01 Jan 2021 07:59:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1027A-with-DDR3-failed-on-CodeWarrior-D-INIT-timeout/m-p/1205530#M7291</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2021-01-01T07:59:17Z</dc:date>
    </item>
    <item>
      <title>Re: LS1027A with DDR3 failed on CodeWarrior - D_INIT timeout</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1027A-with-DDR3-failed-on-CodeWarrior-D-INIT-timeout/m-p/1220458#M7385</link>
      <description>&lt;P&gt;Hello ufedor,&lt;/P&gt;&lt;P&gt;Sorry for the late reply.&lt;/P&gt;&lt;P&gt;Using the DDR Tool Wizard, we were able to configure and program our eMMC device.&lt;/P&gt;&lt;P&gt;Thank you for your help.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Igor&lt;/P&gt;</description>
      <pubDate>Mon, 25 Jan 2021 10:37:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1027A-with-DDR3-failed-on-CodeWarrior-D-INIT-timeout/m-p/1220458#M7385</guid>
      <dc:creator>igor_franco</dc:creator>
      <dc:date>2021-01-25T10:37:58Z</dc:date>
    </item>
  </channel>
</rss>