<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Why does the OpenIL uses the ARM provided toolchain instead of Linaro's toolchain (used in LSDK)? in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Why-does-the-OpenIL-uses-the-ARM-provided-toolchain-instead-of/m-p/1204420#M7275</link>
    <description>&lt;P&gt;Why does the OpenIL uses the ARM provided toolchain instead of Linaro's toolchain (used in LSDK)?&lt;/P&gt;&lt;P&gt;Which one is the recommended toolchain for building the packages for LS1043ARDB?&lt;/P&gt;</description>
    <pubDate>Mon, 28 Dec 2020 04:42:09 GMT</pubDate>
    <dc:creator>ts1234</dc:creator>
    <dc:date>2020-12-28T04:42:09Z</dc:date>
    <item>
      <title>Why does the OpenIL uses the ARM provided toolchain instead of Linaro's toolchain (used in LSDK)?</title>
      <link>https://community.nxp.com/t5/Layerscape/Why-does-the-OpenIL-uses-the-ARM-provided-toolchain-instead-of/m-p/1204420#M7275</link>
      <description>&lt;P&gt;Why does the OpenIL uses the ARM provided toolchain instead of Linaro's toolchain (used in LSDK)?&lt;/P&gt;&lt;P&gt;Which one is the recommended toolchain for building the packages for LS1043ARDB?&lt;/P&gt;</description>
      <pubDate>Mon, 28 Dec 2020 04:42:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Why-does-the-OpenIL-uses-the-ARM-provided-toolchain-instead-of/m-p/1204420#M7275</guid>
      <dc:creator>ts1234</dc:creator>
      <dc:date>2020-12-28T04:42:09Z</dc:date>
    </item>
    <item>
      <title>Re: Why does the OpenIL uses the ARM provided toolchain instead of Linaro's toolchain (used in LSDK)</title>
      <link>https://community.nxp.com/t5/Layerscape/Why-does-the-OpenIL-uses-the-ARM-provided-toolchain-instead-of/m-p/1204772#M7279</link>
      <description>&lt;P&gt;LSDK and Open IL are different Linux kernel based ecosystems, each supporting&lt;BR /&gt;it's own set of target processors and software tools. Each of them use the&lt;BR /&gt;toolchain that is known to properly build all software comprising the target &lt;BR /&gt;image. These target images are different for Open IL adn for LSDK, although&lt;BR /&gt;the core components (Linux, TF-A, u-Boot) are the same. As you probably &lt;BR /&gt;noticed from my response in &lt;A href="https://community.nxp.com/t5/Layerscape/How-do-I-create-and-install-the-NOR-images-for-LS1043ARDB/td-p/1204421" target="_self"&gt;this thread&lt;/A&gt;, LSDK and Open IL&lt;BR /&gt;are different in supported feature sets. If you are selecting the toolcain for &lt;BR /&gt;your project, focus of the features you need, not on the toolchain version or &lt;BR /&gt;it's maintainer. If LSDK satisfies your requirements in a better way, stay with &lt;BR /&gt;LSDK and it's toolchain. Otherwise, consider other approaches like Open IL.&lt;BR /&gt;There is no signle SDK/BSP that can be recommended for all kinds of development&lt;BR /&gt;projects/user applications.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards&lt;BR /&gt;Platon&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 29 Dec 2020 06:49:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Why-does-the-OpenIL-uses-the-ARM-provided-toolchain-instead-of/m-p/1204772#M7279</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2020-12-29T06:49:35Z</dc:date>
    </item>
    <item>
      <title>Re: Why does the OpenIL uses the ARM provided toolchain instead of Linaro's toolchain (used in LSDK)</title>
      <link>https://community.nxp.com/t5/Layerscape/Why-does-the-OpenIL-uses-the-ARM-provided-toolchain-instead-of/m-p/1205143#M7282</link>
      <description>&lt;P&gt;I have noticed that the OpenIL toolchain's glibc does not provide&amp;nbsp;rpcsvc/*.h files. These are available in the Linaro's toolchain.&lt;/P&gt;&lt;P&gt;What was the reason behind the following commit in OpenIL?&lt;/P&gt;&lt;P&gt;&lt;A href="https://github.com/openil/openil/commit/7a8372dacc496a930be8abb39f5c812b2b7fa152#diff-1d29b6dee32177fcc52b4ea69ff253e15772194393f311b6af889665c853b778" target="_blank"&gt;https://github.com/openil/openil/commit/7a8372dacc496a930be8abb39f5c812b2b7fa152#diff-1d29b6dee32177fcc52b4ea69ff253e15772194393f311b6af889665c853b778&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 30 Dec 2020 05:42:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Why-does-the-OpenIL-uses-the-ARM-provided-toolchain-instead-of/m-p/1205143#M7282</guid>
      <dc:creator>ts1234</dc:creator>
      <dc:date>2020-12-30T05:42:34Z</dc:date>
    </item>
  </channel>
</rss>