<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: Buildroot for uboot+kernel+rfs</title>
    <link>https://community.nxp.com/t5/Layerscape/Buildroot-for-uboot-kernel-rfs/m-p/1203767#M7262</link>
    <description>&lt;P&gt;Can I use openil instead of the LSDK?&lt;/P&gt;&lt;P&gt;What is the relationship between OpenIL Linux and the LSDK Linux?&amp;nbsp; Which one should be preferred for LS1043A or LS1023A?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 23 Dec 2020 18:44:19 GMT</pubDate>
    <dc:creator>ts1234</dc:creator>
    <dc:date>2020-12-23T18:44:19Z</dc:date>
    <item>
      <title>Buildroot for uboot+kernel+rfs</title>
      <link>https://community.nxp.com/t5/Layerscape/Buildroot-for-uboot-kernel-rfs/m-p/1202983#M7254</link>
      <description>&lt;P&gt;How do I use LSDK's (flexbuild_lsdk2012.tgz) buildroot package for building uboot+kernel+rfs images.&lt;/P&gt;&lt;P&gt;Currently buildroot is only used for rootfs (rfs). Uboot and Kernel are built separately.&lt;/P&gt;&lt;P&gt;I am looking for the changes required for moving the kernel+uboot build from flex-builder script to buildroot. I also want to create the install images as well through buildroot.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 22 Dec 2020 09:09:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Buildroot-for-uboot-kernel-rfs/m-p/1202983#M7254</guid>
      <dc:creator>ts1234</dc:creator>
      <dc:date>2020-12-22T09:09:47Z</dc:date>
    </item>
    <item>
      <title>Re: Buildroot for uboot+kernel+rfs</title>
      <link>https://community.nxp.com/t5/Layerscape/Buildroot-for-uboot-kernel-rfs/m-p/1203767#M7262</link>
      <description>&lt;P&gt;Can I use openil instead of the LSDK?&lt;/P&gt;&lt;P&gt;What is the relationship between OpenIL Linux and the LSDK Linux?&amp;nbsp; Which one should be preferred for LS1043A or LS1023A?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 23 Dec 2020 18:44:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Buildroot-for-uboot-kernel-rfs/m-p/1203767#M7262</guid>
      <dc:creator>ts1234</dc:creator>
      <dc:date>2020-12-23T18:44:19Z</dc:date>
    </item>
    <item>
      <title>Re: Buildroot for uboot+kernel+rfs</title>
      <link>https://community.nxp.com/t5/Layerscape/Buildroot-for-uboot-kernel-rfs/m-p/1204008#M7265</link>
      <description>&lt;P&gt;You could generate firmware image with the following command in LSDK.&lt;/P&gt;
&lt;P&gt;$ flex-builder -i mkfw -m ls1043ardb -b nor&lt;/P&gt;
&lt;P&gt;The firmware image includes atf, Kernel image, dtb and rootfs filesystem.&lt;/P&gt;</description>
      <pubDate>Thu, 24 Dec 2020 06:57:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Buildroot-for-uboot-kernel-rfs/m-p/1204008#M7265</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2020-12-24T06:57:41Z</dc:date>
    </item>
    <item>
      <title>Re: Buildroot for uboot+kernel+rfs</title>
      <link>https://community.nxp.com/t5/Layerscape/Buildroot-for-uboot-kernel-rfs/m-p/1204016#M7266</link>
      <description>&lt;P&gt;You could use&amp;nbsp;&lt;SPAN&gt;openil&amp;nbsp; instead of LSDK.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Linux Kernel in Openil 1.9 or 1.10 is based on Linux Kernel&amp;nbsp; in LSDK 20.04.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;The applications in Openil are different from LSDK. Both LSDK and Openil support LS1043.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 24 Dec 2020 07:12:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Buildroot-for-uboot-kernel-rfs/m-p/1204016#M7266</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2020-12-24T07:12:02Z</dc:date>
    </item>
  </channel>
</rss>