<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: LS1027A with DDR3L</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1027A-with-DDR3L/m-p/1203087#M7258</link>
    <description>&lt;P&gt;Thank you for the fast answer ufedor.&lt;/P&gt;&lt;P&gt;I marked it as solved.&lt;/P&gt;</description>
    <pubDate>Tue, 22 Dec 2020 13:33:26 GMT</pubDate>
    <dc:creator>igor_franco</dc:creator>
    <dc:date>2020-12-22T13:33:26Z</dc:date>
    <item>
      <title>LS1027A with DDR3L</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1027A-with-DDR3L/m-p/1203042#M7256</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We are developing a custom board based on the LS1027A processor. We used the LS1028ARDB as an evaluation board to understand the functionality of the LS family. The kit uses four DDR4 of 1GB and another one as ECC. In our custom board, we want to use DDR3L instead of DDR4 (with ECC). According to the "Hardware and Layout Design Considerations for DDR4 SDRAM Memory Interfaces" (AN5097), the DQ swapping must consider the nibble:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="igor_franco_0-1608633263975.png" style="width: 462px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/133285i1EE41A5480D33D4A/image-dimensions/462x75?v=v2" width="462" height="75" role="button" title="igor_franco_0-1608633263975.png" alt="igor_franco_0-1608633263975.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;igor_franco_0-1608633263975.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;However, when we read the "Hardware and Layout Design Considerations for DDR3 SDRAM Memory Interfaces" (AN3940, identified in chapter 3.1 of "QorIQ LS1028A Design Checklist", AN12028), it says that the swapping can be performed in a byte:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="igor_franco_1-1608634005148.png" style="width: 485px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/133289i4AE89A5B6D25E8A6/image-dimensions/485x57?v=v2" width="485" height="57" role="button" title="igor_franco_1-1608634005148.png" alt="igor_franco_1-1608634005148.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;igor_franco_1-1608634005148.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;My question is: how can I configure the&amp;nbsp;DQ mapping register x (DDR_DQ_MAPx) to allows the swap inside a byte once it considers only nibbles? Is this register ignored with DDR3L?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you in advance,&lt;/P&gt;&lt;P&gt;Igor&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 22 Dec 2020 10:49:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1027A-with-DDR3L/m-p/1203042#M7256</guid>
      <dc:creator>igor_franco</dc:creator>
      <dc:date>2020-12-22T10:49:23Z</dc:date>
    </item>
    <item>
      <title>Re: LS1027A with DDR3L</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1027A-with-DDR3L/m-p/1203078#M7257</link>
      <description>&lt;P&gt;&amp;gt; Is this register ignored with DDR3L?&lt;/P&gt;
&lt;P&gt;DQ mapping is applicable for DDR4 SDRAM only.&lt;/P&gt;
&lt;P&gt;For DDR3L DQn_MAP registers can be left with default values.&lt;/P&gt;</description>
      <pubDate>Tue, 22 Dec 2020 13:15:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1027A-with-DDR3L/m-p/1203078#M7257</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2020-12-22T13:15:01Z</dc:date>
    </item>
    <item>
      <title>Re: LS1027A with DDR3L</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1027A-with-DDR3L/m-p/1203087#M7258</link>
      <description>&lt;P&gt;Thank you for the fast answer ufedor.&lt;/P&gt;&lt;P&gt;I marked it as solved.&lt;/P&gt;</description>
      <pubDate>Tue, 22 Dec 2020 13:33:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1027A-with-DDR3L/m-p/1203087#M7258</guid>
      <dc:creator>igor_franco</dc:creator>
      <dc:date>2020-12-22T13:33:26Z</dc:date>
    </item>
  </channel>
</rss>