<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: LS1046A 10G SFP+ operation issue</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1046A-10G-SFP-operation-issue/m-p/1201254#M7245</link>
    <description>&lt;P&gt;If you are interfacing LS1046A XFI port to an SFP+ without a PHY, make sure &lt;BR /&gt;you have a retimer in between, like it is done on &lt;A href="http://%20https://www.nxp.com/design/qoriq-developer-resources/layerscape-ls1046a-reference-design-board:LS1046A-RDB" target="_self"&gt;LS1046A-RDB&lt;/A&gt;. The link may&lt;BR /&gt;fail in either direction otherwise. As of the transmitter displayed as internal &lt;BR /&gt;or external in ethtool output, since you are using a "fixed-link", which is &lt;BR /&gt;effectively a zero-PHY driver, this filed is not meaningful.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Platon&lt;/P&gt;</description>
    <pubDate>Thu, 17 Dec 2020 13:55:25 GMT</pubDate>
    <dc:creator>bpe</dc:creator>
    <dc:date>2020-12-17T13:55:25Z</dc:date>
    <item>
      <title>LS1046A 10G SFP+ operation issue</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-10G-SFP-operation-issue/m-p/1199617#M7218</link>
      <description>&lt;P&gt;I have a question about 10G SFP+ operation of lsdk 2004.&lt;/P&gt;&lt;P&gt;After 10G bring-up, i can see interface of 10G SFP+.&lt;/P&gt;&lt;P&gt;And tx count is up. but when i tried ping-test, there was no response. so&amp;nbsp;10G RX operation is not working.&lt;/P&gt;&lt;P&gt;so i check interface with ethtool. i found out that Transceiver is internal mode.&amp;nbsp;&lt;/P&gt;&lt;P&gt;i think Transceiver would be external when fixed-link used.&amp;nbsp;&lt;/P&gt;&lt;P&gt;may i have the reason&amp;nbsp; about rx operation fail ?&lt;/P&gt;&lt;P&gt;i attach some information about status.&lt;/P&gt;&lt;P&gt;* ethtool info.&lt;/P&gt;&lt;P&gt;root@TinyLinux:~# ethtool fm1-mac9&lt;BR /&gt;Settings for fm1-mac9:&lt;BR /&gt;Supported ports: [ ]&lt;BR /&gt;Supported link modes: Not reported&lt;BR /&gt;Supported pause frame use: No&lt;BR /&gt;Supports auto-negotiation: No&lt;BR /&gt;Supported FEC modes: Not reported&lt;BR /&gt;Advertised link modes: Not reported&lt;BR /&gt;Advertised pause frame use: No&lt;BR /&gt;Advertised auto-negotiation: No&lt;BR /&gt;Advertised FEC modes: Not reported&lt;BR /&gt;Speed: 10000Mb/s&lt;BR /&gt;Duplex: Full&lt;BR /&gt;Port: MII&lt;BR /&gt;PHYAD: 0&lt;BR /&gt;Transceiver: internal&lt;BR /&gt;Auto-negotiation: on&lt;BR /&gt;Supports Wake-on: d&lt;BR /&gt;Wake-on: d&lt;BR /&gt;Current message level: 0xffffffff (-1)&lt;BR /&gt;drv probe link timer ifdown ifup rx_err tx_err tx_queued intr tx_done rx_status pktdata hw wol 0xffff8000&lt;BR /&gt;Link detected: yes&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;* ifconfig info&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;root@TinyLinux:~# ifconfig&lt;BR /&gt;fm1-mac9 Link encap:Ethernet HWaddr 00:04:9f:05:3d:0b&lt;BR /&gt;inet addr:192.168.47.131 Bcast:192.168.47.255 Mask:255.255.255.0&lt;BR /&gt;inet6 addr: fe80::204:9fff:fe05:3d0b/64 Scope:Link&lt;BR /&gt;UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1&lt;BR /&gt;RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:9 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:1000&lt;BR /&gt;RX bytes:0 (0.0 B) TX bytes:726 (726.0 B)&lt;BR /&gt;Memory:1af0000-1af0fff&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;* Device Tree Info.&lt;/P&gt;&lt;P&gt;&amp;amp;fman0 {&lt;BR /&gt;ethernet@e4000 {&lt;BR /&gt;phy-handle = &amp;lt;&amp;amp;rgmii_phy1&amp;gt;;&lt;BR /&gt;phy-connection-type = "rgmii-id";&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;ethernet@f0000 { /* 10GEC1 */&lt;BR /&gt;fixed-link = &amp;lt;0 1 10000 0 0&amp;gt;;&lt;BR /&gt;phy-connection-type = "xgmii";&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;mdio@fc000 {&lt;BR /&gt;rgmii_phy1: ethernet-phy@1 {&lt;BR /&gt;reg = &amp;lt;0x0&amp;gt;;&lt;BR /&gt;};&lt;BR /&gt;};&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;* mac reg info&lt;/P&gt;&lt;P&gt;root@TinyLinux:/sys/class/net/fm1-mac9# cat mac_regs&lt;BR /&gt;-------&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;FM MAC - MEMAC -0 (0x8645D000)&lt;BR /&gt;----------------------------------------&lt;/P&gt;&lt;P&gt;0x008645D008: 0x00020843 command_config&lt;BR /&gt;0x008645D00C: 0x059f0400 mac_addr0.mac_addr_l&lt;BR /&gt;0x008645D010: 0x00000b3d mac_addr0.mac_addr_u&lt;BR /&gt;0x008645D014: 0x00002580 maxfrm&lt;BR /&gt;0x008645D02C: 0x00000130 hashtable_ctrl&lt;BR /&gt;0x008645D040: 0x00000042 ievent&lt;BR /&gt;0x008645D044: 0x0000000c tx_ipg_length&lt;BR /&gt;0x008645D04C: 0x63000000 imask&lt;BR /&gt;0x008645D054: 0x0000f000 pause_quanta[i]&lt;BR /&gt;0x008645D058: 0x00000000 pause_quanta[i]&lt;BR /&gt;0x008645D05C: 0x00000000 pause_quanta[i]&lt;BR /&gt;0x008645D060: 0x00000000 pause_quanta[i]&lt;BR /&gt;0x008645D064: 0x00000000 pause_thresh[i]&lt;BR /&gt;0x008645D068: 0x00000000 pause_thresh[i]&lt;BR /&gt;0x008645D06C: 0x00000000 pause_thresh[i]&lt;BR /&gt;0x008645D070: 0x00000000 pause_thresh[i]&lt;BR /&gt;0x008645D074: 0x00000000 rx_pause_status&lt;BR /&gt;0x008645D080: 0x00000000 mac_addr[i].mac_addr_l&lt;BR /&gt;0x008645D084: 0x00000000 mac_addr[i].mac_addr_u&lt;BR /&gt;0x008645D088: 0x00000000 mac_addr[i].mac_addr_l&lt;BR /&gt;0x008645D08C: 0x00000000 mac_addr[i].mac_addr_u&lt;BR /&gt;0x008645D090: 0x00000000 mac_addr[i].mac_addr_l&lt;BR /&gt;0x008645D094: 0x00000000 mac_addr[i].mac_addr_u&lt;BR /&gt;0x008645D098: 0x00000000 mac_addr[i].mac_addr_l&lt;BR /&gt;0x008645D09C: 0x00000000 mac_addr[i].mac_addr_u&lt;BR /&gt;0x008645D0A0: 0x00000000 mac_addr[i].mac_addr_l&lt;BR /&gt;0x008645D0A4: 0x00000000 mac_addr[i].mac_addr_u&lt;BR /&gt;0x008645D0A8: 0x00000000 mac_addr[i].mac_addr_l&lt;BR /&gt;0x008645D0AC: 0x00000000 mac_addr[i].mac_addr_u&lt;BR /&gt;0x008645D0B0: 0x00000000 mac_addr[i].mac_addr_l&lt;BR /&gt;0x008645D0B4: 0x00000000 mac_addr[i].mac_addr_u&lt;BR /&gt;0x008645D0B8: 0x00002000 lpwake_timer&lt;BR /&gt;0x008645D0BC: 0x00000000 sleep_timer&lt;BR /&gt;0x008645D0E0: 0x00000000 statn_config&lt;BR /&gt;0x008645D300: 0x00000000 if_mode&lt;BR /&gt;0x008645D304: 0x00002000 if_status&lt;BR /&gt;0x008645D340: 0x00000000 hg_config&lt;BR /&gt;0x008645D350: 0x00000000 hg_pause_quanta&lt;BR /&gt;0x008645D360: 0x00000000 hg_pause_thresh&lt;BR /&gt;0x008645D370: 0x00000000 hgrx_pause_status&lt;BR /&gt;0x008645D374: 0x00000000 hg_fifos_status&lt;BR /&gt;0x008645D378: 0x00000000 rhm&lt;BR /&gt;0x008645D37C: 0x00000000 thm&lt;BR /&gt;root@TinyLinux:/sys/class/net/fm1-mac9#&lt;/P&gt;&lt;P&gt;root@TinyLinux:/sys/class/net/fm1-mac9/statistics# ls&lt;BR /&gt;collisions rx_errors rx_over_errors tx_dropped&lt;BR /&gt;multicast rx_fifo_errors rx_packets tx_errors&lt;BR /&gt;rx_bytes rx_frame_errors tx_aborted_errors tx_fifo_errors&lt;BR /&gt;rx_compressed rx_length_errors tx_bytes tx_heartbeat_errors&lt;BR /&gt;rx_crc_errors rx_missed_errors tx_carrier_errors tx_packets&lt;BR /&gt;rx_dropped rx_nohandler tx_compressed tx_window_errors&lt;BR /&gt;root@TinyLinux:/sys/class/net/fm1-mac9/statistics# cat tx_bytes&lt;BR /&gt;866&lt;BR /&gt;root@TinyLinux:/sys/class/net/fm1-mac9/statistics# cat rx_errors&lt;BR /&gt;0&lt;BR /&gt;root@TinyLinux:/sys/class/net/fm1-mac9/statistics# cat rx_bytes&lt;BR /&gt;0&lt;BR /&gt;root@TinyLinux:/sys/class/net/fm1-mac9/statistics#&lt;/P&gt;</description>
      <pubDate>Tue, 15 Dec 2020 11:06:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-10G-SFP-operation-issue/m-p/1199617#M7218</guid>
      <dc:creator>JSKIM</dc:creator>
      <dc:date>2020-12-15T11:06:24Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A 10G SFP+ operation issue</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-10G-SFP-operation-issue/m-p/1201254#M7245</link>
      <description>&lt;P&gt;If you are interfacing LS1046A XFI port to an SFP+ without a PHY, make sure &lt;BR /&gt;you have a retimer in between, like it is done on &lt;A href="http://%20https://www.nxp.com/design/qoriq-developer-resources/layerscape-ls1046a-reference-design-board:LS1046A-RDB" target="_self"&gt;LS1046A-RDB&lt;/A&gt;. The link may&lt;BR /&gt;fail in either direction otherwise. As of the transmitter displayed as internal &lt;BR /&gt;or external in ethtool output, since you are using a "fixed-link", which is &lt;BR /&gt;effectively a zero-PHY driver, this filed is not meaningful.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Platon&lt;/P&gt;</description>
      <pubDate>Thu, 17 Dec 2020 13:55:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-10G-SFP-operation-issue/m-p/1201254#M7245</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2020-12-17T13:55:25Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A 10G SFP+ operation issue</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-10G-SFP-operation-issue/m-p/1204271#M7253</link>
      <description>I have created a new topic for your recent questions. Please avoid asking unrelated questions in a single thread in future,</description>
      <pubDate>Tue, 22 Dec 2020 02:56:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-10G-SFP-operation-issue/m-p/1204271#M7253</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2020-12-22T02:56:33Z</dc:date>
    </item>
  </channel>
</rss>