<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ls1028ardb - How to change Code Warrior settings when changing emmc chip in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/ls1028ardb-How-to-change-Code-Warrior-settings-when-changing/m-p/1199554#M7217</link>
    <description>&lt;P&gt;You could refer to section "CodeWarrior Connects to the Bare Board to do Flash Programing" in&amp;nbsp;&lt;A href="https://community.nxp.com/t5/CodeWarrior-for-QorIQ-Knowledge/Use-CodeWarrior-for-ARMv8-to-Debug-U-boot-and-Linux-Kernel-and/ta-p/1114872?attachment-id=18546" target="_blank"&gt;https://community.nxp.com/t5/CodeWarrior-for-QorIQ-Knowledge/Use-CodeWarrior-for-ARMv8-to-Debug-U-boot-and-Linux-Kernel-and/ta-p/1114872?attachment-id=18546&lt;/A&gt;&amp;nbsp;to do flash programing with CodeWarrior.&lt;/P&gt;
&lt;P&gt;To program the empty custom board without valid RCW on the target board, you could modify "USE_SAFE_RCW = True" in CodeWarrior initialization file to use hard-coded RCW to connect to the target board, then do flash programming.&lt;/P&gt;
&lt;P&gt;In CodeWarrior, all eMMC device uses algorithm&amp;nbsp;SD_MMC.bin, so it is possible to use same eMMC flash algorithm even you&lt;SPAN&gt;&amp;nbsp;change the eMmc chip to another manufacturer's chip.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 15 Dec 2020 09:33:00 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2020-12-15T09:33:00Z</dc:date>
    <item>
      <title>ls1028ardb - How to change Code Warrior settings when changing emmc chip</title>
      <link>https://community.nxp.com/t5/Layerscape/ls1028ardb-How-to-change-Code-Warrior-settings-when-changing/m-p/1199408#M7212</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi, I'm using ls1028ardb.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;We are making custom boards, and we are trying to use emmc chips as chips other than those in bsp.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;SPAN&gt;The question here is,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;When I download image to the board using Code Warrior, is there anything need to set up? When connect the board to the host PC, it automatically recognizes the board, and I wonder if it recognizes the same thing even if I change the eMmc chip to another manufacturer's chip.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 15 Dec 2020 06:40:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/ls1028ardb-How-to-change-Code-Warrior-settings-when-changing/m-p/1199408#M7212</guid>
      <dc:creator>pjw</dc:creator>
      <dc:date>2020-12-15T06:40:09Z</dc:date>
    </item>
    <item>
      <title>Re: ls1028ardb - How to change Code Warrior settings when changing emmc chip</title>
      <link>https://community.nxp.com/t5/Layerscape/ls1028ardb-How-to-change-Code-Warrior-settings-when-changing/m-p/1199554#M7217</link>
      <description>&lt;P&gt;You could refer to section "CodeWarrior Connects to the Bare Board to do Flash Programing" in&amp;nbsp;&lt;A href="https://community.nxp.com/t5/CodeWarrior-for-QorIQ-Knowledge/Use-CodeWarrior-for-ARMv8-to-Debug-U-boot-and-Linux-Kernel-and/ta-p/1114872?attachment-id=18546" target="_blank"&gt;https://community.nxp.com/t5/CodeWarrior-for-QorIQ-Knowledge/Use-CodeWarrior-for-ARMv8-to-Debug-U-boot-and-Linux-Kernel-and/ta-p/1114872?attachment-id=18546&lt;/A&gt;&amp;nbsp;to do flash programing with CodeWarrior.&lt;/P&gt;
&lt;P&gt;To program the empty custom board without valid RCW on the target board, you could modify "USE_SAFE_RCW = True" in CodeWarrior initialization file to use hard-coded RCW to connect to the target board, then do flash programming.&lt;/P&gt;
&lt;P&gt;In CodeWarrior, all eMMC device uses algorithm&amp;nbsp;SD_MMC.bin, so it is possible to use same eMMC flash algorithm even you&lt;SPAN&gt;&amp;nbsp;change the eMmc chip to another manufacturer's chip.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 15 Dec 2020 09:33:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/ls1028ardb-How-to-change-Code-Warrior-settings-when-changing/m-p/1199554#M7217</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2020-12-15T09:33:00Z</dc:date>
    </item>
  </channel>
</rss>