<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Temperature sensor on LS1043ARDB in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Temperature-sensor-on-LS1043ARDB/m-p/1199098#M7208</link>
    <description>&lt;P&gt;I have tried lm-sensors to check the temperature. No external device is connected to LS1043ARDB.&lt;/P&gt;&lt;P&gt;Why do I see a high value on temp2?&lt;/P&gt;&lt;P&gt;root@localhost:~# sensors&lt;BR /&gt;adt7461-i2c-0-4c&lt;BR /&gt;Adapter: 2180000.i2c&lt;BR /&gt;temp1: +59.0 C (low = +0.0 C, high = +70.0 C)&lt;BR /&gt;(crit = +85.0 C, hyst = +75.0 C)&lt;BR /&gt;temp2: +76.1 C (low = +0.0 C, high = +70.0 C) ALARM (HIGH)&lt;BR /&gt;(crit = +85.0 C, hyst = +75.0 C)&lt;/P&gt;&lt;P&gt;root@localhost:~#&lt;/P&gt;</description>
    <pubDate>Mon, 14 Dec 2020 18:14:29 GMT</pubDate>
    <dc:creator>ts1234</dc:creator>
    <dc:date>2020-12-14T18:14:29Z</dc:date>
    <item>
      <title>Temperature sensor on LS1043ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/Temperature-sensor-on-LS1043ARDB/m-p/1198679#M7198</link>
      <description>&lt;P&gt;Is there any temperature sensor available on&amp;nbsp;LS1043ARDB?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 14 Dec 2020 07:35:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Temperature-sensor-on-LS1043ARDB/m-p/1198679#M7198</guid>
      <dc:creator>ts1234</dc:creator>
      <dc:date>2020-12-14T07:35:56Z</dc:date>
    </item>
    <item>
      <title>Re: Temperature sensor on LS1043ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/Temperature-sensor-on-LS1043ARDB/m-p/1199062#M7204</link>
      <description>&lt;P&gt;Please refer to the QorIQ LS1043A Reference Design Board Reference Manual, 4.4 Temperature anode and cathode:&lt;/P&gt;
&lt;P&gt;"The LS1043ARDB has two pins, TD1_Anode and TD1_Cathode. These pins are connected to a thermal body diode on the die that allows direct temperature measurement. The pins are connected to an SA56004ED device (U45) with dual-channel thermal monitor. This allows you to take direct die temperature readings with an accuracy of ±1 °C."&lt;/P&gt;</description>
      <pubDate>Mon, 14 Dec 2020 16:37:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Temperature-sensor-on-LS1043ARDB/m-p/1199062#M7204</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2020-12-14T16:37:53Z</dc:date>
    </item>
    <item>
      <title>Re: Temperature sensor on LS1043ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/Temperature-sensor-on-LS1043ARDB/m-p/1199098#M7208</link>
      <description>&lt;P&gt;I have tried lm-sensors to check the temperature. No external device is connected to LS1043ARDB.&lt;/P&gt;&lt;P&gt;Why do I see a high value on temp2?&lt;/P&gt;&lt;P&gt;root@localhost:~# sensors&lt;BR /&gt;adt7461-i2c-0-4c&lt;BR /&gt;Adapter: 2180000.i2c&lt;BR /&gt;temp1: +59.0 C (low = +0.0 C, high = +70.0 C)&lt;BR /&gt;(crit = +85.0 C, hyst = +75.0 C)&lt;BR /&gt;temp2: +76.1 C (low = +0.0 C, high = +70.0 C) ALARM (HIGH)&lt;BR /&gt;(crit = +85.0 C, hyst = +75.0 C)&lt;/P&gt;&lt;P&gt;root@localhost:~#&lt;/P&gt;</description>
      <pubDate>Mon, 14 Dec 2020 18:14:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Temperature-sensor-on-LS1043ARDB/m-p/1199098#M7208</guid>
      <dc:creator>ts1234</dc:creator>
      <dc:date>2020-12-14T18:14:29Z</dc:date>
    </item>
  </channel>
</rss>