<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Linux device tree interrupt IDs in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Linux-device-tree-interrupt-IDs/m-p/472677#M715</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to enable the SECMON_LP RTC on the LS1021ATWR dev board using the svns_rtc driver.&amp;nbsp; I am trying to create an entry in the device tree file ls1021a.dtsi.&amp;nbsp; The bindings documentation states that the interrupts must be specified.&amp;nbsp; From table 5-1 of the ls1021a ARM, I see that the SECMON module is tied to PPI interrupts 142 and 143.&amp;nbsp; But looking at the .dtsi, I can't map any of the interrupt IDs in the device tree to table 5-1.&amp;nbsp; Where can I find the proper device tree interrupt IDS for the SECMON_LP RTC?&amp;nbsp; Thanks.&lt;/P&gt;&lt;P&gt;-Jason&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 19 Feb 2016 22:35:58 GMT</pubDate>
    <dc:creator>jasonhendrix</dc:creator>
    <dc:date>2016-02-19T22:35:58Z</dc:date>
    <item>
      <title>Linux device tree interrupt IDs</title>
      <link>https://community.nxp.com/t5/Layerscape/Linux-device-tree-interrupt-IDs/m-p/472677#M715</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to enable the SECMON_LP RTC on the LS1021ATWR dev board using the svns_rtc driver.&amp;nbsp; I am trying to create an entry in the device tree file ls1021a.dtsi.&amp;nbsp; The bindings documentation states that the interrupts must be specified.&amp;nbsp; From table 5-1 of the ls1021a ARM, I see that the SECMON module is tied to PPI interrupts 142 and 143.&amp;nbsp; But looking at the .dtsi, I can't map any of the interrupt IDs in the device tree to table 5-1.&amp;nbsp; Where can I find the proper device tree interrupt IDS for the SECMON_LP RTC?&amp;nbsp; Thanks.&lt;/P&gt;&lt;P&gt;-Jason&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Feb 2016 22:35:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Linux-device-tree-interrupt-IDs/m-p/472677#M715</guid>
      <dc:creator>jasonhendrix</dc:creator>
      <dc:date>2016-02-19T22:35:58Z</dc:date>
    </item>
    <item>
      <title>Re: Linux device tree interrupt IDs</title>
      <link>https://community.nxp.com/t5/Layerscape/Linux-device-tree-interrupt-IDs/m-p/472678#M716</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Basic information regarding interrupts property encoding can be found here:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://lxr.free-electrons.com/source/Documentation/devicetree/bindings/arm/gic.txt?v=3.10" title="http://lxr.free-electrons.com/source/Documentation/devicetree/bindings/arm/gic.txt?v=3.10"&gt;Linux/Documentation/devicetree/bindings/arm/gic.txt - Linux Cross Reference - Free Electrons&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The second cell, which is the interrupt number, is the chip Manual Table 5-1 value minus 32. See how&lt;/P&gt;&lt;P&gt;mapping is done in gic_irq_domain_xlate(), file irq-gic.c&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Platon&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 20 Feb 2016 03:22:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Linux-device-tree-interrupt-IDs/m-p/472678#M716</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2016-02-20T03:22:18Z</dc:date>
    </item>
  </channel>
</rss>