<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Set up hugepage in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Set-up-hugepage/m-p/1194787#M7144</link>
    <description>&lt;P&gt;Yes, these are the values I want to set.&lt;/P&gt;&lt;P&gt;But my question is where do I specify it?&lt;/P&gt;&lt;P&gt;I tried modifying /etc/sysctl.conf and /boot/grub/ls2088ardb_grub.cfg, both without success&lt;/P&gt;</description>
    <pubDate>Mon, 07 Dec 2020 15:21:43 GMT</pubDate>
    <dc:creator>LeNormich</dc:creator>
    <dc:date>2020-12-07T15:21:43Z</dc:date>
    <item>
      <title>Set up hugepage</title>
      <link>https://community.nxp.com/t5/Layerscape/Set-up-hugepage/m-p/1193356#M7125</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm on LS2088&lt;/P&gt;&lt;P&gt;I just wanted to know if there was another way of setting up hugepages than forcing the /boot/grub/ls2088ardb_grub.cfg&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;I feel like it's not the right way but i couldn't find other ways...&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Thu, 03 Dec 2020 16:05:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Set-up-hugepage/m-p/1193356#M7125</guid>
      <dc:creator>LeNormich</dc:creator>
      <dc:date>2020-12-03T16:05:14Z</dc:date>
    </item>
    <item>
      <title>Re: Set up hugepage</title>
      <link>https://community.nxp.com/t5/Layerscape/Set-up-hugepage/m-p/1194386#M7132</link>
      <description>&lt;P&gt;You could set up hugepage in Linux Kernel bootargs, please refer to the following.&lt;/P&gt;
&lt;P&gt;default_hugepagesz=1024m hugepagesz=1024m hugepages=8&lt;/P&gt;</description>
      <pubDate>Mon, 07 Dec 2020 05:15:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Set-up-hugepage/m-p/1194386#M7132</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2020-12-07T05:15:53Z</dc:date>
    </item>
    <item>
      <title>Re: Set up hugepage</title>
      <link>https://community.nxp.com/t5/Layerscape/Set-up-hugepage/m-p/1194787#M7144</link>
      <description>&lt;P&gt;Yes, these are the values I want to set.&lt;/P&gt;&lt;P&gt;But my question is where do I specify it?&lt;/P&gt;&lt;P&gt;I tried modifying /etc/sysctl.conf and /boot/grub/ls2088ardb_grub.cfg, both without success&lt;/P&gt;</description>
      <pubDate>Mon, 07 Dec 2020 15:21:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Set-up-hugepage/m-p/1194787#M7144</guid>
      <dc:creator>LeNormich</dc:creator>
      <dc:date>2020-12-07T15:21:43Z</dc:date>
    </item>
    <item>
      <title>Re: Set up hugepage</title>
      <link>https://community.nxp.com/t5/Layerscape/Set-up-hugepage/m-p/1201099#M7242</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Under u-boot, configure bootargs as the following.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;setenv bootargs "console=ttyS1,115200 root=/dev/ram0 earlycon=uart8250,mmio,0x21c0600 ramdisk_size=0x2000000 default_hugepagesz=1024m hugepagesz=1024m hugepages=8"&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 17 Dec 2020 08:41:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Set-up-hugepage/m-p/1201099#M7242</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2020-12-17T08:41:34Z</dc:date>
    </item>
  </channel>
</rss>