<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LS1028A DisplayPort Voltage Levels in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1028A-DisplayPort-Voltage-Levels/m-p/1189612#M7101</link>
    <description>&lt;P&gt;DP_HPD signal of the LS1028A is 3.3V tolerant.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;AUX signal path consists of two segments, first is DP bus itself (covered by VESA specifcations) and AC coupled connection to the LS1028A pins. &lt;BR /&gt;Max common mode voltage of 2.0V is a DP 1.3 specification. This DC voltage is removed from the LS1028A due to AC coupling. So in fact 1V supply is enough to be compliant with VESA specifications.&lt;/P&gt;
&lt;P&gt;Protection device is used for high-level ESD protection. It is connected to DP bus where the voltage can be as high as a sum of common mode voltage (DC) plus dynamic voltage of differential signals.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Bulat&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 26 Nov 2020 09:39:37 GMT</pubDate>
    <dc:creator>Bulat</dc:creator>
    <dc:date>2020-11-26T09:39:37Z</dc:date>
    <item>
      <title>LS1028A DisplayPort Voltage Levels</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1028A-DisplayPort-Voltage-Levels/m-p/1188471#M7081</link>
      <description>&lt;P&gt;I am working to interface the LS1028A's DisplayPort, and have questions surrounding the voltage level and limits for DisplayPort.&lt;/P&gt;&lt;P&gt;Described in the LS1028A datasheet, the power domain for DisplayPort is "DP_SVDD". This supply is based on a filtered VDD (1.0V). I have found several references to DisplayPort's physical interface being upwards of 3.3V. The DisplayPort lanes are outputs, but the DisplayPort Aux can be an input. I am concerned with a 3.3V signal on these pins if the domain is VDD. I found no reference to protection against this scenario.&lt;/P&gt;&lt;P&gt;Is there any input protection against receiving 3.3V on the DisplayPort Aux input? Can they accept this voltage?&lt;/P&gt;</description>
      <pubDate>Wed, 25 Nov 2020 00:07:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1028A-DisplayPort-Voltage-Levels/m-p/1188471#M7081</guid>
      <dc:creator>jimmymm</dc:creator>
      <dc:date>2020-11-25T00:07:52Z</dc:date>
    </item>
    <item>
      <title>Re: LS1028A DisplayPort Voltage Levels</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1028A-DisplayPort-Voltage-Levels/m-p/1188642#M7089</link>
      <description>&lt;P&gt;&lt;SPAN class="caseEventBody"&gt;&lt;SPAN class="caseEventRow"&gt;&lt;SPAN class="feeditemtext cxfeeditemtext"&gt;&amp;nbsp;I am not sure what are "several references to DisplayPort's physical interface being upwards of 3.3V", please clarify.&lt;BR /&gt;From our side, the user must not exceed specifications listed in the LS1028A data sheet.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="caseEventBody"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="caseEventBody"&gt;Bulat&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 25 Nov 2020 06:22:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1028A-DisplayPort-Voltage-Levels/m-p/1188642#M7089</guid>
      <dc:creator>Bulat</dc:creator>
      <dc:date>2020-11-25T06:22:42Z</dc:date>
    </item>
    <item>
      <title>Re: LS1028A DisplayPort Voltage Levels</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1028A-DisplayPort-Voltage-Levels/m-p/1189065#M7097</link>
      <description>&lt;P&gt;According to the VESA DisplayPort 1.2 standard, Hot Plug Detect has a voltage range of 2.25V minimum to 3.6V maximum. This is an input to the LS1028A with a OVDD (1.8V) power domain.&lt;/P&gt;&lt;P&gt;The LS1028A's AUX channel is an Input/Output and has peak-to-peak differential voltages ranging up to 1.38V with a max common mode voltage of 2.0V. The power domain for these pins are DP_SVDD (1.0V).&amp;nbsp;&lt;/P&gt;&lt;P&gt;Many protection circuitry components targeted for DisplayPort applications include a working voltage of 3.3V. This includes the Nexperia&amp;nbsp;PUSB3FR4 utilized on the LS1028A's Reference Design Board.&lt;/P&gt;</description>
      <pubDate>Wed, 25 Nov 2020 15:11:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1028A-DisplayPort-Voltage-Levels/m-p/1189065#M7097</guid>
      <dc:creator>jimmymm</dc:creator>
      <dc:date>2020-11-25T15:11:06Z</dc:date>
    </item>
    <item>
      <title>Re: LS1028A DisplayPort Voltage Levels</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1028A-DisplayPort-Voltage-Levels/m-p/1189612#M7101</link>
      <description>&lt;P&gt;DP_HPD signal of the LS1028A is 3.3V tolerant.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;AUX signal path consists of two segments, first is DP bus itself (covered by VESA specifcations) and AC coupled connection to the LS1028A pins. &lt;BR /&gt;Max common mode voltage of 2.0V is a DP 1.3 specification. This DC voltage is removed from the LS1028A due to AC coupling. So in fact 1V supply is enough to be compliant with VESA specifications.&lt;/P&gt;
&lt;P&gt;Protection device is used for high-level ESD protection. It is connected to DP bus where the voltage can be as high as a sum of common mode voltage (DC) plus dynamic voltage of differential signals.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Bulat&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 26 Nov 2020 09:39:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1028A-DisplayPort-Voltage-Levels/m-p/1189612#M7101</guid>
      <dc:creator>Bulat</dc:creator>
      <dc:date>2020-11-26T09:39:37Z</dc:date>
    </item>
  </channel>
</rss>