<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LS1012A Boot from SD Card in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1012A-Boot-from-SD-Card/m-p/1188358#M7079</link>
    <description>&lt;P&gt;&amp;gt; Is it possible to boot from SD Card or eMMC?&lt;/P&gt;
&lt;P&gt;No - refer to the QorIQ LS1012A Reference Manual, Table 4-8. RCW source encodings.&lt;/P&gt;
&lt;P&gt;&amp;gt; Or the boot only can be performed by QSPI?&lt;/P&gt;
&lt;P&gt;Yes.&lt;/P&gt;</description>
    <pubDate>Tue, 24 Nov 2020 17:09:01 GMT</pubDate>
    <dc:creator>ufedor</dc:creator>
    <dc:date>2020-11-24T17:09:01Z</dc:date>
    <item>
      <title>LS1012A Boot from SD Card</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1012A-Boot-from-SD-Card/m-p/1188197#M7078</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm using the LS1012A Freeway board as an evaluation board. I noticed in the Getting Started Guide document that the board uses a QSPI to load the RCW. However, we desired to use only a MMC device. Is it possible to boot from SD Card or eMMC? Or the boot only can be performed by QSPI?&lt;/P&gt;&lt;P&gt;Thank you in advance,&lt;/P&gt;&lt;P&gt;Igor&lt;/P&gt;</description>
      <pubDate>Tue, 24 Nov 2020 12:44:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1012A-Boot-from-SD-Card/m-p/1188197#M7078</guid>
      <dc:creator>igor_franco</dc:creator>
      <dc:date>2020-11-24T12:44:57Z</dc:date>
    </item>
    <item>
      <title>Re: LS1012A Boot from SD Card</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1012A-Boot-from-SD-Card/m-p/1188358#M7079</link>
      <description>&lt;P&gt;&amp;gt; Is it possible to boot from SD Card or eMMC?&lt;/P&gt;
&lt;P&gt;No - refer to the QorIQ LS1012A Reference Manual, Table 4-8. RCW source encodings.&lt;/P&gt;
&lt;P&gt;&amp;gt; Or the boot only can be performed by QSPI?&lt;/P&gt;
&lt;P&gt;Yes.&lt;/P&gt;</description>
      <pubDate>Tue, 24 Nov 2020 17:09:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1012A-Boot-from-SD-Card/m-p/1188358#M7079</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2020-11-24T17:09:01Z</dc:date>
    </item>
    <item>
      <title>Re: LS1012A Boot from SD Card</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1012A-Boot-from-SD-Card/m-p/1188363#M7080</link>
      <description>&lt;P&gt;Hello, ufedor,&lt;/P&gt;&lt;P&gt;Thank you for your answer.&lt;/P&gt;&lt;P&gt;I will mark it as the solution.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Igor&lt;/P&gt;</description>
      <pubDate>Tue, 24 Nov 2020 17:15:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1012A-Boot-from-SD-Card/m-p/1188363#M7080</guid>
      <dc:creator>igor_franco</dc:creator>
      <dc:date>2020-11-24T17:15:44Z</dc:date>
    </item>
  </channel>
</rss>