<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: LS1046 data transfer via PCIe</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1046-data-transfer-via-PCIe/m-p/1188160#M7077</link>
    <description>&lt;P&gt;HI &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/52411"&gt;@yipingwang&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks for your response.&lt;/P&gt;&lt;P&gt;we are using LS1046 as RC.&lt;/P&gt;&lt;P&gt;Our requirement is to transfer data via PCIe using QDMA.Is this possible in LS1046.Does the DMA engine inside LS1046 support data transfer from LS1046 to a slave device via PCIe .If so can you provide any sample application ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 24 Nov 2020 12:06:37 GMT</pubDate>
    <dc:creator>diljithka</dc:creator>
    <dc:date>2020-11-24T12:06:37Z</dc:date>
    <item>
      <title>LS1046 data transfer via PCIe</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046-data-transfer-via-PCIe/m-p/1185922#M7033</link>
      <description>&lt;P&gt;Does LS1046 has the support data transfer via PCIe. we have a requirement for memory to pci memory and pci memory to memory t data transaction using this QDMA block in LS1046.Does LS1046 has the support for datat transfer via PCIe? can you provide the DMA driver support and sample application for the PCIe data transfer.?&lt;/P&gt;</description>
      <pubDate>Thu, 19 Nov 2020 09:54:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046-data-transfer-via-PCIe/m-p/1185922#M7033</guid>
      <dc:creator>diljithka</dc:creator>
      <dc:date>2020-11-19T09:54:09Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046 data transfer via PCIe</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046-data-transfer-via-PCIe/m-p/1187826#M7069</link>
      <description>&lt;P&gt;Do you use&amp;nbsp;LS1046 as EP or RC device?&lt;/P&gt;
&lt;P&gt;Please refer to the following in Linux source code.&lt;/P&gt;
&lt;P&gt;drivers/pci/controller/dwc/pci-layerscape-ep.c&lt;/P&gt;
&lt;P&gt;drivers/misc/pci_endpoint_test.c&lt;/P&gt;
&lt;P&gt;Documentation/PCI/endpoint/pci-test-howto.rst&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 24 Nov 2020 03:49:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046-data-transfer-via-PCIe/m-p/1187826#M7069</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2020-11-24T03:49:24Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046 data transfer via PCIe</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046-data-transfer-via-PCIe/m-p/1188160#M7077</link>
      <description>&lt;P&gt;HI &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/52411"&gt;@yipingwang&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks for your response.&lt;/P&gt;&lt;P&gt;we are using LS1046 as RC.&lt;/P&gt;&lt;P&gt;Our requirement is to transfer data via PCIe using QDMA.Is this possible in LS1046.Does the DMA engine inside LS1046 support data transfer from LS1046 to a slave device via PCIe .If so can you provide any sample application ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 24 Nov 2020 12:06:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046-data-transfer-via-PCIe/m-p/1188160#M7077</guid>
      <dc:creator>diljithka</dc:creator>
      <dc:date>2020-11-24T12:06:37Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046 data transfer via PCIe</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046-data-transfer-via-PCIe/m-p/1188719#M7090</link>
      <description>&lt;P&gt;We use the specific dmatest.c and fsl-qdma.c to test memory/PCIe DMA performance on ls1046a platform with LSDK kernel. We set PCIe address using:&lt;/P&gt;
&lt;P&gt;echo [#pcie addr] &amp;gt; /sys/module/dmatest/parameters/pci_phys_addr&lt;/P&gt;
&lt;P&gt;Please refer to Readme.txt in the attachment.&lt;/P&gt;</description>
      <pubDate>Wed, 25 Nov 2020 07:49:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046-data-transfer-via-PCIe/m-p/1188719#M7090</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2020-11-25T07:49:39Z</dc:date>
    </item>
  </channel>
</rss>