<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックPOR Status Register 1, How to set RSP_DIS bit</title>
    <link>https://community.nxp.com/t5/Layerscape/POR-Status-Register-1-How-to-set-RSP-DIS-bit/m-p/1187812#M7067</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;LS2044A&lt;/P&gt;&lt;P&gt;We want to use ASLEEP/GPIO1_28 as an output pin. But in the documentation, section&amp;nbsp;4.9.5 Power-On Reset Sequence Detailed Description, the ASLEEP signal is enabled if CFG_RSP_DIS=0.&lt;/P&gt;&lt;P&gt;The&amp;nbsp;CFG_RSP_DIS's value is defined in section&amp;nbsp;8.3.2 POR Status Register 1 (PORSR1).&lt;/P&gt;&lt;P&gt;But I cannot figure out which pin will enable or disable RSP_DIS bit at POR.&lt;/P&gt;&lt;P&gt;And I have the same question for PORSR1's SOC bit.&lt;/P&gt;&lt;P&gt;My question is: How I can select RSP_DIS and SOC bits in PORSR1 ?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Tue, 24 Nov 2020 03:10:40 GMT</pubDate>
    <dc:creator>benoitmasse</dc:creator>
    <dc:date>2020-11-24T03:10:40Z</dc:date>
    <item>
      <title>POR Status Register 1, How to set RSP_DIS bit</title>
      <link>https://community.nxp.com/t5/Layerscape/POR-Status-Register-1-How-to-set-RSP-DIS-bit/m-p/1187812#M7067</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;LS2044A&lt;/P&gt;&lt;P&gt;We want to use ASLEEP/GPIO1_28 as an output pin. But in the documentation, section&amp;nbsp;4.9.5 Power-On Reset Sequence Detailed Description, the ASLEEP signal is enabled if CFG_RSP_DIS=0.&lt;/P&gt;&lt;P&gt;The&amp;nbsp;CFG_RSP_DIS's value is defined in section&amp;nbsp;8.3.2 POR Status Register 1 (PORSR1).&lt;/P&gt;&lt;P&gt;But I cannot figure out which pin will enable or disable RSP_DIS bit at POR.&lt;/P&gt;&lt;P&gt;And I have the same question for PORSR1's SOC bit.&lt;/P&gt;&lt;P&gt;My question is: How I can select RSP_DIS and SOC bits in PORSR1 ?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Tue, 24 Nov 2020 03:10:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/POR-Status-Register-1-How-to-set-RSP-DIS-bit/m-p/1187812#M7067</guid>
      <dc:creator>benoitmasse</dc:creator>
      <dc:date>2020-11-24T03:10:40Z</dc:date>
    </item>
    <item>
      <title>Re: POR Status Register 1, How to set RSP_DIS bit</title>
      <link>https://community.nxp.com/t5/Layerscape/POR-Status-Register-1-How-to-set-RSP-DIS-bit/m-p/1187841#M7072</link>
      <description>&lt;P&gt;This is an internal factory-test config signal that we don't support for customers’ use and, most importantly, that customers do not need to use/tweak for proper operation of the device.&lt;/P&gt;
&lt;P&gt;As such, we'll pursue removing references to the signal name from the docs going forward.&lt;/P&gt;</description>
      <pubDate>Tue, 24 Nov 2020 04:20:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/POR-Status-Register-1-How-to-set-RSP-DIS-bit/m-p/1187841#M7072</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2020-11-24T04:20:49Z</dc:date>
    </item>
    <item>
      <title>Re: POR Status Register 1, How to set RSP_DIS bit</title>
      <link>https://community.nxp.com/t5/Layerscape/POR-Status-Register-1-How-to-set-RSP-DIS-bit/m-p/1188487#M7083</link>
      <description>&lt;P&gt;Ok,&amp;nbsp;&lt;/P&gt;&lt;P&gt;If I understand well, I do not have any restriction to use GPIO1_28. The ASLEEP will not be driven as output before RCW loading.&lt;/P&gt;&lt;P&gt;Reference Table 4.6 Reference Manual (09/2020) Stage 10,&amp;nbsp;&lt;/P&gt;&lt;P&gt;The ASLEEP pin is also enabled at this point if the Reset Sequence Pause is enabled&lt;BR /&gt;(CFG_RSP_DIS=0); otherwise ASLEEP pin is enabled later in the reset sequence.&lt;/P&gt;&lt;P&gt;Does not apply in my case.&lt;/P&gt;&lt;P&gt;Is it right ?&lt;/P&gt;</description>
      <pubDate>Wed, 25 Nov 2020 01:08:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/POR-Status-Register-1-How-to-set-RSP-DIS-bit/m-p/1188487#M7083</guid>
      <dc:creator>benoitmasse</dc:creator>
      <dc:date>2020-11-25T01:08:37Z</dc:date>
    </item>
  </channel>
</rss>