<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 IFC GPCM Burst Mode versus Address LS2044</title>
    <link>https://community.nxp.com/t5/Layerscape/IFC-GPCM-Burst-Mode-versus-Address-LS2044/m-p/1184152#M7008</link>
    <description>&lt;P&gt;Hi !&lt;/P&gt;&lt;P&gt;IFC in GPCM mode, 20 bit address.&lt;/P&gt;&lt;P&gt;The limit size of burst, is it limited by the number of bits on the unmuxed address bus ?&lt;/P&gt;&lt;P&gt;Let say we have a bus with 20 bit,&lt;/P&gt;&lt;P&gt;LSB are connected to A3-A2-A1-A0 and MSB are connected to AD15-0.&lt;/P&gt;&lt;P&gt;In case of 8 bits, the longest burst will be 16 beats.&lt;/P&gt;&lt;P&gt;In case of 16 bits, the longest burst will be 8 beats.&lt;/P&gt;&lt;P&gt;Merci beaucoup, Thank a lot&lt;/P&gt;&lt;P&gt;&amp;nbsp;Is this is correct ?&lt;/P&gt;</description>
    <pubDate>Tue, 17 Nov 2020 02:14:06 GMT</pubDate>
    <dc:creator>benoitmasse</dc:creator>
    <dc:date>2020-11-17T02:14:06Z</dc:date>
    <item>
      <title>IFC GPCM Burst Mode versus Address LS2044</title>
      <link>https://community.nxp.com/t5/Layerscape/IFC-GPCM-Burst-Mode-versus-Address-LS2044/m-p/1184152#M7008</link>
      <description>&lt;P&gt;Hi !&lt;/P&gt;&lt;P&gt;IFC in GPCM mode, 20 bit address.&lt;/P&gt;&lt;P&gt;The limit size of burst, is it limited by the number of bits on the unmuxed address bus ?&lt;/P&gt;&lt;P&gt;Let say we have a bus with 20 bit,&lt;/P&gt;&lt;P&gt;LSB are connected to A3-A2-A1-A0 and MSB are connected to AD15-0.&lt;/P&gt;&lt;P&gt;In case of 8 bits, the longest burst will be 16 beats.&lt;/P&gt;&lt;P&gt;In case of 16 bits, the longest burst will be 8 beats.&lt;/P&gt;&lt;P&gt;Merci beaucoup, Thank a lot&lt;/P&gt;&lt;P&gt;&amp;nbsp;Is this is correct ?&lt;/P&gt;</description>
      <pubDate>Tue, 17 Nov 2020 02:14:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/IFC-GPCM-Burst-Mode-versus-Address-LS2044/m-p/1184152#M7008</guid>
      <dc:creator>benoitmasse</dc:creator>
      <dc:date>2020-11-17T02:14:06Z</dc:date>
    </item>
    <item>
      <title>Re: IFC GPCM Burst Mode versus Address LS2044</title>
      <link>https://community.nxp.com/t5/Layerscape/IFC-GPCM-Burst-Mode-versus-Address-LS2044/m-p/1184260#M7009</link>
      <description>&lt;P&gt;Please consider that general address connection for the 8-bit data bus is:&lt;/P&gt;
&lt;P&gt;IFC_A[11:0] -&amp;gt; A[11:0]&lt;/P&gt;
&lt;P&gt;IFC_AD[15:0] -&amp;gt; A[27:12]&lt;/P&gt;
&lt;P&gt;and for 16-bit data bus it is:&lt;/P&gt;
&lt;P&gt;IFC_A[11:1] -&amp;gt; A[10:0]&lt;/P&gt;
&lt;P&gt;IFC_AD[15:0] -&amp;gt; A[26:11]&lt;/P&gt;
&lt;P&gt;The GPCM burst length is determined by the CSORn_GPCM[BURST_LEN] - refer to the QorIQ LS2088A Reference Manual, 17.3.6 Chip-Select Option register - GPCM (CSOR0_GPCM - CSOR7_GPCM).&lt;/P&gt;</description>
      <pubDate>Tue, 17 Nov 2020 06:26:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/IFC-GPCM-Burst-Mode-versus-Address-LS2044/m-p/1184260#M7009</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2020-11-17T06:26:33Z</dc:date>
    </item>
  </channel>
</rss>